Hi all,
My customer wonder that if the DVR RDK has the nand flash bad block management module in it? Because the u-boot kernel and filesystem are need to be flashed to nand flash. So he want to know if this module is already exist in the u-boot source code, it can scan and flag the bad block while booting, and then it can auto-skip the bad block while flah the image. And if so ,where can I find these part in the RDK, thanks!