This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM625: AM625 compatible PMIC options

Part Number: AM625
Other Parts Discussed in Thread: TPS6522005-EP

Tool/software:

Hi Team,

Initially, we were looking to use the TPS6521903 PMIC with the AM625 processor in our system. However, we require the storage temperature to be -55°C ~ 85°C, and the mentioned PMIC part doesn't support the lower side limit of the temperature. 

1. Could you please confirm if the TPS6521903 part would be able to meet the -55°C lower limit storage temperature requirement?

If not, we have found one another PMIC TPS6522005-EP that meets our storage temperature requirements.

2. Could you please confirm if this PMIC TPS6522005-EP is compatible with the AM625 processor?

Thanks & Regards,
Sahil Nayak

  • Hi Team,

    Please let us know if you have any updates to share with us.

  • Hi Team,

    We are looking for a quick response on this, so we can have further clarity to decide on the PMIC.

  • Hi Sahil, 

    Apologies for the delay, this thread was incorrectly assigned to the wrong team earlier. 

    1. As stated in the datasheet, unfortunately TPS6521903 is only qualified for -40°C lower limit storage temperature. This will not meet the -55°C requirement. 

    2. TPS6522005-EP is the extended performance device within the same family, this is qualified for -65°C lower limit.

    Yes, this device can be compatible with AM625. TPS6522005-EP is a user-programmable device, so the settings come as a blank configuration.
    The configuration can mirror that of the TPS6521903 configurations to be compatible with AM625.
    NVM programming details can be found in this document: https://www.ti.com/lit/pdf/SLVUCM5

    Let me know if you have any further questions about this device family or regarding the programming steps.

    Best Regards, 
    Sarah