This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

8168 evm spi0 eeprom

Hi

    I want to test the eeprom. but I can't find the related device point in /dev after the board's linux boot up.

From the evm schematics, the eeprom is connected to spi0.

Which name is the device point?

The EZSDK version which I am using is 5_02_02_60.