Tool/software:
Hi Ti Experts.
I config the DPI output.


Tool/software:
Hi Ti Experts.
I config the DPI output.


Hi,
To verify correct configuration, can you share the output of kmstest?
Our EVMs do not directly expose DPI, so difficult for us to directly probe PCLK.
Hello Divyansh Mittal:
here is the log after runing kmstest:
root@am62axx-evm:/opt/edgeai-gst-apps# kmstest
Connector 0/@40: DPI-1
Crtc 0/@38: 1280x720@79.24 76.782 1280/26/8/8/? 720/8/2/3/? 79 (79.24) 0x0 0x48
Plane 0/@31: 0,0-1280x720
Fb 49 1280x720-XR24
press enter to exit
Hi,
Thanks for confirming. Software-wise your DPI configuration seems to be working.
Let me check internally if we have the capability to verify the clocks. Please expect a response by mid next week.
Hi Meng,
The clock looks very weak. Can you please share the rest of the display schematics? Can you capture also one of the data signals so we be sure it is not an oscilloscope measurement issue?
Thanks,
Stan
Hi Meng,
Can you please try to short out R9723 = 0 and try measurement again?
Thanks,
Stan
Hi Meng,
VOUT0_PCLK does not look correct. You should be able to see something like below. Channel 1 is VOUT0_DATA0 and channel 2 is VOUT0_PCLK.

In out SKEVM, we are able to probe these signals on the HDMI transmitter. Is this what you see on the DPI side?
Best regards,
Luis Parga