Part Number: PROCESSOR-SDK-J784S4
Tool/software:
Hi experts,
I am using J784S4_EVM with SDK10.
In my case, I am trying to give firewall 104 (GPIOMUX INTRTR) from mcu1_0 to C7X_0.
I need a flexible mapping of the IRQ for different applications and I can't rebuild the mcu1_0 each time with a different config (config from sciclient_defaultBoardcfg_rm.c).
The master of my app will be the c7x core 0, that's why I would like to config the GPIOMUX INTRTR from this core.
I have modify Ipc_setupSciServer() of ipc_echo_testb_freertos application
/* give gpio interrupt router firewall to c7x core 1 */
struct tisci_msg_fwl_change_owner_info_req req_fw_change_owner = {
.fwl_id = (uint16_t) CSL_STD_FW_GPIOMUX_INTRTR0_INTR_ROUTER_CFG_ID,
.region = (uint16_t) 0,
.owner_index = (uint8_t) TISCI_HOST_ID_C7X_0_1
};
struct tisci_msg_fwl_change_owner_info_resp resp = {0};
uint32_t timeout = 0xFFFFFFFFU;
int32_t ret = CSL_PASS;
ret = Sciclient_firewallChangeOwnerInfo(&req_fw_change_owner, &resp, timeout);
if (ret != CSL_PASS)
{
App_printf("[Firewall] Error : failed change owner of gpio intrtr\n");
}
else
{
App_printf("[Firewall] change owner of gpio intrtr success\n");
}
I have rebuilt the SPL to boot on linux.
But the return value is != CSL_PASS.
When I try to change an other firewall owner with the same code, it works.
That's why, I would like to know if it is possible to change every firewall owner.
Thanks for your help
Charles