This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM368 performance same as DM365



Hi ,all

I confused  about the performance of DM368. I use dvsdk_2_10_00_17 and  kernel version is 2.6.18.

I modify the ubl according to http://processors.wiki.ti.com/index.php/DM36x_to_DM368_NAND_UBL_porting_guide.

and also provide 1.35V voltage.

When the board boot up ,I Cat /proc/davinci_clocks

# cat /proc/davinci_clocks
ADCIF_CLK 170000000 0
KEYSCAN_CLK 24000000 0
RTC_CLK 24000000 0
VOICECODEC_CLK 20571428 0
USBCLK 24000000 1
PWM3_CLK 24000000 0
PWM2_CLK 24000000 0
PWM1_CLK 24000000 0
PWM0_CLK 24000000 0
AEMIFCLK 170000000 3
gpio 170000000 1
SPICLK 170000000 1
MMCSDCLK1 97142857 1
MMCSDCLK0 97142857 1
McBSPCLK 170000000 1
I2CCLK 24000000 1
EMACCLK 170000000 1
HPI 170000000 0
UART1 24000000 1
UART0 24000000 1
ARMCLK 432000000 0

 

This seams that the ARMCLK is already  432MHz.

But the performance is not upgrade.

I tried H.264 encode ,Jpeg encode The performance of them are same as DM365.

There are some other details I should modify?

thanks

zhiqiang