This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AMIC120: EtherCAT Slave Controller (ESC) for LEO space application

Part Number: AMIC120
Other Parts Discussed in Thread: AMIC110, AM263P4

Tool/software:

Hi TI experts,

TI offers the AMIC110/120 and other processors/SOCs to support Ethernet based deterministic fieldbus protocols like EtherCAT.

If I needed an EtherCAT slave controller (ESC) component for a LEO (low earth orbit, "new space") space application, which component from TI's portfolio would I use?

As a minimum application requirement, the component would need to be packaged in space enhanced plastic (SEP) and test data should be available for 30 kRad TID (Si) and SEL immunity to 43MeV-cm2/mg at 125°C.

Any product TI currently could recommend to be used in this specific application scenario?

Thank you.