This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

NAND flash interface to OMAP3530



hi all

am working on devkit8000 board (OMAP 3530). i have to interface  MLC based 4 GByte NAND flash

(part number is MT29F32G08CBACAWP from micron) to GPIO pins.

The GPIO pins 132,133,134,135,136 137, 138 and 139 are configured as DATA input and output pins and

GPIO pins 130,131,141,156,167,158 and 159 are control pins like ALE,CE, CLE, WP, RE etc.

I have done pad configurations. I am looking a sample code for writing and reading data to/from the NAND flash,

 please share with me.

thanks and regards

N Reddy