Part Number: AM62A7-Q1
Hi,
We have desigend customized board taking reference of SK_AM62A_LP.
Changes from the EVK :1 : MMC1_SD_EN : Assignment changed from IO Expander (EVK) to SOC pin M21 (Custom Board).2 : Operation voltage for the data lines are 3.3V in the Custom Board.
Plesae help to debug below error while booting from SD card.
-Boot SPL 2024.04-ti-ga970f6e51043 (Nov 13 2024 - 14:26:23 +0000)
SYSFW ABI: 4.0 (firmware rev 0x000a '10.1.8--v10.01.08 (Fiery Fox)')
Trying to boot from MMC2
i2c_write: error waiting for data ACK (status=0x116)
pca953x gpio@22: Error reading output register
Card did not respond to voltage select! : -110
spl: mmc init failed with error: -95
SPL: failed to boot from all boot devices
### ERROR ### Please RESET the board ###
ÿ!E
Regards,
Tejas Patel