Other Parts Discussed in Thread: DM3730
When I was working with the MSP430F55xx chips I remember reading somewhere that you can create an MSC device and an HID device using only the USB peripheral on the MSP430. I am wondering if it is possible to do the same using the DM3730? Specifically, I am looking to stream video over USB using UVC and to use HID to control the actual device.
Is this possible? If so, can someone point me in the right direction? Any documentation on something similar would help.
Thanks!
NJC