Other Parts Discussed in Thread: SYSBIOS
Hi, compared to EZSDK 5.01/dm8168 I have heavy problems to get simple CE samples running on DSP of dm8148, with EZSDK 5.03. F.e. universal_copy, started this way:
CE_DEBUG=3 ./app_remote.xv5T -p DSP -e universal_copy -s xe674
leads to an infinite loop of these messages:
Ipc_attach: Ipc_procSyncStart failed!
Obviously there are differences between the CMEM settings between EZSDK 5.03 for dm8168 and the EZSDK 5.03 for dm8148. I am very unsure about at which positions I should change the memory map configration - if at all this is the reason for the problem.
Regards,
Joern.