This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM620-Q1: Does AM620-Q1 support the I2S interface to STA710?

Part Number: AM620-Q1

Hi team,

does AM620-Q1 HSI2S driver support the modified I2S data format "HD-Radio" of ST Micro STA710?

HD AM/FM has 32Bit per frame and in none HD radios (AM/FM/DAB) format will look 100% the same way, but frames are then only 24Bit long.

The frame sync is active high only for the first bit of each frame. It does not have a symmetric frame clock like in audio I2S signals.

Thanks and best regards,

Til

I can share the datasheet extract of this data format over email if needed.