My question is regarding the interpretation of the diagram on page 196 of the SPRS614A document. We are currently bringing up the first prototype of our board with a DM8168 SoC, and I am in the process of routing the DDR3 of the first major revision to the design. We designed the first prototypes as an exact copy of EVM revision E board, at least as far as the DDR3 is concerned. For the revision I am working on now, we are trying to implement a DDR3 system more suited to our needs, much more compact and with all of the traces buried. In October and November, I came up with a design using a pencil and calculator that I believe complies with all of the rules in section 8.3.2 of the SPRS614a document. It has ten layers and four x16 DDR3 memories instead of 8 x8. Each EMIF has two chips mounted in a mirror configuration, one on TOP, one on BOTTOM. As I was routing the design in our CAD package, I started to realize that Figure 8-28 is somewhat open to interpretation (to me anyway).
See the attached PDF for my attempt to represent my question in a graphical manner. It is clearly stated in Table 8-24 that A3 (the length between the stubs to the pins of the two devices) can be no more than 660 mils, and it even gives a special looser limit of 125 mils for the A3 skew in the mirrored configuration. But what is not specified (at least not in any way that I can distinguish) is whether it is allowed to have one device electrically "before" the other in some traces and electrically "after" in others. Figure 8-24 gave me the impression that it was allowed, because it is a natural consequence of the way the stubs are drawn in the diagram. In my annotation to Figure 8-28 you will find a section view that shows the two possibilities. In Case 1, the trace arrives on an inner layer from the Netra on transmission line A2 and hits a via where it splits, and the stub connects to the device on TOP (U21). The trace continues on as transmission line A3 to the next via where it splits and the stub connects to the device on BOTTOM (U22). In Case 2, everything is the same except the traces arrives to U22 BEFORE it gets to U21. My guts tell me that this is exactly what was intended in mirrored routing, but my guts have been known to be wrong. Can someone please confirm that this is correct? Is it allowed to route the stubs to the closest possible connection point, even if that means that half of the signals will reach U21 first and half will reach U22 first? Thank you.