AM67A: Three Independent Video Outputs with DSI and LVDS

Part Number: AM67A
Other Parts Discussed in Thread: AM62P, AM67

Hello,

My customer is looking to implement a three screen system using only DSI and LVDS (DPI pinout not currently available on their board).

Two questions:

1) Can there be two separate video pipelines connected to LVDS when in 2 output, 4-Lane (Single Link) mode. I see some answers here for AM62 saying no and AM62P saying yes, but nothing really on AM67A.

2) Is there a second DSI port available to generate an additional screen output thru DSI? This is a direct question from the customer. My understanding is that there is only 1 DSI port on the AM67A, but I wanted to double check before answering that question.

Best,

Ryan