AM62A7: The night scene has become incredibly dark, almost invisible

Part Number: AM62A7


Hi Experts,

With the help of a professional, I've fixed the blown-out highlights issue by configuring the registers.

However, the night scene has become incredibly dark, almost invisible. 

Is this a WDR curve issue?

Below are my WDR files and the Raw image.

files.rar 

I am using the Linux SDK 

And the program I am running is based on the imx219 modification of edge-gst-apps(My sensor is OX03C10,it's a HDR4 sensor)

I write registers in the driver file

1: I should debug the ISP while ensuring it's not overexposed, right?
2: The X coordinates of the ISP knee points, from smallest to largest, represent low light, medium light, and bright light, and the Y coordinate represents the converted light intensity, right?
3: So if I want to raise shadows, I need to raise the Y axis of the points in the low-light range, and if I want to lower highlights, I need to lower the Y axis of the points in the bright light range, right?\

Best Regards,

Meng