Part Number: TDA4VE-Q1
Other Parts Discussed in Thread: DRA829
Is there a guideline for recommend DRAM size based on the target application for TDA4VE88?
I'd like some rough numbers considering 2 scenarios:
- 4x 3MPixel @ 60fps cameras with pedestrian detection.
- 4x 3MPixel @ 60fps cameras with Surround Vision and pedestrian detection.
Also, this SoC has two DRAM buses / ranks. Is it mandatory to use both considering these applications?
Why the EVM schematics (PROC078E8C(001)_SCH) has only 1 DRAM bus?
Thank you in advance,
Rodrigo