This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Error in using kernel module linux-2.6.37-psp04.01.00.06.patch2



Hi,
I am using ezsdk_5_03_01_15 and linux-2.6.37-psp04.01.00.06.patch2 and using omx-ti81xx-src_05_02_00_30 on TI-J4 EVM(TI8148) .
 
We have kernel module in our framework which internally calls OMX. In this module I am trying allocate shared memory(0xB0000000), and facing error "Device or resource busy".
 
But If I use the same shared memory(0xB0000000) in OMX test application(iL Client), its working fine.
I found from kernel prints that allocate_resource kernel API fails. Is there any changes in this kernel release .. ?, related to resource allocation etc.
And I also observed that the same set-up i.e.  same framework module using (0xB000000) built with earlier versions of kernel viz. linux-2.6.37-psp04.01.00.05.patch1, happening successfully.
Please can  any one  provide me Info regarding changes in kernel linux-2.6.37-psp04.01.00.06.patch2.