Part Number: TDA2P-ACD
In the data sheet of TDA2Px, tc(DDR_CLK) is mentioned as 2.5ns max in table Table 7-42,which translates to a frequency of 400MHz, which means that we can run DDR3 data at maximum 800Mbps, but it supports DDR3-1333 and DDR3-1600, which have higher data rates. Also, Table 5-1 says the same. Can you please sort out this confusion.