This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SK-AM62B-P1: Ethernet problem

Part Number: SK-AM62B-P1

Hi all,

According to Daolin Qui's Questions:

  1. I am using ti-processor-sdk-linux-am62xx-evm-11.00.09.04
  2. This is on TI EVM
  3. First of all i downloaded to SDK on my vm linux, then implemented steps 1.1 to 1.4 which is described here:https://software-dl.ti.com/processor-sdk-linux/esd/AM62X/latest/exports/docs/linux/Overview/Top_Level_Makefile.html

     after completed all steps, inserted sd card inside the board, i could get to linux or u-boot window but ethernet was not functioning, then added another necessary drivers or things from menuconfig in the boot directory of sdk, build u-boot again, but still had ethernet problem.

    4.  I cannot insert whole boot log as code because it says please enter in english and then i cannot submit it. I can give that information when i ping $serverip it says:

=> ping $serverip
link up on port 1, speed 1000, full duplex
Using ethernet@8000000port@1 device
host 10.x.x.xxx is alive

but when i ping $ipaddr from computer it says destination not reachable, so i can not reach board form computer, but can reach computer from board

Thanks in advance. 

Best Regards

  • HI Sevki,

    after completed all steps, inserted sd card inside the board, i could get to linux or u-boot window but ethernet was not functioning

    Just to be clear is Ethernet not functional in U-boot or is it not functional in Linux? Your test in 4. implies you were only testing in the U-boot environment, is that correct?

    but when i ping $ipaddr from computer it says destination not reachable, so i can not reach board form computer, but can reach computer from board

    In the U-boot environment, it is expected that the EVM cannot receive any ping packets from the computer because U-boot is a stateless environment. This means that U-boot does not run any kind of network daemon that will be able to react to any packets received. Each network transaction needs the hardware to be completely initialized because U-boot cannot hold any specific state. Sending packets out from the EVM in U-boot on the other hand is possible because U-boot has full control over initializing the necessary hardware to complete the network transaction.

    Let us know if you also have problems with Ethernet in the Linux environment.

    -Daolin

  • Hi Daolin,

    Thanks. Ethernet is not functional in both Linux and u-boot. 

    Best Regards

  • Hi Sevki, 

    As I explained, the way you described Ethernet communication not working when the host PC pings the EVM while the EVM is in U-boot environment is expected.

    From the Linux environment can you share specifically what commands you are using and what the output looks like? Additionally for the boot log if you cannot insert it, feel free to direct message me on E2E with a text file of the boot log. 

    Also, please describe your test setup (i.e. no external switching between the EVM and host PC and only one port connected on the EVM to the host PC with the other port left unconnected?)

    -Daolin

  • U-Boot SPL 2025.01-gcd91d7360181-dirty (Nov 04 2025 - 14:08:20 +0100)
    SYSFW ABI: 4.0 (firmware rev 0x000b '11.0.7--v11.00.07 (Fancy Rat)')
    Changed A53 CPU frequency to 1250000000Hz (T grade) in DT
    SPL initial stack usage: 13424 bytes
    Trying to boot from MMC2
    Authentication passed
    Authentication passed
    Authentication passed
    Authentication passed
    Authentication passed
    Starting ATF on ARM64 core...
    
    NOTICE:  BL31: v2.12.0(release):11.00.08-1-gb11beb2b6-dirty
    NOTICE:  BL31: Built : 12:35:58, Mar 24 2025
    
    U-Boot SPL 2025.01-gcd91d7360181-dirty (Nov 04 2025 - 14:08:32 +0100)
    SYSFW ABI: 4.0 (firmware rev 0x000b '11.0.7--v11.00.07 (Fancy Rat)')
    SPL initial stack usage: 1952 bytes
    Trying to boot from MMC2
    Authentication passed
    Authentication passed
    
    
    U-Boot 2025.01-gcd91d7360181-dirty (Nov 04 2025 - 14:08:32 +0100)
    
    SoC:   AM62X SR1.0 HS-FS
    Model: Texas Instruments AM625 SK
    DRAM:  2 GiB
    Core:  83 devices, 32 uclasses, devicetree: separate
    MMC:   mmc@fa10000: 0, mmc@fa00000: 1
    Loading Environment from FAT... OK
    In:    serial
    Out:   serial
    Err:   serial
    Net:   eth0: ethernet@8000000port@1, eth1: ethernet@8000000port@2
    
    Hit any key to stop autoboot:  0
    switch to partitions #0, OK
    mmc1 is current device
    SD/MMC found on device 1
    574 bytes read in 4 ms (139.6 KiB/s)
    Loaded env from uEnv.txt
    Importing environment from mmc1 ...
    22256128 bytes read in 1892 ms (11.2 MiB/s)
    61630 bytes read in 6 ms (9.8 MiB/s)
    Working FDT set to 88000000
    ## Flattened Device Tree blob at 88000000
       Booting using the fdt blob at 0x88000000
    Working FDT set to 88000000
       Loading Device Tree to 000000008feed000, end 000000008fffffff ... OK
    Working FDT set to 8feed000
    
    Starting kernel ...
    
    [    0.000000] Booting Linux on physical CPU 0x0000000000 [0x410fd034]
    [    0.000000] Linux version 6.12.17-gc85877d40f8e-dirty (administrator@AM62xx-VirtualBox) (aarch64-oe-linux-gcc (GCC) 13.3.0, GNU ld (GNU Binutils) 2.42.0.20240723) #2 SMP PREEMPT Tue Nov  4 16:28:53 CET 2025
    [    0.000000] KASLR disabled due to lack of seed
    [    0.000000] Machine model: Texas Instruments AM625 SK
    [    0.000000] earlycon: ns16550a0 at MMIO32 0x0000000002800000 (options '')
    [    0.000000] printk: legacy bootconsole [ns16550a0] enabled
    [    0.000000] efi: UEFI not found.
    [    0.000000] Reserved memory: created CMA memory pool at 0x00000000f7600000, size 128 MiB
    [    0.000000] OF: reserved mem: initialized node linux,cma, compatible id shared-dma-pool
    [    0.000000] OF: reserved mem: 0x00000000f7600000..0x00000000ff5fffff (131072 KiB) map reusable linux,cma
    [    0.000000] OF: reserved mem: 0x000000009e800000..0x000000009fffffff (24576 KiB) nomap non-reusable optee@9e800000
    [    0.000000] OF: reserved mem: 0x0000000080000000..0x000000008007ffff (512 KiB) nomap non-reusable tfa@80000000
    [    0.000000] OF: reserved mem: 0x00000000ff700000..0x00000000ffffffff (9216 KiB) nomap non-reusable framebuffer@ff700000
    [    0.000000] OF: reserved mem: 0x000000009c700000..0x000000009c7fffff (1024 KiB) map non-reusable ramoops@9c700000
    [    0.000000] Reserved memory: created DMA memory pool at 0x000000009c800000, size 3 MiB
    [    0.000000] OF: reserved mem: initialized node ipc-memories@9c800000, compatible id shared-dma-pool
    [    0.000000] OF: reserved mem: 0x000000009c800000..0x000000009cafffff (3072 KiB) nomap non-reusable ipc-memories@9c800000
    [    0.000000] Reserved memory: created DMA memory pool at 0x000000009cb00000, size 1 MiB
    [    0.000000] OF: reserved mem: initialized node m4f-dma-memory@9cb00000, compatible id shared-dma-pool
    [    0.000000] OF: reserved mem: 0x000000009cb00000..0x000000009cbfffff (1024 KiB) nomap non-reusable m4f-dma-memory@9cb00000
    [    0.000000] Reserved memory: created DMA memory pool at 0x000000009cc00000, size 14 MiB
    [    0.000000] OF: reserved mem: initialized node m4f-memory@9cc00000, compatible id shared-dma-pool
    [    0.000000] OF: reserved mem: 0x000000009cc00000..0x000000009d9fffff (14336 KiB) nomap non-reusable m4f-memory@9cc00000
    [    0.000000] Reserved memory: created DMA memory pool at 0x000000009da00000, size 1 MiB
    [    0.000000] OF: reserved mem: initialized node r5f-dma-memory@9da00000, compatible id shared-dma-pool
    [    0.000000] OF: reserved mem: 0x000000009da00000..0x000000009dafffff (1024 KiB) nomap non-reusable r5f-dma-memory@9da00000
    [    0.000000] Reserved memory: created DMA memory pool at 0x000000009db00000, size 12 MiB
    [    0.000000] OF: reserved mem: initialized node r5f-memory@9db00000, compatible id shared-dma-pool
    [    0.000000] OF: reserved mem: 0x000000009db00000..0x000000009e6fffff (12288 KiB) nomap non-reusable r5f-memory@9db00000
    [    0.000000] Zone ranges:
    [    0.000000]   DMA      [mem 0x0000000080000000-0x00000000ffffffff]
    [    0.000000]   DMA32    empty
    [    0.000000]   Normal   empty
    [    0.000000] Movable zone start for each node
    [    0.000000] Early memory node ranges
    [    0.000000]   node   0: [mem 0x0000000080000000-0x000000008007ffff]
    [    0.000000]   node   0: [mem 0x0000000080080000-0x000000009c7fffff]
    [    0.000000]   node   0: [mem 0x000000009c800000-0x000000009e6fffff]
    [    0.000000]   node   0: [mem 0x000000009e700000-0x000000009e7fffff]
    [    0.000000]   node   0: [mem 0x000000009e800000-0x000000009fffffff]
    [    0.000000]   node   0: [mem 0x00000000a0000000-0x00000000ff6fffff]
    [    0.000000]   node   0: [mem 0x00000000ff700000-0x00000000ffffffff]
    [    0.000000] Initmem setup node 0 [mem 0x0000000080000000-0x00000000ffffffff]
    [    0.000000] psci: probing for conduit method from DT.
    [    0.000000] psci: PSCIv1.1 detected in firmware.
    [    0.000000] psci: Using standard PSCI v0.2 function IDs
    [    0.000000] psci: Trusted OS migration not required
    [    0.000000] psci: SMC Calling Convention v1.5
    [    0.000000] percpu: Embedded 22 pages/cpu s51672 r8192 d30248 u90112
    [    0.000000] Detected VIPT I-cache on CPU0
    [    0.000000] CPU features: detected: GIC system register CPU interface
    [    0.000000] CPU features: detected: ARM erratum 845719
    [    0.000000] alternatives: applying boot alternatives
    [    0.000000] Kernel command line: console=ttyS2,115200n8 earlycon=ns16550a,mmio32,0x02800000 mtdparts=spi-nand0:512k(ospi_nand.tiboot3),2m(ospi_nand.tispl),4m(ospi_nand.u-boot),256k(ospi_nand.env),256k(ospi_nand.env.backup),98048k@32m(ospi_nand.rootfs),256k@130816k(ospi_nand.phypattern) root=PARTUUID=358acc89-02 rw rootfstype=ext4 rootwait
    [    0.000000] Unknown kernel command line parameters "mtdparts=spi-nand0:512k(ospi_nand.tiboot3),2m(ospi_nand.tispl),4m(ospi_nand.u-boot),256k(ospi_nand.env),256k(ospi_nand.env.backup),98048k@32m(ospi_nand.rootfs),256k@130816k(ospi_nand.phypattern)", will be passed to user space.
    [    0.000000] Dentry cache hash table entries: 262144 (order: 9, 2097152 bytes, linear)
    [    0.000000] Inode-cache hash table entries: 131072 (order: 8, 1048576 bytes, linear)
    [    0.000000] Built 1 zonelists, mobility grouping on.  Total pages: 524288
    [    0.000000] mem auto-init: stack:all(zero), heap alloc:off, heap free:off
    [    0.000000] software IO TLB: SWIOTLB bounce buffer size adjusted to 2MB
    [    0.000000] software IO TLB: area num 4.
    [    0.000000] software IO TLB: mapped [mem 0x00000000f4d00000-0x00000000f4f00000] (2MB)
    [    0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=4, Nodes=1
    [    0.000000] rcu: Preemptible hierarchical RCU implementation.
    [    0.000000] rcu:     RCU event tracing is enabled.
    [    0.000000] rcu:     RCU restricting CPUs from NR_CPUS=512 to nr_cpu_ids=4.
    [    0.000000]  Trampoline variant of Tasks RCU enabled.
    [    0.000000]  Tracing variant of Tasks RCU enabled.
    [    0.000000] rcu: RCU calculated value of scheduler-enlistment delay is 25 jiffies.
    [    0.000000] rcu: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=4
    [    0.000000] RCU Tasks: Setting shift to 2 and lim to 1 rcu_task_cb_adjust=1 rcu_task_cpu_ids=4.
    [    0.000000] RCU Tasks Trace: Setting shift to 2 and lim to 1 rcu_task_cb_adjust=1 rcu_task_cpu_ids=4.
    [    0.000000] NR_IRQS: 64, nr_irqs: 64, preallocated irqs: 0
    [    0.000000] GICv3: GIC: Using split EOI/Deactivate mode
    [    0.000000] GICv3: 256 SPIs implemented
    [    0.000000] GICv3: 0 Extended SPIs implemented
    [    0.000000] Root IRQ handler: gic_handle_irq
    [    0.000000] GICv3: GICv3 features: 16 PPIs
    [    0.000000] GICv3: GICD_CTRL.DS=0, SCR_EL3.FIQ=1
    [    0.000000] GICv3: CPU0: found redistributor 0 region 0:0x0000000001880000
    [    0.000000] ITS [mem 0x01820000-0x0182ffff]
    [    0.000000] GIC: enabling workaround for ITS: Socionext Synquacer pre-ITS
    [    0.000000] ITS@0x0000000001820000: Devices Table too large, reduce ids 20->19
    [    0.000000] ITS@0x0000000001820000: allocated 524288 Devices @80c00000 (flat, esz 8, psz 64K, shr 0)
    [    0.000000] ITS: using cache flushing for cmd queue
    [    0.000000] GICv3: using LPI property table @0x0000000080450000
    [    0.000000] GIC: using cache flushing for LPI property table
    [    0.000000] GICv3: CPU0: using allocated LPI pending table @0x0000000080460000
    [    0.000000] rcu: srcu_init: Setting srcu_struct sizes based on contention.
    [    0.000000] arch_timer: cp15 timer(s) running at 200.00MHz (phys).
    [    0.000000] clocksource: arch_sys_counter: mask: 0x3ffffffffffffff max_cycles: 0x2e2049d3e8, max_idle_ns: 440795210634 ns
    [    0.000001] sched_clock: 58 bits at 200MHz, resolution 5ns, wraps every 4398046511102ns
    [    0.008755] Console: colour dummy device 80x25
    [    0.013379] Calibrating delay loop (skipped), value calculated using timer frequency.. 400.00 BogoMIPS (lpj=800000)
    [    0.024069] pid_max: default: 32768 minimum: 301
    [    0.028911] LSM: initializing lsm=capability,selinux
    [    0.034063] SELinux:  Initializing.
    [    0.038284] Mount-cache hash table entries: 4096 (order: 3, 32768 bytes, linear)
    [    0.045879] Mountpoint-cache hash table entries: 4096 (order: 3, 32768 bytes, linear)
    [    0.066479] rcu: Hierarchical SRCU implementation.
    [    0.071435] rcu:     Max phase no-delay instances is 1000.
    [    0.077041] Timer migration: 1 hierarchy levels; 8 children per group; 1 crossnode level
    [    0.085941] EFI services will not be available.
    [    0.094639] smp: Bringing up secondary CPUs ...
    [    0.107741] Detected VIPT I-cache on CPU1
    [    0.107862] GICv3: CPU1: found redistributor 1 region 0:0x00000000018a0000
    [    0.107889] GICv3: CPU1: using allocated LPI pending table @0x0000000080470000
    [    0.107952] CPU1: Booted secondary processor 0x0000000001 [0x410fd034]
    [    0.115818] Detected VIPT I-cache on CPU2
    [    0.115907] GICv3: CPU2: found redistributor 2 region 0:0x00000000018c0000
    [    0.115922] GICv3: CPU2: using allocated LPI pending table @0x0000000080480000
    [    0.115967] CPU2: Booted secondary processor 0x0000000002 [0x410fd034]
    [    0.119730] Detected VIPT I-cache on CPU3
    [    0.119810] GICv3: CPU3: found redistributor 3 region 0:0x00000000018e0000
    [    0.119832] GICv3: CPU3: using allocated LPI pending table @0x0000000080490000
    [    0.119868] CPU3: Booted secondary processor 0x0000000003 [0x410fd034]
    [    0.120015] smp: Brought up 1 node, 4 CPUs
    [    0.199770] SMP: Total of 4 processors activated.
    [    0.204586] CPU: All CPU(s) started at EL2
    [    0.208795] CPU features: detected: 32-bit EL0 Support
    [    0.214056] CPU features: detected: CRC32 instructions
    [    0.219375] alternatives: applying system-wide alternatives
    [    0.225912] Memory: 1825088K/2097152K available (12928K kernel code, 1254K rwdata, 4644K rodata, 2752K init, 639K bss, 132132K reserved, 131072K cma-reserved)
    [    0.242003] devtmpfs: initialized
    [    0.255206] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 7645041785100000 ns
    [    0.265258] futex hash table entries: 1024 (order: 4, 65536 bytes, linear)
    [    0.277512] 27152 pages in range for non-PLT usage
    [    0.277551] 518672 pages in range for PLT usage
    [    0.282981] pinctrl core: initialized pinctrl subsystem
    [    0.293662] DMI not present or invalid.
    [    0.300505] NET: Registered PF_NETLINK/PF_ROUTE protocol family
    [    0.308419] DMA: preallocated 256 KiB GFP_KERNEL pool for atomic allocations
    [    0.316512] DMA: preallocated 256 KiB GFP_KERNEL|GFP_DMA pool for atomic allocations
    [    0.325359] DMA: preallocated 256 KiB GFP_KERNEL|GFP_DMA32 pool for atomic allocations
    [    0.334164] audit: initializing netlink subsys (disabled)
    [    0.340184] audit: type=2000 audit(0.224:1): state=initialized audit_enabled=0 res=1
    [    0.340792] thermal_sys: Registered thermal governor 'step_wise'
    [    0.348131] thermal_sys: Registered thermal governor 'power_allocator'
    [    0.354339] cpuidle: using governor menu
    [    0.365274] hw-breakpoint: found 6 breakpoint and 4 watchpoint registers.
    [    0.372337] ASID allocator initialised with 65536 entries
    [    0.384376] /bus@f0000/interrupt-controller@1800000: Fixed dependency cycle(s) with /bus@f0000/interrupt-controller@1800000
    [    0.395901] /bus@f0000/i2c@20000000/tps6598x@3f/connector: Fixed dependency cycle(s) with /bus@f0000/dwc3-usb@f900000/usb@31000000
    [    0.407934] /bus@f0000/i2c@20010000/bridge-hdmi@3b: Fixed dependency cycle(s) with /bus@f0000/dss@30200000
    [    0.417873] /bus@f0000/dwc3-usb@f900000/usb@31000000: Fixed dependency cycle(s) with /bus@f0000/i2c@20000000/tps6598x@3f/connector
    [    0.429953] /bus@f0000/dss@30200000: Fixed dependency cycle(s) with /bus@f0000/i2c@20010000/bridge-hdmi@3b
    [    0.445144] /bus@f0000/i2c@20000000/tps6598x@3f/connector: Fixed dependency cycle(s) with /bus@f0000/dwc3-usb@f900000/usb@31000000
    [    0.457334] /bus@f0000/i2c@20010000/bridge-hdmi@3b: Fixed dependency cycle(s) with /bus@f0000/dss@30200000
    [    0.468175] /bus@f0000/dwc3-usb@f900000/usb@31000000: Fixed dependency cycle(s) with /bus@f0000/i2c@20000000/tps6598x@3f/connector
    [    0.481117] /bus@f0000/i2c@20010000/bridge-hdmi@3b: Fixed dependency cycle(s) with /bus@f0000/dss@30200000
    [    0.491067] /bus@f0000/dss@30200000: Fixed dependency cycle(s) with /bus@f0000/i2c@20010000/bridge-hdmi@3b
    [    0.502908] /bus@f0000/i2c@20010000/bridge-hdmi@3b: Fixed dependency cycle(s) with /connector-hdmi
    [    0.512195] /connector-hdmi: Fixed dependency cycle(s) with /bus@f0000/i2c@20010000/bridge-hdmi@3b
    [    0.523661] HugeTLB: registered 1.00 GiB page size, pre-allocated 0 pages
    [    0.530677] HugeTLB: 0 KiB vmemmap can be freed for a 1.00 GiB page
    [    0.537110] HugeTLB: registered 32.0 MiB page size, pre-allocated 0 pages
    [    0.544052] HugeTLB: 0 KiB vmemmap can be freed for a 32.0 MiB page
    [    0.550462] HugeTLB: registered 2.00 MiB page size, pre-allocated 0 pages
    [    0.557407] HugeTLB: 0 KiB vmemmap can be freed for a 2.00 MiB page
    [    0.563817] HugeTLB: registered 64.0 KiB page size, pre-allocated 0 pages
    [    0.570758] HugeTLB: 0 KiB vmemmap can be freed for a 64.0 KiB page
    [    0.579459] k3-chipinfo 43000014.chipid: Family:AM62X rev:SR1.0 JTAGID[0x0bb7e02f] Detected
    [    0.592284] iommu: Default domain type: Translated
    [    0.597214] iommu: DMA domain TLB invalidation policy: strict mode
    [    0.604183] SCSI subsystem initialized
    [    0.608575] usbcore: registered new interface driver usbfs
    [    0.614220] usbcore: registered new interface driver hub
    [    0.619684] usbcore: registered new device driver usb
    [    0.625553] pps_core: LinuxPPS API ver. 1 registered
    [    0.630645] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>
    [    0.640001] PTP clock support registered
    [    0.644058] EDAC MC: Ver: 3.0.0
    [    0.647743] scmi_core: SCMI protocol bus registered
    [    0.653113] FPGA manager framework
    [    0.656710] Advanced Linux Sound Architecture Driver Initialized.
    [    0.664085] vgaarb: loaded
    [    0.667378] clocksource: Switched to clocksource arch_sys_counter
    [    0.674023] VFS: Disk quotas dquot_6.6.0
    [    0.678078] VFS: Dquot-cache hash table entries: 512 (order 0, 4096 bytes)
    [    0.693227] NET: Registered PF_INET protocol family
    [    0.698584] IP idents hash table entries: 32768 (order: 6, 262144 bytes, linear)
    [    0.708012] tcp_listen_portaddr_hash hash table entries: 1024 (order: 2, 16384 bytes, linear)
    [    0.716852] Table-perturb hash table entries: 65536 (order: 6, 262144 bytes, linear)
    [    0.724801] TCP established hash table entries: 16384 (order: 5, 131072 bytes, linear)
    [    0.733025] TCP bind hash table entries: 16384 (order: 7, 524288 bytes, linear)
    [    0.741133] TCP: Hash tables configured (established 16384 bind 16384)
    [    0.748135] UDP hash table entries: 1024 (order: 3, 32768 bytes, linear)
    [    0.755083] UDP-Lite hash table entries: 1024 (order: 3, 32768 bytes, linear)
    [    0.762663] NET: Registered PF_UNIX/PF_LOCAL protocol family
    [    0.769185] RPC: Registered named UNIX socket transport module.
    [    0.775287] RPC: Registered udp transport module.
    [    0.780102] RPC: Registered tcp transport module.
    [    0.784913] RPC: Registered tcp-with-tls transport module.
    [    0.790529] RPC: Registered tcp NFSv4.1 backchannel transport module.
    [    0.797135] NET: Registered PF_XDP protocol family
    [    0.802065] PCI: CLS 0 bytes, default 64
    [    0.808002] Initialise system trusted keyrings
    [    0.812934] workingset: timestamp_bits=46 max_order=19 bucket_order=0
    [    0.819988] squashfs: version 4.0 (2009/01/31) Phillip Lougher
    [    0.826334] NFS: Registering the id_resolver key type
    [    0.831556] Key type id_resolver registered
    [    0.835842] Key type id_legacy registered
    [    0.839970] nfs4filelayout_init: NFSv4 File Layout Driver Registering...
    [    0.846828] nfs4flexfilelayout_init: NFSv4 Flexfile Layout Driver Registering...
    [    0.907708] Key type asymmetric registered
    [    0.911929] Asymmetric key parser 'x509' registered
    [    0.917054] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 244)
    [    0.924882] io scheduler mq-deadline registered
    [    0.929532] io scheduler kyber registered
    [    0.933679] io scheduler bfq registered
    [    0.941413] pinctrl-single 4084000.pinctrl: 34 pins, size 136
    [    0.948121] pinctrl-single f4000.pinctrl: 171 pins, size 684
    [    0.956050] ledtrig-cpu: registered to indicate activity on CPUs
    [    0.969257] Serial: 8250/16550 driver, 4 ports, IRQ sharing enabled
    [    0.986997] loop: module loaded
    [    0.991782] megasas: 07.727.03.00-rc1
    [    1.000271] tun: Universal TUN/TAP device driver, 1.6
    [    1.006781] VFIO - User Level meta-driver version: 0.3
    [    1.013387] usbcore: registered new interface driver usb-storage
    [    1.020272] i2c_dev: i2c /dev entries driver
    [    1.026636] sdhci: Secure Digital Host Controller Interface driver
    [    1.033045] sdhci: Copyright(c) Pierre Ossman
    [    1.037779] sdhci-pltfm: SDHCI platform and OF driver helper
    [    1.044310] SMCCC: SOC_ID: ARCH_SOC_ID not implemented, skipping ....
    [    1.051700] usbcore: registered new interface driver usbhid
    [    1.057412] usbhid: USB HID core driver
    [    1.062935] hw perfevents: enabled with armv8_cortex_a53 PMU driver, 7 (0,8000003f) counters available
    [    1.073291] optee: probing for conduit method.
    [    1.077905] optee: revision 4.5 (ef1ebdc23034a804)
    [    1.078387] optee: dynamic shared memory is enabled
    [    1.089245] optee: initialized driver
    [    1.089364] random: crng init done
    [    1.095902] Initializing XFRM netlink socket
    [    1.100915] NET: Registered PF_PACKET protocol family
    [    1.106196] Key type dns_resolver registered
    [    1.120257] registered taskstats version 1
    [    1.124953] Loading compiled-in X.509 certificates
    [    1.145726] ti-sci 44043000.system-controller: ABI: 4.0 (firmware rev 0x000b '11.0.7--v11.00.07 (Fancy Rat)')
    [    1.231190] /bus@f0000/i2c@20000000/tps6598x@3f/connector: Fixed dependency cycle(s) with /bus@f0000/dwc3-usb@f900000/usb@31000000
    [    1.243389] omap_i2c 20000000.i2c: bus 0 rev0.12 at 400 kHz
    [    1.250806] /connector-hdmi: Fixed dependency cycle(s) with /bus@f0000/i2c@20010000/bridge-hdmi@3b
    [    1.260108] /bus@f0000/dss@30200000: Fixed dependency cycle(s) with /bus@f0000/i2c@20010000/bridge-hdmi@3b
    [    1.270078] /bus@f0000/i2c@20010000/bridge-hdmi@3b: Fixed dependency cycle(s) with /connector-hdmi
    [    1.279312] /bus@f0000/i2c@20010000/bridge-hdmi@3b: Fixed dependency cycle(s) with /bus@f0000/dss@30200000
    [    1.289816] omap_i2c 20010000.i2c: bus 1 rev0.12 at 100 kHz
    [    1.297322] omap_i2c 20020000.i2c: bus 2 rev0.12 at 400 kHz
    [    1.303914] ti-sci-intr bus@f0000:interrupt-controller@a00000: Interrupt Router 3 domain created
    [    1.313280] ti-sci-inta 48000000.interrupt-controller: Interrupt Aggregator domain 28 created
    [    1.323698] simple-framebuffer ff700000.framebuffer: framebuffer at 0xff700000, 0x8ca000 bytes
    [    1.332553] simple-framebuffer ff700000.framebuffer: format=a8r8g8b8, mode=1920x1200x32, linelength=7680
    [    1.358127] Console: switching to colour frame buffer device 240x75
    [    1.379044] simple-framebuffer ff700000.framebuffer: fb0: simplefb registered!
    [    1.388089] ti-udma 485c0100.dma-controller: Number of rings: 82
    [    1.397306] ti-udma 485c0100.dma-controller: Channels: 48 (bchan: 18, tchan: 12, rchan: 18)
    [    1.409019] ti-udma 485c0000.dma-controller: Number of rings: 150
    [    1.420823] ti-udma 485c0000.dma-controller: Channels: 35 (tchan: 20, rchan: 15)
    [    1.431836] printk: legacy console [ttyS2] disabled
    [    1.437290] 2800000.serial: ttyS2 at MMIO 0x2800000 (irq = 238, base_baud = 3000000) is a 8250
    [    1.446215] printk: legacy console [ttyS2] enabled
    [    1.446215] printk: legacy console [ttyS2] enabled
    [    1.456038] printk: legacy bootconsole [ns16550a0] disabled
    [    1.456038] printk: legacy bootconsole [ns16550a0] disabled
    [    1.484094] 7 fixed-partitions partitions found on MTD device fc40000.spi.0
    [    1.491098] Creating 7 MTD partitions on "fc40000.spi.0":
    [    1.496520] 0x000000000000-0x000000080000 : "ospi.tiboot3"
    [    1.503778] 0x000000080000-0x000000280000 : "ospi.tispl"
    [    1.510587] 0x000000280000-0x000000680000 : "ospi.u-boot"
    [    1.517549] 0x000000680000-0x0000006c0000 : "ospi.env"
    [    1.524182] 0x0000006c0000-0x000000700000 : "ospi.env.backup"
    [    1.531247] 0x000000800000-0x000003fc0000 : "ospi.rootfs"
    [    1.538224] 0x000003fc0000-0x000004000000 : "ospi.phypattern"
    [    1.797573] davinci_mdio 8000f00.mdio: Configuring MDIO in manual mode
    [    1.839389] davinci_mdio 8000f00.mdio: davinci mdio revision 9.7, bus freq 1000000
    [    1.850320] am65-cpsw-nuss 8000000.ethernet: initializing am65 cpsw nuss version 0x6BA01103, cpsw version 0x6BA81103 Ports: 3 quirks:00000006
    [    1.863458] am65-cpsw-nuss 8000000.ethernet: initialized cpsw ale version 1.5
    [    1.870606] am65-cpsw-nuss 8000000.ethernet: ALE Table size 512, Policers 32
    [    1.878848] am65-cpsw-nuss 8000000.ethernet: CPTS ver 0x4e8a010c, freq:500000000, add_val:1 pps:1
    [    1.902646] am65-cpsw-nuss 8000000.ethernet: set new flow-id-base 19
    [    1.915204] /bus@f0000/i2c@20000000/tps6598x@3f/connector: Fixed dependency cycle(s) with /bus@f0000/dwc3-usb@f900000/usb@31000000
    [    1.927446] /bus@f0000/dwc3-usb@f900000/usb@31000000: Fixed dependency cycle(s) with /bus@f0000/i2c@20000000/tps6598x@3f/connector
    [    1.945762] xhci-hcd xhci-hcd.0.auto: xHCI Host Controller
    [    1.951336] xhci-hcd xhci-hcd.0.auto: new USB bus registered, assigned bus number 1
    [    1.959177] xhci▒
    U-Boot SPL 2025.01-gcd91d7360181-dirty (Nov 04 2025 - 14:08:20 +0100)
    SYSFW ABI: 4.0 (firmware rev 0x000b '11.0.7--v11.00.07 (Fancy Rat)')
    Changed A53 CPU frequency to 1250000000Hz (T grade) in DT
    SPL initial stack usage: 13424 bytes
    Trying to boot from MMC2
    Authentication passed
    Authentication passed
    Authentication passed
    Authentication passed
    Authentication passed
    Starting ATF on ARM64 core...
    
    NOTICE:  BL31: v2.12.0(release):11.00.08-1-gb11beb2b6-dirty
    NOTICE:  BL31: Built : 12:35:58, Mar 24 2025
    
    U-Boot SPL 2025.01-gcd91d7360181-dirty (Nov 04 2025 - 14:08:32 +0100)
    SYSFW ABI: 4.0 (firmware rev 0x000b '11.0.7--v11.00.07 (Fancy Rat)')
    SPL initial stack usage: 1952 bytes
    Trying to boot from MMC2
    Authentication passed
    Authentication passed
    
    
    U-Boot 2025.01-gcd91d7360181-dirty (Nov 04 2025 - 14:08:32 +0100)
    
    SoC:   AM62X SR1.0 HS-FS
    Model: Texas Instruments AM625 SK
    DRAM:  2 GiB
    Core:  83 devices, 32 uclasses, devicetree: separate
    MMC:   mmc@fa10000: 0, mmc@fa00000: 1
    Loading Environment from FAT... OK
    In:    serial
    Out:   serial
    Err:   serial
    Net:   eth0: ethernet@8000000port@1, eth1: ethernet@8000000port@2
    
    Hit any key to stop autoboot:  0
    switch to partitions #0, OK
    mmc1 is current device
    SD/MMC found on device 1
    574 bytes read in 3 ms (186.5 KiB/s)
    Loaded env from uEnv.txt
    Importing environment from mmc1 ...
    22256128 bytes read in 250 ms (84.9 MiB/s)
    61630 bytes read in 7 ms (8.4 MiB/s)
    Working FDT set to 88000000
    ## Flattened Device Tree blob at 88000000
       Booting using the fdt blob at 0x88000000
    Working FDT set to 88000000
       Loading Device Tree to 000000008feed000, end 000000008fffffff ... OK
    Working FDT set to 8feed000
    
    Starting kernel ...
    
    [    0.000000] Booting Linux on physical CPU 0x0000000000 [0x410fd034]
    [    0.000000] Linux version 6.12.17-gc85877d40f8e-dirty (administrator@AM62xx-VirtualBox) (aarch64-oe-linux-gcc (GCC) 13.3.0, GNU ld (GNU Binutils) 2.42.0.20240723) #2 SMP PREEMPT Tue Nov  4 16:28:53 CET 2025
    [    0.000000] KASLR disabled due to lack of seed
    [    0.000000] Machine model: Texas Instruments AM625 SK
    [    0.000000] earlycon: ns16550a0 at MMIO32 0x0000000002800000 (options '')
    [    0.000000] printk: legacy bootconsole [ns16550a0] enabled
    [    0.000000] efi: UEFI not found.
    [    0.000000] Reserved memory: created CMA memory pool at 0x00000000f7600000, size 128 MiB
    [    0.000000] OF: reserved mem: initialized node linux,cma, compatible id shared-dma-pool
    [    0.000000] OF: reserved mem: 0x00000000f7600000..0x00000000ff5fffff (131072 KiB) map reusable linux,cma
    [    0.000000] OF: reserved mem: 0x000000009e800000..0x000000009fffffff (24576 KiB) nomap non-reusable optee@9e800000
    [    0.000000] OF: reserved mem: 0x0000000080000000..0x000000008007ffff (512 KiB) nomap non-reusable tfa@80000000
    [    0.000000] OF: reserved mem: 0x00000000ff700000..0x00000000ffffffff (9216 KiB) nomap non-reusable framebuffer@ff700000
    [    0.000000] OF: reserved mem: 0x000000009c700000..0x000000009c7fffff (1024 KiB) map non-reusable ramoops@9c700000
    [    0.000000] Reserved memory: created DMA memory pool at 0x000000009c800000, size 3 MiB
    [    0.000000] OF: reserved mem: initialized node ipc-memories@9c800000, compatible id shared-dma-pool
    [    0.000000] OF: reserved mem: 0x000000009c800000..0x000000009cafffff (3072 KiB) nomap non-reusable ipc-memories@9c800000
    [    0.000000] Reserved memory: created DMA memory pool at 0x000000009cb00000, size 1 MiB
    [    0.000000] OF: reserved mem: initialized node m4f-dma-memory@9cb00000, compatible id shared-dma-pool
    [    0.000000] OF: reserved mem: 0x000000009cb00000..0x000000009cbfffff (1024 KiB) nomap non-reusable m4f-dma-memory@9cb00000
    [    0.000000] Reserved memory: created DMA memory pool at 0x000000009cc00000, size 14 MiB
    [    0.000000] OF: reserved mem: initialized node m4f-memory@9cc00000, compatible id shared-dma-pool
    [    0.000000] OF: reserved mem: 0x000000009cc00000..0x000000009d9fffff (14336 KiB) nomap non-reusable m4f-memory@9cc00000
    [    0.000000] Reserved memory: created DMA memory pool at 0x000000009da00000, size 1 MiB
    [    0.000000] OF: reserved mem: initialized node r5f-dma-memory@9da00000, compatible id shared-dma-pool
    [    0.000000] OF: reserved mem: 0x000000009da00000..0x000000009dafffff (1024 KiB) nomap non-reusable r5f-dma-memory@9da00000
    [    0.000000] Reserved memory: created DMA memory pool at 0x000000009db00000, size 12 MiB
    [    0.000000] OF: reserved mem: initialized node r5f-memory@9db00000, compatible id shared-dma-pool
    [    0.000000] OF: reserved mem: 0x000000009db00000..0x000000009e6fffff (12288 KiB) nomap non-reusable r5f-memory@9db00000
    [    0.000000] Zone ranges:
    [    0.000000]   DMA      [mem 0x0000000080000000-0x00000000ffffffff]
    [    0.000000]   DMA32    empty
    [    0.000000]   Normal   empty
    [    0.000000] Movable zone start for each node
    [    0.000000] Early memory node ranges
    [    0.000000]   node   0: [mem 0x0000000080000000-0x000000008007ffff]
    [    0.000000]   node   0: [mem 0x0000000080080000-0x000000009c7fffff]
    [    0.000000]   node   0: [mem 0x000000009c800000-0x000000009e6fffff]
    [    0.000000]   node   0: [mem 0x000000009e700000-0x000000009e7fffff]
    [    0.000000]   node   0: [mem 0x000000009e800000-0x000000009fffffff]
    [    0.000000]   node   0: [mem 0x00000000a0000000-0x00000000ff6fffff]
    [    0.000000]   node   0: [mem 0x00000000ff700000-0x00000000ffffffff]
    [    0.000000] Initmem setup node 0 [mem 0x0000000080000000-0x00000000ffffffff]
    [    0.000000] psci: probing for conduit method from DT.
    [    0.000000] psci: PSCIv1.1 detected in firmware.
    [    0.000000] psci: Using standard PSCI v0.2 function IDs
    [    0.000000] psci: Trusted OS migration not required
    [    0.000000] psci: SMC Calling Convention v1.5
    [    0.000000] percpu: Embedded 22 pages/cpu s51672 r8192 d30248 u90112
    [    0.000000] Detected VIPT I-cache on CPU0
    [    0.000000] CPU features: detected: GIC system register CPU interface
    [    0.000000] CPU features: detected: ARM erratum 845719
    [    0.000000] alternatives: applying boot alternatives
    [    0.000000] Kernel command line: console=ttyS2,115200n8 earlycon=ns16550a,mmio32,0x02800000 mtdparts=spi-nand0:512k(ospi_nand.tiboot3),2m(ospi_nand.tispl),4m(ospi_nand.u-boot),256k(ospi_nand.env),256k(ospi_nand.env.backup),98048k@32m(ospi_nand.rootfs),256k@130816k(ospi_nand.phypattern) root=PARTUUID=358acc89-02 rw rootfstype=ext4 rootwait
    [    0.000000] Unknown kernel command line parameters "mtdparts=spi-nand0:512k(ospi_nand.tiboot3),2m(ospi_nand.tispl),4m(ospi_nand.u-boot),256k(ospi_nand.env),256k(ospi_nand.env.backup),98048k@32m(ospi_nand.rootfs),256k@130816k(ospi_nand.phypattern)", will be passed to user space.
    [    0.000000] Dentry cache hash table entries: 262144 (order: 9, 2097152 bytes, linear)
    [    0.000000] Inode-cache hash table entries: 131072 (order: 8, 1048576 bytes, linear)
    [    0.000000] Built 1 zonelists, mobility grouping on.  Total pages: 524288
    [    0.000000] mem auto-init: stack:all(zero), heap alloc:off, heap free:off
    [    0.000000] software IO TLB: SWIOTLB bounce buffer size adjusted to 2MB
    [    0.000000] software IO TLB: area num 4.
    [    0.000000] software IO TLB: mapped [mem 0x00000000f4d00000-0x00000000f4f00000] (2MB)
    [    0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=4, Nodes=1
    [    0.000000] rcu: Preemptible hierarchical RCU implementation.
    [    0.000000] rcu:     RCU event tracing is enabled.
    [    0.000000] rcu:     RCU restricting CPUs from NR_CPUS=512 to nr_cpu_ids=4.
    [    0.000000]  Trampoline variant of Tasks RCU enabled.
    [    0.000000]  Tracing variant of Tasks RCU enabled.
    [    0.000000] rcu: RCU calculated value of scheduler-enlistment delay is 25 jiffies.
    [    0.000000] rcu: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=4
    [    0.000000] RCU Tasks: Setting shift to 2 and lim to 1 rcu_task_cb_adjust=1 rcu_task_cpu_ids=4.
    [    0.000000] RCU Tasks Trace: Setting shift to 2 and lim to 1 rcu_task_cb_adjust=1 rcu_task_cpu_ids=4.
    [    0.000000] NR_IRQS: 64, nr_irqs: 64, preallocated irqs: 0
    [    0.000000] GICv3: GIC: Using split EOI/Deactivate mode
    [    0.000000] GICv3: 256 SPIs implemented
    [    0.000000] GICv3: 0 Extended SPIs implemented
    [    0.000000] Root IRQ handler: gic_handle_irq
    [    0.000000] GICv3: GICv3 features: 16 PPIs
    [    0.000000] GICv3: GICD_CTRL.DS=0, SCR_EL3.FIQ=1
    [    0.000000] GICv3: CPU0: found redistributor 0 region 0:0x0000000001880000
    [    0.000000] ITS [mem 0x01820000-0x0182ffff]
    [    0.000000] GIC: enabling workaround for ITS: Socionext Synquacer pre-ITS
    [    0.000000] ITS@0x0000000001820000: Devices Table too large, reduce ids 20->19
    [    0.000000] ITS@0x0000000001820000: allocated 524288 Devices @80c00000 (flat, esz 8, psz 64K, shr 0)
    [    0.000000] ITS: using cache flushing for cmd queue
    [    0.000000] GICv3: using LPI property table @0x0000000080450000
    [    0.000000] GIC: using cache flushing for LPI property table
    [    0.000000] GICv3: CPU0: using allocated LPI pending table @0x0000000080460000
    [    0.000000] rcu: srcu_init: Setting srcu_struct sizes based on contention.
    [    0.000000] arch_timer: cp15 timer(s) running at 200.00MHz (phys).
    [    0.000000] clocksource: arch_sys_counter: mask: 0x3ffffffffffffff max_cycles: 0x2e2049d3e8, max_idle_ns: 440795210634 ns
    [    0.000001] sched_clock: 58 bits at 200MHz, resolution 5ns, wraps every 4398046511102ns
    [    0.008753] Console: colour dummy device 80x25
    [    0.013376] Calibrating delay loop (skipped), value calculated using timer frequency.. 400.00 BogoMIPS (lpj=800000)
    [    0.024063] pid_max: default: 32768 minimum: 301
    [    0.028906] LSM: initializing lsm=capability,selinux
    [    0.034050] SELinux:  Initializing.
    [    0.038276] Mount-cache hash table entries: 4096 (order: 3, 32768 bytes, linear)
    [    0.045870] Mountpoint-cache hash table entries: 4096 (order: 3, 32768 bytes, linear)
    [    0.066476] rcu: Hierarchical SRCU implementation.
    [    0.071435] rcu:     Max phase no-delay instances is 1000.
    [    0.077027] Timer migration: 1 hierarchy levels; 8 children per group; 1 crossnode level
    [    0.085950] EFI services will not be available.
    [    0.090965] smp: Bringing up secondary CPUs ...
    [    0.096399] Detected VIPT I-cache on CPU1
    [    0.096512] GICv3: CPU1: found redistributor 1 region 0:0x00000000018a0000
    [    0.096536] GICv3: CPU1: using allocated LPI pending table @0x0000000080470000
    [    0.096604] CPU1: Booted secondary processor 0x0000000001 [0x410fd034]
    [    0.097590] Detected VIPT I-cache on CPU2
    [    0.097676] GICv3: CPU2: found redistributor 2 region 0:0x00000000018c0000
    [    0.097697] GICv3: CPU2: using allocated LPI pending table @0x0000000080480000
    [    0.097738] CPU2: Booted secondary processor 0x0000000002 [0x410fd034]
    [    0.098602] Detected VIPT I-cache on CPU3
    [    0.098683] GICv3: CPU3: found redistributor 3 region 0:0x00000000018e0000
    [    0.098698] GICv3: CPU3: using allocated LPI pending table @0x0000000080490000
    [    0.098737] CPU3: Booted secondary processor 0x0000000003 [0x410fd034]
    [    0.098887] smp: Brought up 1 node, 4 CPUs
    [    0.178643] SMP: Total of 4 processors activated.
    [    0.183456] CPU: All CPU(s) started at EL2
    [    0.187669] CPU features: detected: 32-bit EL0 Support
    [    0.192940] CPU features: detected: CRC32 instructions
    [    0.198257] alternatives: applying system-wide alternatives
    [    0.204765] Memory: 1825088K/2097152K available (12928K kernel code, 1254K rwdata, 4644K rodata, 2752K init, 639K bss, 132132K reserved, 131072K cma-reserved)
    [    0.220878] devtmpfs: initialized
    [    0.234179] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 7645041785100000 ns
    [    0.244211] futex hash table entries: 1024 (order: 4, 65536 bytes, linear)
    [    0.256493] 27152 pages in range for non-PLT usage
    [    0.256532] 518672 pages in range for PLT usage
    [    0.261967] pinctrl core: initialized pinctrl subsystem
    [    0.272655] DMI not present or invalid.
    [    0.279517] NET: Registered PF_NETLINK/PF_ROUTE protocol family
    [    0.287424] DMA: preallocated 256 KiB GFP_KERNEL pool for atomic allocations
    [    0.295487] DMA: preallocated 256 KiB GFP_KERNEL|GFP_DMA pool for atomic allocations
    [    0.304361] DMA: preallocated 256 KiB GFP_KERNEL|GFP_DMA32 pool for atomic allocations
    [    0.313166] audit: initializing netlink subsys (disabled)
    [    0.319177] audit: type=2000 audit(0.200:1): state=initialized audit_enabled=0 res=1
    [    0.319778] thermal_sys: Registered thermal governor 'step_wise'
    [    0.327125] thermal_sys: Registered thermal governor 'power_allocator'
    [    0.333330] cpuidle: using governor menu
    [    0.344271] hw-breakpoint: found 6 breakpoint and 4 watchpoint registers.
    [    0.351322] ASID allocator initialised with 65536 entries
    [    0.363444] /bus@f0000/interrupt-controller@1800000: Fixed dependency cycle(s) with /bus@f0000/interrupt-controller@1800000
    [    0.374988] /bus@f0000/i2c@20000000/tps6598x@3f/connector: Fixed dependency cycle(s) with /bus@f0000/dwc3-usb@f900000/usb@31000000
    [    0.387030] /bus@f0000/i2c@20010000/bridge-hdmi@3b: Fixed dependency cycle(s) with /bus@f0000/dss@30200000
    [    0.396968] /bus@f0000/dwc3-usb@f900000/usb@31000000: Fixed dependency cycle(s) with /bus@f0000/i2c@20000000/tps6598x@3f/connector
    [    0.409047] /bus@f0000/dss@30200000: Fixed dependency cycle(s) with /bus@f0000/i2c@20010000/bridge-hdmi@3b
    [    0.424207] /bus@f0000/i2c@20000000/tps6598x@3f/connector: Fixed dependency cycle(s) with /bus@f0000/dwc3-usb@f900000/usb@31000000
    [    0.436399] /bus@f0000/i2c@20010000/bridge-hdmi@3b: Fixed dependency cycle(s) with /bus@f0000/dss@30200000
    [    0.447253] /bus@f0000/dwc3-usb@f900000/usb@31000000: Fixed dependency cycle(s) with /bus@f0000/i2c@20000000/tps6598x@3f/connector
    [    0.460178] /bus@f0000/i2c@20010000/bridge-hdmi@3b: Fixed dependency cycle(s) with /bus@f0000/dss@30200000
    [    0.470128] /bus@f0000/dss@30200000: Fixed dependency cycle(s) with /bus@f0000/i2c@20010000/bridge-hdmi@3b
    [    0.481989] /bus@f0000/i2c@20010000/bridge-hdmi@3b: Fixed dependency cycle(s) with /connector-hdmi
    [    0.491257] /connector-hdmi: Fixed dependency cycle(s) with /bus@f0000/i2c@20010000/bridge-hdmi@3b
    [    0.502686] HugeTLB: registered 1.00 GiB page size, pre-allocated 0 pages
    [    0.509680] HugeTLB: 0 KiB vmemmap can be freed for a 1.00 GiB page
    [    0.516110] HugeTLB: registered 32.0 MiB page size, pre-allocated 0 pages
    [    0.523052] HugeTLB: 0 KiB vmemmap can be freed for a 32.0 MiB page
    [    0.529467] HugeTLB: registered 2.00 MiB page size, pre-allocated 0 pages
    [    0.536408] HugeTLB: 0 KiB vmemmap can be freed for a 2.00 MiB page
    [    0.542819] HugeTLB: registered 64.0 KiB page size, pre-allocated 0 pages
    [    0.549760] HugeTLB: 0 KiB vmemmap can be freed for a 64.0 KiB page
    [    0.558483] k3-chipinfo 43000014.chipid: Family:AM62X rev:SR1.0 JTAGID[0x0bb7e02f] Detected
    [    0.568058] iommu: Default domain type: Translated
    [    0.573003] iommu: DMA domain TLB invalidation policy: strict mode
    [    0.580016] SCSI subsystem initialized
    [    0.584418] usbcore: registered new interface driver usbfs
    [    0.590076] usbcore: registered new interface driver hub
    [    0.595548] usbcore: registered new device driver usb
    [    0.601405] pps_core: LinuxPPS API ver. 1 registered
    [    0.606490] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>
    [    0.615850] PTP clock support registered
    [    0.619900] EDAC MC: Ver: 3.0.0
    [    0.623591] scmi_core: SCMI protocol bus registered
    [    0.628968] FPGA manager framework
    [    0.632561] Advanced Linux Sound Architecture Driver Initialized.
    [    0.639972] vgaarb: loaded
    [    0.643273] clocksource: Switched to clocksource arch_sys_counter
    [    0.649939] VFS: Disk quotas dquot_6.6.0
    [    0.653996] VFS: Dquot-cache hash table entries: 512 (order 0, 4096 bytes)
    [    0.669036] NET: Registered PF_INET protocol family
    [    0.674394] IP idents hash table entries: 32768 (order: 6, 262144 bytes, linear)
    [    0.683809] tcp_listen_portaddr_hash hash table entries: 1024 (order: 2, 16384 bytes, linear)
    [    0.692638] Table-perturb hash table entries: 65536 (order: 6, 262144 bytes, linear)
    [    0.700585] TCP established hash table entries: 16384 (order: 5, 131072 bytes, linear)
    [    0.708809] TCP bind hash table entries: 16384 (order: 7, 524288 bytes, linear)
    [    0.716918] TCP: Hash tables configured (established 16384 bind 16384)
    [    0.723920] UDP hash table entries: 1024 (order: 3, 32768 bytes, linear)
    [    0.730857] UDP-Lite hash table entries: 1024 (order: 3, 32768 bytes, linear)
    [    0.738436] NET: Registered PF_UNIX/PF_LOCAL protocol family
    [    0.744960] RPC: Registered named UNIX socket transport module.
    [    0.751052] RPC: Registered udp transport module.
    [    0.755865] RPC: Registered tcp transport module.
    [    0.760685] RPC: Registered tcp-with-tls transport module.
    [    0.766297] RPC: Registered tcp NFSv4.1 backchannel transport module.
    [    0.772891] NET: Registered PF_XDP protocol family
    [    0.777821] PCI: CLS 0 bytes, default 64
    [    0.783867] Initialise system trusted keyrings
    [    0.788806] workingset: timestamp_bits=46 max_order=19 bucket_order=0
    [    0.795860] squashfs: version 4.0 (2009/01/31) Phillip Lougher
    [    0.802148] NFS: Registering the id_resolver key type
    [    0.807365] Key type id_resolver registered
    [    0.811646] Key type id_legacy registered
    [    0.815771] nfs4filelayout_init: NFSv4 File Layout Driver Registering...
    [    0.822641] nfs4flexfilelayout_init: NFSv4 Flexfile Layout Driver Registering...
    [    0.883564] Key type asymmetric registered
    [    0.887778] Asymmetric key parser 'x509' registered
    [    0.892898] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 244)
    [    0.900727] io scheduler mq-deadline registered
    [    0.905373] io scheduler kyber registered
    [    0.909524] io scheduler bfq registered
    [    0.917256] pinctrl-single 4084000.pinctrl: 34 pins, size 136
    [    0.923968] pinctrl-single f4000.pinctrl: 171 pins, size 684
    [    0.931868] ledtrig-cpu: registered to indicate activity on CPUs
    [    0.945074] Serial: 8250/16550 driver, 4 ports, IRQ sharing enabled
    [    0.962842] loop: module loaded
    [    0.967673] megasas: 07.727.03.00-rc1
    [    0.976179] tun: Universal TUN/TAP device driver, 1.6
    [    0.982701] VFIO - User Level meta-driver version: 0.3
    [    0.989275] usbcore: registered new interface driver usb-storage
    [    0.996124] i2c_dev: i2c /dev entries driver
    [    1.002485] sdhci: Secure Digital Host Controller Interface driver
    [    1.008888] sdhci: Copyright(c) Pierre Ossman
    [    1.013609] sdhci-pltfm: SDHCI platform and OF driver helper
    [    1.020106] SMCCC: SOC_ID: ARCH_SOC_ID not implemented, skipping ....
    [    1.027492] usbcore: registered new interface driver usbhid
    [    1.033220] usbhid: USB HID core driver
    [    1.038757] hw perfevents: enabled with armv8_cortex_a53 PMU driver, 7 (0,8000003f) counters available
    [    1.049129] optee: probing for conduit method.
    [    1.053744] optee: revision 4.5 (ef1ebdc23034a804)
    [    1.054225] optee: dynamic shared memory is enabled
    [    1.065106] optee: initialized driver
    [    1.065215] random: crng init done
    [    1.071538] Initializing XFRM netlink socket
    [    1.076766] NET: Registered PF_PACKET protocol family
    [    1.082055] Key type dns_resolver registered
    [    1.096147] registered taskstats version 1
    [    1.100833] Loading compiled-in X.509 certificates
    [    1.120001] ti-sci 44043000.system-controller: ABI: 4.0 (firmware rev 0x000b '11.0.7--v11.00.07 (Fancy Rat)')
    [    1.204785] /bus@f0000/i2c@20000000/tps6598x@3f/connector: Fixed dependency cycle(s) with /bus@f0000/dwc3-usb@f900000/usb@31000000
    [    1.216973] omap_i2c 20000000.i2c: bus 0 rev0.12 at 400 kHz
    [    1.224929] /connector-hdmi: Fixed dependency cycle(s) with /bus@f0000/i2c@20010000/bridge-hdmi@3b
    [    1.234258] /bus@f0000/dss@30200000: Fixed dependency cycle(s) with /bus@f0000/i2c@20010000/bridge-hdmi@3b
    [    1.244239] /bus@f0000/i2c@20010000/bridge-hdmi@3b: Fixed dependency cycle(s) with /connector-hdmi
    [    1.253476] /bus@f0000/i2c@20010000/bridge-hdmi@3b: Fixed dependency cycle(s) with /bus@f0000/dss@30200000
    [    1.263949] omap_i2c 20010000.i2c: bus 1 rev0.12 at 100 kHz
    [    1.271487] omap_i2c 20020000.i2c: bus 2 rev0.12 at 400 kHz
    [    1.277539] ti-sci-intr bus@f0000:interrupt-controller@a00000: Interrupt Router 3 domain created
    [    1.286862] ti-sci-inta 48000000.interrupt-controller: Interrupt Aggregator domain 28 created
    [    1.297397] simple-framebuffer ff700000.framebuffer: framebuffer at 0xff700000, 0x8ca000 bytes
    [    1.306295] simple-framebuffer ff700000.framebuffer: format=a8r8g8b8, mode=1920x1200x32, linelength=7680
    [    1.331932] Console: switching to colour frame buffer device 240x75
    [    1.352854] simple-framebuffer ff700000.framebuffer: fb0: simplefb registered!
    [    1.361776] ti-udma 485c0100.dma-controller: Number of rings: 82
    [    1.371017] ti-udma 485c0100.dma-controller: Channels: 48 (bchan: 18, tchan: 12, rchan: 18)
    [    1.382662] ti-udma 485c0000.dma-controller: Number of rings: 150
    [    1.394444] ti-udma 485c0000.dma-controller: Channels: 35 (tchan: 20, rchan: 15)
    [    1.405445] printk: legacy console [ttyS2] disabled
    [    1.410905] 2800000.serial: ttyS2 at MMIO 0x2800000 (irq = 238, base_baud = 3000000) is a 8250
    [    1.419902] printk: legacy console [ttyS2] enabled
    [    1.419902] printk: legacy console [ttyS2] enabled
    [    1.429602] printk: legacy bootconsole [ns16550a0] disabled
    [    1.429602] printk: legacy bootconsole [ns16550a0] disabled
    [    1.448090] 7 fixed-partitions partitions found on MTD device fc40000.spi.0
    [    1.455102] Creating 7 MTD partitions on "fc40000.spi.0":
    [    1.460505] 0x000000000000-0x000000080000 : "ospi.tiboot3"
    [    1.467802] 0x000000080000-0x000000280000 : "ospi.tispl"
    [    1.474660] 0x000000280000-0x000000680000 : "ospi.u-boot"
    [    1.481542] 0x000000680000-0x0000006c0000 : "ospi.env"
    [    1.488114] 0x0000006c0000-0x000000700000 : "ospi.env.backup"
    [    1.495399] 0x000000800000-0x000003fc0000 : "ospi.rootfs"
    [    1.502373] 0x000003fc0000-0x000004000000 : "ospi.phypattern"
    [    1.763135] davinci_mdio 8000f00.mdio: Configuring MDIO in manual mode
    [    1.803286] davinci_mdio 8000f00.mdio: davinci mdio revision 9.7, bus freq 1000000
    [    1.814272] am65-cpsw-nuss 8000000.ethernet: initializing am65 cpsw nuss version 0x6BA01103, cpsw version 0x6BA81103 Ports: 3 quirks:00000006
    [    1.827408] am65-cpsw-nuss 8000000.ethernet: initialized cpsw ale version 1.5
    [    1.834556] am65-cpsw-nuss 8000000.ethernet: ALE Table size 512, Policers 32
    [    1.842812] am65-cpsw-nuss 8000000.ethernet: CPTS ver 0x4e8a010c, freq:500000000, add_val:1 pps:1
    [    1.865469] am65-cpsw-nuss 8000000.ethernet: set new flow-id-base 19
    [    1.877782] /bus@f0000/i2c@20000000/tps6598x@3f/connector: Fixed dependency cycle(s) with /bus@f0000/dwc3-usb@f900000/usb@31000000
    [    1.889770] /bus@f0000/dwc3-usb@f900000/usb@31000000: Fixed dependency cycle(s) with /bus@f0000/i2c@20000000/tps6598x@3f/connector
    [    1.907497] xhci-hcd xhci-hcd.0.auto: xHCI Host Controller
    [    1.913096] xhci-hcd xhci-hcd.0.auto: new USB bus registered, assigned bus number 1
    [    1.920938] xhci-hcd xhci-hcd.0.auto: USB3 root hub has no ports
    [    1.926943] xhci-hcd xhci-hcd.0.auto: hcc params 0x0258fe6d hci version 0x110 quirks 0x0000808020000010
    [    1.936424] xhci-hcd xhci-hcd.0.auto: irq 253, io mem 0x31100000
    [    1.943592] hub 1-0:1.0: USB hub found
    [    1.947393] hub 1-0:1.0: 1 port detected
    [    1.955945] mmc0: CQHCI version 5.10
    [    1.963180] pca953x 1-0022: supply vcc not found, using dummy regulator
    [    1.970630] pca953x 1-0022: using AI
    [    1.995908] mmc0: SDHCI controller on fa10000.mmc [fa10000.mmc] using ADMA 64-bit
    [    2.004195] davinci_mdio 8000f00.mdio: Configuring MDIO in manual mode
    [    2.043280] davinci_mdio 8000f00.mdio: davinci mdio revision 9.7, bus freq 1000000
    [    2.056796] davinci_mdio 8000f00.mdio: phy[0]: device 8000f00.mdio:00, driver TI DP83867
    [    2.065021] davinci_mdio 8000f00.mdio: phy[1]: device 8000f00.mdio:01, driver TI DP83867
    [    2.075894] clk: Disabling unused clocks
    [    2.088857] mmc0: Command Queue Engine enabled
    [    2.089371] PM: genpd: Disabling unused power domains
    [    2.090264] mmc1: CQHCI version 5.10
    [    2.093391] mmc0: new HS200 MMC card at address 0001
    [    2.098773] ALSA device list:
    [    2.106873] mmcblk0: mmc0:0001 G1M15L 29.6 GiB
    [    2.107116]   No soundcards found.
    [    2.112056]  mmcblk0: p1 p2
    [    2.121539] mmcblk0boot0: mmc0:0001 G1M15L 31.5 MiB
    [    2.128038] mmcblk0boot1: mmc0:0001 G1M15L 31.5 MiB
    [    2.134273] mmcblk0rpmb: mmc0:0001 G1M15L 4.00 MiB, chardev (239:0)
    [    2.139331] mmc1: SDHCI controller on fa00000.mmc [fa00000.mmc] using ADMA 64-bit
    [    2.148437] Waiting for root device PARTUUID=358acc89-02...
    [    2.204269] mmc1: new ultra high speed SDR104 SDHC card at address 59b4
    [    2.211918] mmcblk1: mmc1:59b4 USDU1 14.9 GiB
    [    2.218986]  mmcblk1: p1 p2
    [    3.642010] EXT4-fs (mmcblk1p2): recovery complete
    [    3.648973] EXT4-fs (mmcblk1p2): mounted filesystem c6a68527-5e9d-48da-a29f-8135709202a8 r/w with ordered data mode. Quota mode: none.
    [    3.661182] VFS: Mounted root (ext4 filesystem) on device 179:98.
    [    3.671149] devtmpfs: mounted
    [    3.676253] Freeing unused kernel memory: 2752K
    [    3.680915] Run /sbin/init as init process
    [    3.986949] systemd[1]: System time before build time, advancing clock.
    [    4.046381] NET: Registered PF_INET6 protocol family
    [    4.052932] Segment Routing with IPv6
    [    4.056742] In-situ OAM (IOAM) with IPv6
    [    4.104961] systemd[1]: systemd 255.17^ running in system mode (+PAM -AUDIT -SELINUX -APPARMOR +IMA -SMACK +SECCOMP -GCRYPT -GNUTLS -OPENSSL +ACL +BLKID -CURL -ELFUTILS -FIDO2 -IDN2 -IDN -IPTC +KMOD -LIBCRYPTSETUP +LIBFDISK -PCRE2 -PWQUALITY -P11KIT -QRENCODE -TPM2 -BZIP2 -LZ4 -XZ -ZLIB +ZSTD -BPF_FRAMEWORK -XKBCOMMON +UTMP +SYSVINIT default-hierarchy=unified)
    [    4.136943] systemd[1]: Detected architecture arm64.
    
    Welcome to Arago 2025.01!
    
    [    4.155172] systemd[1]: Hostname set to <am62xx-evm>.
    [    4.440088] systemd[1]: Configuration file /usr/lib/systemd/system/ti-apps-launcher.service is marked executable. Please remove executable permission bits. Proceeding anyway.
    [    4.491574] systemd[1]: Configuration file /usr/lib/systemd/system/seva-launcher.service is marked executable. Please remove executable permission bits. Proceeding anyway.
    [    4.589989] systemd[1]: /usr/lib/systemd/system/bt-enable.service:9: Standard output type syslog is obsolete, automatically updating to journal. Please update your unit file, and consider removing the setting altogether.
    [    4.785740] systemd[1]: Queued start job for default target Graphical Interface.
    [    4.830873] systemd[1]: Created slice Slice /system/getty.
    [  OK  ] Created slice Slice /system/getty.
    [    4.850776] systemd[1]: Created slice Slice /system/modprobe.
    [  OK  ] Created slice Slice /system/modprobe.
    [    4.874501] systemd[1]: Created slice Slice /system/serial-getty.
    [  OK  ] Created slice Slice /system/serial-getty.
    [    4.893617] systemd[1]: Created slice User and Session Slice.
    [  OK  ] Created slice User and Session Slice.
    [    4.911955] systemd[1]: Started Dispatch Password Requests to Console Directory Watch.
    [  OK  ] Started Dispatch Password Requests to Console Directory Watch.
    [    4.931800] systemd[1]: Started Forward Password Requests to Wall Directory Watch.
    [  OK  ] Started Forward Password Requests to Wall Directory Watch.
    [    4.951564] systemd[1]: Expecting device /dev/ttyS2...
             Expecting device /dev/ttyS2...
    [    4.967620] systemd[1]: Reached target Path Units.
    [  OK  ] Reached target Path Units.
    [    4.983465] systemd[1]: Reached target Remote File Systems.
    [  OK  ] Reached target Remote File Systems.
    [    4.999441] systemd[1]: Reached target Slice Units.
    [  OK  ] Reached target Slice Units.
    [    5.015462] systemd[1]: Reached target Swaps.
    [  OK  ] Reached target Swaps.
    [    5.090090] systemd[1]: Listening on RPCbind Server Activation Socket.
    [  OK  ] Listening on RPCbind Server Activation Socket.
    [    5.107715] systemd[1]: Reached target RPC Port Mapper.
    [  OK  ] Reached target RPC Port Mapper.
    [    5.132492] systemd[1]: Listening on Process Core Dump Socket.
    [  OK  ] Listening on Process Core Dump Socket.
    [    5.152133] systemd[1]: Listening on initctl Compatibility Named Pipe.
    [  OK  ] Listening on initctl Compatibility Named Pipe.
    [    5.173259] systemd[1]: Listening on Journal Audit Socket.
    [  OK  ] Listening on Journal Audit Socket.
    [    5.192537] systemd[1]: Listening on Journal Socket (/dev/log).
    [  OK  ] Listening on Journal Socket (/dev/log).
    [    5.212570] systemd[1]: Listening on Journal Socket.
    [  OK  ] Listening on Journal Socket.
    [    5.232665] systemd[1]: Listening on Network Service Netlink Socket.
    [  OK  ] Listening on Network Service Netlink Socket.
    [    5.254263] systemd[1]: Listening on udev Control Socket.
    [  OK  ] Listening on udev Control Socket.
    [    5.272385] systemd[1]: Listening on udev Kernel Socket.
    [  OK  ] Listening on udev Kernel Socket.
    [    5.292414] systemd[1]: Listening on User Database Manager Socket.
    [  OK  ] Listening on User Database Manager Socket.
    [    5.347885] systemd[1]: Mounting Huge Pages File System...
             Mounting Huge Pages File System...
    [    5.370449] systemd[1]: Mounting POSIX Message Queue File System...
             Mounting POSIX Message Queue File System...
    [    5.394145] systemd[1]: Mounting Kernel Debug File System...
             Mounting Kernel Debug File System...
    [    5.412398] systemd[1]: Kernel Trace File System was skipped because of an unmet condition check (ConditionPathExists=/sys/kernel/tracing).
    [    5.433272] systemd[1]: Mounting Temporary Directory /tmp...
             Mounting Temporary Directory /tmp...
    [    5.460330] systemd[1]: Starting Create List of Static Device Nodes...
             Starting Create List of Static Device Nodes...
    [    5.486626] systemd[1]: Starting Load Kernel Module configfs...
             Starting Load Kernel Module configfs...
    [    5.510798] systemd[1]: Starting Load Kernel Module drm...
             Starting Load Kernel Module drm...
    [    5.534969] systemd[1]: Starting Load Kernel Module fuse...
             Starting Load Kernel Module fuse...
    [    5.561168] systemd[1]: Starting Start psplash boot splash screen...
             Starting Start psplash boot splash screen...
    [    5.592127] systemd[1]: Starting RPC Bind...
             Starting RPC Bind...
    [    5.604231] systemd[1]: File System Check on Root Device was skipped because of an unmet condition check (ConditionPathIsReadWrite=!/).
    [    5.604795] fuse: init (API version 7.41)
    [    5.629391] systemd[1]: Starting Journal Service...
             Starting Journal Service...
    [    5.661180] systemd[1]: Starting Load Kernel Modules...
             Starting Load Kernel Modules...
    [    5.692300] systemd[1]: Starting Generate network units from Kernel command line...
             Starting Generate network units from Kernel command line...
    [    5.751801] systemd[1]: Starting Remount Root and Kernel File Systems...
             Starting Remount Root and Kernel File Systems...
    [    5.772370] systemd-journald[133]: Collecting audit messages is enabled.
    [    5.784837] systemd[1]: Starting Coldplug All udev Devices...
             Starting Coldplug All udev Devices...
    [    5.826015] systemd[1]: Started Start psplash boot splash screen.
    [    5.832049] EXT4-fs (mmcblk1p2): re-mounted c6a68527-5e9d-48da-a29f-8135709202a8 r/w. Quota mode: none.
    [  OK  ] Started Start psplash boot splash screen.
    [    5.858765] systemd[1]: Started RPC Bind.
    [  OK  ] Started RPC Bind.
    [    5.872373] systemd[1]: Started Journal Service.
    [  OK  ] Started Journal Service.
    [  OK  ] Mounted Huge Pages File System.
    [  OK  ] Mounted POSIX Message Queue File System.
    [  OK  ] Mounted Kernel Debug File System.
    [  OK  ] Mounted Temporary Directory /tmp.
    [  OK  ] Finished Create List of Static Device Nodes.
    [  OK  ] Finished Load Kernel Module configfs.
    [  OK  ] Finished Load Kernel Module drm.
    [  OK  ] Finished Load Kernel Module fuse.
    [  OK  ] Finished Load Kernel Modules.
    [  OK  ] Finished Generate network units from Kernel command line.
    [  OK  ] Finished Remount Root and Kernel File Systems.
             Mounting FUSE Control File System...
             Mounting Kernel Configuration File System...
    [  OK  ] Started Start psplash-systemd progress communication helper.
             Starting Flush Journal to Persistent Storage...
             Starting Apply Kernel Variables...
             Starting Create Static Device Nodes in /dev gracefully...
    [  OK  ] Mounted FUSE Control File System.
    [    6.303882] systemd-journald[133]: Received client request to flush runtime journal.
    [  OK  ] Mounted Kernel Configuration File System.
    [  OK  ] Finished Flush Journal to Persistent Storage.
    [  OK  ] Finished Apply Kernel Variables.
    [  OK  ] Finished Create Static Device Nodes in /dev gracefully.
             Starting Create Static Device Nodes in /dev...
    [  OK  ] Finished Create Static Device Nodes in /dev.
    [  OK  ] Reached target Preparation for Local File Systems.
             Mounting /var/volatile...
    [    6.604065] audit: type=1334 audit(1736360579.616:2): prog-id=6 op=LOAD
    [    6.610802] audit: type=1334 audit(1736360579.620:3): prog-id=7 op=LOAD
             Starting Rule-based Manager for Device Events and Files...
    [  OK  ] Finished Coldplug All udev Devices.
    [  OK  ] Mounted /var/volatile.
             Starting Load/Save OS Random Seed...
    [  OK  ] Reached target Local File Systems.
             Starting Create System Files and Directories...
    [  OK  ] Finished Load/Save OS Random Seed.
    [  OK  ] Finished Create System Files and Directories.
    [    6.883884] audit: type=1334 audit(1736360579.896:4): prog-id=8 op=LOAD
             Starting Network Name Resolution...
    [    6.932903] audit: type=1334 audit(1736360579.944:5): prog-id=9 op=LOAD
             Starting Network Time Synchronization...
             Starting Record System Boot/Shutdown in UTMP...
    [    6.981493] audit: type=1334 audit(1736360579.992:6): prog-id=10 op=LOAD
    [    6.988408] audit: type=1334 audit(1736360580.000:7): prog-id=11 op=LOAD
    [    6.995200] audit: type=1334 audit(1736360580.004:8): prog-id=12 op=LOAD
             Starting User Database Manager...
    [  OK  ] Finished Record System Boot/Shutdown in UTMP.
    [  OK  ] Started User Database Manager.
    [  OK  ] Started Rule-based Manager for Device Events and Files.
    [  OK  ] Found device /dev/ttyS2.
    [  OK  ] Started Network Time Synchronization.
    [  OK  ] Reached target System Time Set.
    [  OK  ] Started Network Name Resolution.
    [  OK  ] Reached target Host and Network Name Lookups.
    [  OK  ] Reached target System Initialization.
    [  OK  ] Started Daily rotation of log files.
    [  OK  ] Started Daily Cleanup of Temporary Directories.
    [  OK  ] Reached target Timer Units.
    [  OK  ] Listening on Avahi mDNS/DNS-SD Stack Activation Socket.
    [  OK  ] Listening on D-Bus System Message Bus Socket.
             Starting Docker Socket for the API...
    [  OK  ] Listening on dropbear.socket.
    [  OK  ] Listening on PC/SC Smart Card Daemon Activation Socket.
    [    7.867467] audit: type=1334 audit(1736834477.204:9): prog-id=13 op=LOAD
             Starting D-Bus System Message Bus...
             Starting Reboot and dump vmcore via kexec...
    [  OK  ] Listening on Docker Socket for the API.
    [  OK  ] Reached target Socket Units.
    [  OK  ] Finished Reboot and dump vmcore via kexec.
    [  OK  ] Started D-Bus System Message Bus.
    [  OK  ] Reached target Basic System.
    [  OK  ] Started Job spooling tools.
             Starting Avahi mDNS/DNS-SD Stack...
    [  OK  ] Started Periodic Command Scheduler.
             Starting Print notice about GPLv3 packages...
             Starting IPv6 Packet Filtering Framework...
             Starting IPv4 Packet Filtering Framework...
    [  OK  ] Started irqbalance daemon.
    [  OK  ] Started Multiple Spanning Tree Protocol Daemon.
             Starting Telephony service...
             Starting PulseAudio Sound System...
             Starting Expand the rootfs partiti…to full size of the boot device....
    [  OK  ] Started Seva Launcher Service.
    [  OK  ] Started strongSwan IPsec IKEv1/IKEv2 daemon using ipsec.conf.
    [    8.770530] audit: type=1334 audit(1736834478.108:10): prog-id=14 op=LOAD
    [    8.779480] audit: type=1334 audit(1736834478.116:11): prog-id=15 op=LOAD
             Starting User Login Management...
             Starting Telnet Server...
    [  OK  ] Finished IPv6 Packet Filtering Framework.
    [  OK  ] Finished IPv4 Packet Filtering Framework.
    [  OK  ] Finished Telnet Server.
    [  OK  ] Reached target Preparation for Network.
             Starting Network Configuration...
    [  OK  ] Started Telephony service.
    [  OK  ] Started Avahi mDNS/DNS-SD Stack.
    [    9.462661] Bluetooth: Core ver 2.22
    [    9.466787] NET: Registered PF_BLUETOOTH protocol family
    [    9.475374] Bluetooth: HCI device and connection manager initialized
    [    9.482475] Bluetooth: HCI socket layer initialized
    [    9.489381] Bluetooth: L2CAP socket layer initialized
    [    9.503464] Bluetooth: SCO socket layer initialized
    [  OK  ] Started User Login Management.
    [    9.636499] omap-mailbox 29000000.mailbox: omap mailbox rev 0x66fc9100
    [    9.653941] at24 0-0051: supply vcc not found, using dummy regulator
    [    9.686723] at24 0-0051: 65536 byte 24c512 EEPROM, writable, 1 bytes/write
    [    9.766644] cfg80211: Loading compiled-in X.509 certificates for regulatory database
    [    9.804659] tps6598x 0-003f: Unable to find the interrupt, switching to polling
    [    9.821786] pstore: Using crash dump compression: deflate
    [    9.827668] pstore: Registered ramoops as persistent store backend
    [    9.831238] Loaded X.509 cert 'sforshee: 00b28ddf47aef9cea7'
    [    9.834819] ramoops: using 0x100000@0x9c700000, ecc: 0
    [    9.840409] Loaded X.509 cert 'wens: 61c038651aabdcf94bd0ac7ff06c7248db18c600'
    [    9.872708] rtc-ti-k3 2b1f0000.rtc: registered as rtc0
    [    9.880727] k3-m4-rproc 5000000.m4fss: assigned reserved memory node m4f-dma-memory@9cb00000
    [    9.897914] k3-m4-rproc 5000000.m4fss: configured M4F for remoteproc mode
    [    9.910258] remoteproc remoteproc0: 5000000.m4fss is available
    [    9.952290] platform 78000000.r5f: R5F core may have been powered on by a different host, programmed state (0) != actual state (1)
    [    9.968813] platform 78000000.r5f: configured R5F for IPC-only mode
    [  OK  ] Finished Expand the rootfs partitio[    9.980300] remoteproc remoteproc0: powering up 5000000.m4fss
    n to full size of the boot device..
    [    9.992714] remoteproc remoteproc0: Booting fw image am62-mcu-m4f0_0-fw, size 55100
    [   10.008832] rproc-virtio rproc-virtio.2.auto: assigned reserved memory node m4f-dma-memory@9cb00000
    [   10.023849] platform 78000000.r5f: assigned reserved memory node r5f-dma-memory@9da00000
    [   10.062735] remoteproc remoteproc1: 78000000.r5f is available
    [   10.069705] remoteproc remoteproc1: attaching to 78000000.r5f
    [   10.098697] virtio_rpmsg_bus virtio0: rpmsg host is online
    [   10.099454] virtio_rpmsg_bus virtio0: creating channel ti.ipc4.ping-pong addr 0xd
    [   10.113437] rproc-virtio rproc-virtio.3.auto: assigned reserved memory node r5f-dma-memory@9da00000
    [   10.114083] rproc-virtio rproc-virtio.2.auto: registered virtio0 (type 7)
    [   10.129500] remoteproc remoteproc0: remote processor 5000000.m4fss is now up
    [  OK  ] Started Network Configuration.
    [  OK  ] Reached target Network.
    [   10.173708] virtio_rpmsg_bus virtio0: creating channel rpmsg_chrdev addr 0xe
    [   10.194574] am65-cpsw-nuss 8000000.ethernet eth0: PHY [8000f00.mdio:00] driver [TI DP83867] (irq=POLL)
    [   10.209444] am65-cpsw-nuss 8000000.ethernet eth0: configuring for phy/rgmii-rxid link mode
             Starting Enable and configure wl18xx bluetooth stack...
             Starting containerd container runtime...
    [   10.323585] virtio_rpmsg_bus virtio1: rpmsg host is online
    [   10.324291] virtio_rpmsg_bus virtio1: creating channel ti.ipc4.ping-pong addr 0xd
    [   10.335810] rproc-virtio rproc-virtio.3.auto: registered virtio1 (type 7)
    [   10.343716] virtio_rpmsg_bus virtio1: creating channel rpmsg_chrdev addr 0xe
    [   10.347826] remoteproc remoteproc1: remote processor 78000000.r5f is now attached
    [   10.350385] am65-cpsw-nuss 8000000.ethernet eth1: PHY [8000f00.mdio:01] driver [TI DP83867] (irq=POLL)
    [   10.350415] am65-cpsw-nuss 8000000.ethernet eth1: configuring for phy/rgmii-rxid link mode
             Starting LLDP daemon...
    [  OK  ] Started Netperf Benchmark Server.
    [   10.429127] sii902x 1-003b: supply iovcc not found, using dummy regulator
    [   10.439849] sii902x 1-003b: supply cvcc12 not found, using dummy regulator
             Starting Simple Network Management Protocol (SNMP) Daemon....
    [   10.462006] i2c i2c-1: Added multiplexed i2c bus 3
             Starting Permit User Sessions...
    [   10.499597] [drm] Initialized tidss 1.0.0 for 30200000.dss on minor 0
    [   10.511401] tidss 30200000.dss: [drm] Cannot find any crtc or sizes
    [   10.520237] tidss 30200000.dss: [drm] Cannot find any crtc or sizes
    [  OK  ] Finished Enable and configure wl18xx bluetooth stack.
    [  OK  ] Started PulseAudio Sound System.
    [  OK  ] Reached target Hardware activated USB gadget.
    [  OK  ] Finished Permit User Sessions.
    [  OK  ] Started emptty display manager.
    [  OK  ] Started Getty on tty1.
    [  OK  ] Started Serial Getty on ttyS2.
    [  OK  ] Reached target Login Prompts.
             Starting ti-apps-launcher service...
    [  OK  ] Created slice Slice /system/tee-supplicant.
    [  OK  ] Started TEE Supplicant on teepriv0.
    [  OK  ] Started LLDP daemon.
    [   11.641501] remoteproc remoteproc2: 30074000.pru is available
    [   11.648328] remoteproc remoteproc3: 30078000.pru is available
    [  OK  ] Listening on Load/Save RF Kill Switch Status /dev/rfkill Watch.
             Starting Virtual Console Setup...
    [   12.216749] 30068000.serial: ttyS0 at MMIO 0x30068000 (irq = 431, base_baud = 12000000) is a 16550A
    [  OK  ] Created slice Slice /system/systemd-fsck.
             Expecting device /dev/mmcblk0p1...
             Starting Save/Restore Sound Card State...
    [  OK  ] Finished Save/Restore Sound Card State.
    [  OK  ] Reached target Sound Card.
    [  OK  ] Found device /dev/mmcblk0p1.
             Starting File System Check on /dev/mmcblk0p1...
    [  OK  ] Finished Virtual Console Setup.
    [  OK  ] Finished File System Check on /dev/mmcblk0p1.
             Mounting /run/media/mmcblk0p1...
    [  OK  ] Mounted /run/media/mmcblk0p1.
             Expecting device /dev/mmcblk1p1...
    
     _____                    _____           _         _
    |  _  |___ ___ ___ ___   |  _  |___ ___  |_|___ ___| |_
    |     |  _| .'| . | . |  |   __|  _| . | | | -_|  _|  _|
    |__|__|_| |__,|_  |___|  |__|  |_| |___|_| |___|___|_|
                  |___|                    |___|
    
    Arago Project am62xx-evm ttyS2
    
    Arago 2025.01 am62xx-evm ttyS2
    
    am62xx-evm login: [   18.275110] kauditd_printk_skb: 2 callbacks suppressed
    [   18.275131] audit: type=1006 audit(1736834487.612:14): pid=712 uid=0 subj=kernel old-auid=4294967295 auid=1000 tty=(none) old-ses=4294967295 ses=1 res=1
    [   18.294107] audit: type=1300 audit(1736834487.612:14): arch=c00000b7 syscall=64 success=yes exit=4 a0=8 a1=fffff6ed2258 a2=4 a3=1 items=0 ppid=1 pid=712 auid=1000 uid=0 gid=0 euid=0 suid=0 fsuid=0 egid=0 sgid=0 fsgid=0 tty=(none) ses=1 comm="(systemd)" exe="/usr/lib/systemd/systemd-executor" subj=kernel key=(null)
    [   18.321968] audit: type=1327 audit(1736834487.612:14): proctitle="(systemd)"
    ***************************************************************
    ***************************************************************
    NOTICE: This file system contains the following GPL-3.0 packages:
            adwaita-icon-theme-symbolic
            autoconf
            bash-dev
            bash
            bc
            binutils
            cifs-utils
            coreutils-stdbuf
            coreutils
            cpio
            cpp-symlinks
            cpp
            dosfstools
            elfutils-dev
            elfutils
            findutils
            g++-symlinks
            g++
            gawk
            gcc-symlinks
            gcc
            gdb
            gdbserver
            gettext
            glmark2
            gnu-config
            grub-common
            grub-editenv
            grub-efi
            gzip
            hidapi
            kbd-dev
            kbd-keymaps-pine
            less
            libasm1
            libatomic-dev
            libatomic1
            libbfd
            libdebuginfod1
            libdw1
            libelf1
            libgcc-s-dev
            libgcc1
            libgdbm-compat4
            libgdbm-dev
            libgdbm6
            libgettextlib
            libgettextsrc
            libgmp-dev
            libgmp10
            libgmpxx4
            libgnutls-dev
            libgnutls-openssl27
            libgomp1
            libidn2-0
            libidn2-dev
            libmpc3
            libmpfr6
            libopcodes
            libqt6core5compat-plugins
            libqt6core5compat-qmlplugins
            libqt6core5compat6
            libqt6shadertools-dev
            libqt6shadertools-plugins
            libqt6shadertools-qmlplugins
            libqt6shadertools6
            libreadline-dev
            libreadline8
            libstdc++-dev
            libstdc++6
            libtasn1-dev
            libunistring-dev
            libunistring5
            m4
            make
            nettle-dev
            nettle
            parted
            piglit
            qt3d-plugins
            qt3d-qmlplugins
            qt3d
            qtbase-dev
            qtbase-examples
            qtbase-plugins
            qtbase-qmlplugins
            qtbase-staticdev
            qtbase
            qtdeclarative-dev
            qtdeclarative-plugins
            qtdeclarative-qmlplugins
            qtdeclarative-staticdev
            qtdeclarative-tools
            qtdeclarative
            qtlanguageserver-dev
            qtlanguageserver-plugins
            qtlanguageserver-qmlplugins
            qtlanguageserver-staticdev
            qtlanguageserver
            qtmultimedia-plugins
            qtmultimedia-qmlplugins
            qtmultimedia
            qtquick3d-plugins
            qtquick3d-qmlplugins
            qtquick3d
            qtquicktimeline-plugins
            qtquicktimeline-qmlplugins
            qtquicktimeline
            qtsvg-dev
            qtsvg-plugins
            qtsvg-qmlplugins
            qtsvg
            qttools-plugins
            qttools-qmlplugins
            qttools
            qtwayland-dev
            qtwayland-plugins
            qtwayland-qmlplugins
            qtwayland
            tar
            which
    
    If you do not wish to distribute GPL-3.0 components please remove
    the above packages prior to distribution.  This can be done using
    the opkg remove command.  i.e.:
        opkg remove <package>
    Where <package> is the name printed in the list above
    
    NOTE: If the package is a dependency of another package you
          will be notified of the dependent packages.  You should
          use the --force-removal-of-dependent-packages option to
          also remove the dependent packages as well
    ***************************************************************
    ***************************************************************
    

    Hi Daolin, thanks for reply, above is the boot log

    in linux environment i use ethtool eth0 and eth1 respectively and it says:

    root@am62xx-evm:~# ethtool eth1
    Settings for eth1:
            Supported ports: [ TP    MII ]
            Supported link modes:   10baseT/Half 10baseT/Full
                                    100baseT/Half 100baseT/Full
                                    1000baseT/Full
            Supported pause frame use: Symmetric
            Supports auto-negotiation: Yes
            Supported FEC modes: Not reported
            Advertised link modes:  10baseT/Half 10baseT/Full
                                    100baseT/Half 100baseT/Full
                                    1000baseT/Full
            Advertised pause frame use: Symmetric
            Advertised auto-negotiation: Yes
            Advertised FEC modes: Not reported
            Speed: 10Mb/s
            Duplex: Half
            Auto-negotiation: on
            master-slave cfg: preferred slave
            master-slave status: unknown
            Port: Twisted Pair
            PHYAD: 1
            Transceiver: external
            MDI-X: Unknown
            Supports Wake-on: ubgs
            Wake-on: d
            SecureOn password: 00:00:00:00:00:00
            Current message level: 0x000020f7 (8439)
                                   drv probe link ifdown ifup rx_err tx_err hw
            Link detected: no

    there is a zyxel switch between board and computer, i use just one port, i tried both ports on board

    Best Regards

  • Hi Sevki,

    Thanks for sharing these details. I noticed right away that the "ethtool eth1" shows "Link detected: no". Was this output resulting from when you were testing eth0 or eth1? If you were testing with eth1, then this is a problem because it shows that there is no link established between the board and the switch you are using. A link is needed before communication can happen between the board and computer. 

    -Daolin