Other Parts Discussed in Thread: AM3517
Hi,
I have two bus-powered usb flash dirves. A has MaxPower 100 mA and B has MaxPower 500 mA.
I plug A drive to USB0 (HOST Mode), it's work and I could see this device on Storage Manager in WINCE.
When I plug B drive to USB0, it doesn't work. But when I put a self-powered hub between B drive and USB0, the B drive works and I could see this device on Storage Manager in WINCE.
Is there any power constraint of USB0 on AM3517 EVM ?
Thanks.