This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM62L: Multiple Errors and Warnings observed in EVK Boot Log (TFA, Kernel, Systemd)

Part Number: AM62L

Hi Support ,

I have been observing several recurring errors and warnings in our boot logs, even when using the standard binaries but none of them is a major issue .But i would like to know the reason behind these boot prints.

Could you please explain the reason and significance of the following print messages and why they are seen in the boot log?

Observed Log Messages:

  1. ERROR: Agent 0 Protocol 0x10 Message 0x7: not supported

  2. [FAILED] Failed to start Start psplash boot splash screen

  3. clk: failed to reparent 0_ADC0 to 2_ADC0: -22

  4. [FAILED] Failed to start Load/Save Screen Bâhtness of backlight:30500000.dsi.0.

  5. sysctl table check failed: ioctl/(null) procname is null

  6. sysctl table check failed: ioctl/(null) No proc_handler

  7. DMI not present or invalid

Any insight into this would be greatly appreciated.

Thank you