Other Parts Discussed in Thread: OMAPL138, OMAP-L138, AM1808
Hi,
Right now i started working with u-boot-2010.12-psp03.21.00.04 i am facing some issues while creating the ais file.
first of all i downloaded the sdk file from ti web. arm-arago-linux-gnueabi compiler using form linux-devkit folder.
my board configured for da850evm_config.
after the compilation i have two files u-boot, u-boot.bin.
i used ti hexgen tool to create ais file for uart boot.
Setting for INI files
BootMode=UART
crcCheckType=NO_CRC
[PLLANDCLOCKCONFIG]
PLL0CFG0 = 0x00080001
PLL0CFG1 = 0x00000b05
PERIPHCLKCFG = 0x00000051
[EMIF3DDR]
PLL1CFG0 = 0x08010001
PLL1CFG1 = 0x00000002
DDRPHYC1R = 0x00000043
SDCR = 0x00134632
SDTIMR = 0x24923209
SDTIMR2 = 0x7C14C722
SDRCR = 0x00000249
CLK2XSRC = 0x00000000
[INPUTFILE]
FILENAME=u-boot.bin
LOADADDRESS=0xC1080000
ENTRYPOINTADDRESS=0xC1080000
After the ais file creation i loaded uart.bin file with sft_omapl138.exe when it executes it is throwing error (I/o reading error).
Please help me resolve the issues.
Regards
jithin