This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM8168 C6ACCEL Canny Edge detection benchmark result...

I have to decide whether C6ACCEL Canny Edge Detection algorithm is used or not.

Is there any benchmark result on DM8168 of C6ACCEL Canny Edge Detection for 160x120 input image?

Is Canny Edge Detection algorithm satisfying the frame rate 60 fps(about 11.5 ms)?

In addition to the above question, are there any documents which describes C6ACCEL Video Analytics Allgorithm?