Other Parts Discussed in Thread: DM3730
Hi
I am having Mistral EVM(Rev G) with DM37XX on it.
I am using Gingerbread 2.3 devkit 1.o as my android development platform.
I am getting following error when I change display resolution to 1280x720 with display mode DVI.
omapdss DSI error: Requested pixel clock not possible with the current OMAP2_DSS_MIN_FCK_PER_PCK setting. Turning the constraint off.
Despite this error I can see the GUI screen on TV but display shows black strip on the right edge and some details gets stripped off on the left edge.
Kernel command lines I have tried are given below-:
Kernel command line: console=ttyS0,115200n8 androidboot.console=ttyS0 mem=256M root=/dev/mmcblk0p2 rw rootfstype=ext3 rootdelay=1 init=/init ip=off mpurate=7
20 omap_vout.vid1_static_vrfb_alloc=y vram=16M omapfb.vram=0:8M,1:4M,2:4M omapfb.mode=dvi:1280x720@25 omapdss.def_disp="dvi"
Kernel command line: console=ttyS0,115200n8 androidboot.console=ttyS0 mem=256M root=/dev/mmcblk0p2 rw rootfstype=ext3 rootdelay=1 init=/init ip=off mpurate=7
20 omap_vout.vid1_static_vrfb_alloc=y vram=16M omapfb.vram=0:8M,1:4M,2:4M omapfb.mode=dvi:1280x720 omapdss.def_disp="dvi"
Kernel command line: console=ttyS0,115200n8 androidboot.console=ttyS0 mem=256M root=/dev/mmcblk0p2 rw rootfstype=ext3 rootdelay=1 init=/init ip=off mpurate=7
20 omap_vout.vid1_static_vrfb_alloc=y vram=16M omapfb.vram=0:8M,1:4M,2:4M omapfb.mode=dvi:1280x720@50 omapdss.def_disp="dvi"
Is it possible to set 1280x720 as my resolution with this HW platform and this particular android version?
Please note that-:
1)There are no issues with kernel command line as it works fine for 1024x768 and 640x480 without any error.
2)There is no issue with TV as it is full HD LED tv and it supports above mentioned display modes.
What could be the possible solution?
Thanks,
Regards,
Prashant.