Part Number: AM5726
#1. I have an impression that the AVS driver check on-chip temperature in 1ms period to adjust AVS power supply. Please point me to the code where reflect it?
#2. If the custom board power supply desgin doesn't support AVS adjusting, it did not consider in the AVS feature, what will the driver do? will it adjust CPU frequence?
#3. The Kernel configurature is Performnace. will the lpm driver ajust CPU frequency automatically according to system loading or temperature? is there a configuration implement that?