This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Graphics SDK 4.05.00.03 X11 Support with Input



We have been running the pre-packaged X11 binaries provided with the Graphics SDK to begin development of our applications under Enlightenment using E17's OpenGL accelerating Compositing support.  As mentioned in the release notes, this performs well provided the cursor is disabled in the Xorg.conf.  Disabling the cursor, however, causes the X server to crash anytime keyboard or mouse input is received while it looks for the cursor position.

One of the approaches we were evaluating to get input working with our Qt based application was to patch the X server source to avoid this crash.  To that end, we had a few questions:

  • Are there any patches necessary to the Xorg sources for operation in DRI mode with the PVR driver?
  • Is the source for the PVR X11 driver available either through TI or Imagination Tech.?  Or are binaries available for later versions of the X server?
  • Are there any other issues we may run into in trying to use our own Xorg build?
Thanks for any assistance you can offer.
  • Nick - we are looking into this, and will respond soon.

  • Hi, just wanted to add my support to Nick's post. All of the things he is interested in are also important for us to know.

    Ralph

  • Hi Ralph,

    We have resolved all issues that Nick had reported by providing him with a release drop.

    You can download the same release with this ftp instructions

    The ftp pickup directory 'usithok' was created on 03/01/2012 05:30:00.
    The files from the dropoff area have been moved to the pickup directory and are available for 7 days.
    
    To retrieve the files from the pickup directory:
    
      1. Open an ftp session to ftppickup.ti.com.
             ftp ftppickup.ti.com
    
      2. Login with the userid 'pickup'.
             Name: pickup
    
      3. Enter the password.
             Password: piurh!
    
      4. Change directories to the pickup directory.
             ftp> cd /pub/share/usithok
    
         Note: If you are using a graphical ftp client, you will not 
               see the hidden pickup directory name usithok appear 
               in the file list.  You will need to use a manual 
               'Change Directory' or 'CD' command to change into the 
               dropoff directory.
    
      5. Set the file transfer mode to ascii or binary as necessary.
             ftp> bin
    
      6. Transfer the file.
             ftp> get <file>
    
      7. End the ftp session.
             ftp> quit
    
    The files can also be retrieved with the url:
    
      ftp://pickup@ftppickup.ti.com/pub/share/usithok
    
    List of files in the pickup directory 'usithok':
    Graphics_SDK_setuplinux_4_06_00_01.bin
    
    (please download it now as it will expire by 8th March).

    Nick,

    Can you please click on verify answer & close this query?

    Thanks,

    Prathap.

  • Yes, Prathap was able to provide an engineering build which resolved all of these issues and more.

     

    Thanks.

  • Hi Prathap,

    Thanks for the link. Can I take it that this release will be the same as the publicly available graphics SDK version 4.06.00.01 when it comes out?

    Ralph

  • Ralph,

    Yes almost close to that.  Some minor items below will also be resolved. Anyways they should not impact you & you can use this release till we make an official drop.

    1)Shader compilation issue with use of return statement in void functions & multiple returns in a function reported by Nick.

    2)Debug build metrics issue.

    3)Cleanup of install_dri.sh reported by you.

    Our plan is to make the official release by 1st week of April.

    Thanks,

    Prathap.

  • Okay, good. I'd verify your post if I could!