This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Adding new sections to linker command file

Hi,

I need to create some shared memory space in DDR which will be used to communicate between several devices.

linker.cmd states:

* Do not modify this file; it is automatically generated from the template
 * linkcmd.xdt in the ti.targets package and will be overwritten.

I would like to change

MEMORY
{
    IRAM (RWX) : org = 0x10800000, len = 0x40000
    OCMC (RWX) : org = 0x40300000, len = 0x20000
    DDR3_RAM : org = 0x80000000, len = 0x10000000
}

to

MEMORY
{
    IRAM (RWX) : org = 0x10800000, len = 0x40000
    OCMC (RWX) : org = 0x40300000, len = 0x20000
    MY_RAM : org = 0x80000000, len = 0x01000000
    DDR3_RAM : org = 0x81000000, len = 0x0F000000                                          
}

Any statically allocated buffers would end up in .bss somewhere in DDR3_RAM.

MY_RAM would be kept clear.

I have two questions

1. How do I implement this change, when the file is overwritten?

2. How do I statically allocate into MY_RAM with a section declaration when allocating the buffer?

something like???

 char my_buffer __attribute__ ((section ("MY_RAM")));

Thanks,

Michael.