This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA4VL-Q1: [MMC] Device support for 2MHz clock

Part Number: TDA4VL-Q1
Other Parts Discussed in Thread: TDA4VL

Hi,

We are currently using and external clock fror driving one of our on board ASICs. We would like to replace this clock source with the TDA4VL SoC. Can you confirm if there is a clock output on the TDA4VL which is capable of providing  2MHz +/- 0.05% ? From the datasheet I see some outputs named however they are at higher frequency or "should not be used as a clock source for external devices on a board." Maybe I am missing some other options?

Thanks

Brian