This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

USB disk performs slower than SD memory

Hi all,

I am using following configurations.

Platform: WinCE OMAP 3730

DVSDK version: dvsdk_wince_01_11_00_02

BSP version:  01.02.00

We have our directshow filters developed for a media player application. I am running MPEG2 clip with bitrate 9 Mbps from SD memory and the clip works fine woth this setup. But if I try to play the same clip from USB disk, I hear breaks in audio. As per my knowledge, USB must provide better performance than SD memory and hance work faster.

Can you please provide any hints about this issue?

 

Regards,

Vinuta