Part Number: AM5726
Other Parts Discussed in Thread: TPS659037
We have connected a QSPI flash to the AM5726 processor according to the picture.
The bank power supply for all these pins is corrcet (1.8V) The communication is not stable. Also with the oscilloscop. It looks as if the RTCLK input is not a input.
For testing we put all these pins into simple GPIO mode. Also with R139=150 Ohm The RTCLK input pin falsies the SCLK output signal.
What is wrong with these "input" pins? Do we have a hardware corruption? Why?
This is the signal at the RTLK "input" (blue) pin when toggeling SCLK (violet). Also as stupid IO.