Part Number: AM69
Other Parts Discussed in Thread: UNIFLASH
We are looking to program uboot using USB or UART on the AM69 without having an SDcard. In the AM69 SDK docs , It lists that we should be able to use USB: https://software-dl.ti.com/jacinto7/esd/processor-sdk-linux-am69/11_00_10_01/exports/docs/linux/Foundational_Components/U-Boot/UG-DFU.html.
It also states that we can use Uniflash as well: https://software-dl.ti.com/jacinto7/esd/processor-sdk-linux-am69/11_00_10_01/exports/docs/linux/Foundational_Components/Tools/Flash_Tools.html
We are not able to get either of these to work on the AM69-SK. In the case of USB and dfu-util it cannot detect the connection. From what I have read this may be due to the AM69-SK using a usb hub. Please let us know if this is the case and our options. Our prototypes will not use the hub so we hope that is the limitation
Also, I downloaded Uniflash, but there is no configuration for AM69 processors. Can you provide more information regarding this as well?
If there are other options supported such as UART, please let us know.