Other Parts Discussed in Thread: TDA4VM
Hi,
I am using the following documentation for installing and using the procecessor sdk linux for TDA4VM ==> software-dl.ti.com/.../Ove…
We have a j721e device named "j721excp01evm" and i am working on this. I am stuck in the initial sdk installation step. specifically while doing "Yocto Scarthgap based build " which is specified in the documentation which I provided above.
Below given is the error which i am getting ==>
tisdk@74f134eb899b:/u/tisdk/tisdk/build$ MACHINE=am62xx-evm bitbake -k tisdk-default-image
ERROR: Logfile of failure stored in: /u/tisdk/tisdk/build/arago-tmp-default-glibc/work/aarch64-oe-linux/seva-launcher/v1.0.7/temp/log.do_fetch.1536603
ERROR: Task (/u/tisdk/tisdk/sources/meta-tisdk/meta-ti-foundational/recipes-demos/seva/seva-launcher.bb:do_fetch) failed with exit code '1'
ERROR: ti-cgt-pru-native-2.3.3-r0 do_fetch: Fetcher failure: Fetch command export PSEUDO_DISABLED=1; export SSL_CERT_DIR="/etc/ssl/certs"; export SSL_CERT_FILE="/etc/ssl/certs/ca-certificates.crt"; export PATH="/u/tisdk/tisdk/sources/oe-core/scripts/native-intercept:/u/tisdk/tisdk/sources/oe-core/scripts:/u/tisdk/tisdk/build/arago-tmp-default-glibc/work/x86_64-linux/ti-cgt-pru-native/2.3.3/recipe-sysroot-native/usr/bin/x86_64-linux:/u/tisdk/tisdk/build/arago-tmp-default-glibc/work/x86_64-linux/ti-cgt-pru-native/2.3.3/recipe-sysroot-native/usr/bin:/u/tisdk/tisdk/build/arago-tmp-default-glibc/work/x86_64-linux/ti-cgt-pru-native/2.3.3/recipe-sysroot-native/usr/sbin:/u/tisdk/tisdk/build/arago-tmp-default-glibc/work/x86_64-linux/ti-cgt-pru-native/2.3.3/recipe-sysroot-native/usr/bin:/u/tisdk/tisdk/build/arago-tmp-default-glibc/work/x86_64-linux/ti-cgt-pru-native/2.3.3/recipe-sysroot-native/sbin:/u/tisdk/tisdk/build/arago-tmp-default-glibc/work/x86_64-linux/ti-cgt-pru-native/2.3.3/recipe-sysroot-native/bin:/u/tisdk/tisdk/sources/bitbake/bin:/u/tisdk/tisdk/build/arago-tmp-default-glibc/hosttools"; export HOME="/home/tisdk"; /usr/bin/env wget -t 2 -T 100 -O /u/tisdk/tisdk/downloads/ti_cgt_pru_2.3.3_linux_installer_x86.bin.tmp -P /u/tisdk/tisdk/downloads 'http://software-dl.ti.com/codegen/esd/cgt_public_sw/PRU/2.3.3/ti_cgt_pru_2.3.3_linux_installer_x86.…' --progress=dot -v failed with exit code 8, see logfile for output
ERROR: ti-cgt-pru-native-2.3.3-r0 do_fetch: Bitbake Fetcher Error: FetchError('Unable to fetch URL from any source.', 'software-dl.ti.com/.../ti_cgt_pru_2.3.3_linux_installer_x86.…
ERROR: Logfile of failure stored in: /u/tisdk/tisdk/build/arago-tmp-default-glibc/work/x86_64-linux/ti-cgt-pru-native/2.3.3/temp/log.do_fetch.1536350
ERROR: Task (virtual:native:/u/tisdk/tisdk/sources/meta-ti/meta-ti-extras/recipes-ti/devtools/ti-cgt-pru_2.3.3.bb:do_fetch) failed with exit code '1'
ERROR: opengl-es-cts-3.2.9.3-r0 do_fetch: Fetcher failure: Fetch command export PSEUDO_DISABLED=1; export SSL_CERT_DIR="/etc/ssl/certs"; export SSL_CERT_FILE="/etc/ssl/certs/ca-certificates.crt"; export PATH="/u/tisdk/tisdk/build/arago-tmp-default-glibc/work/aarch64-oe-linux/opengl-es-cts/3.2.9.3/recipe-sysroot-native/usr/bin/python3-native:/u/tisdk/tisdk/sources/oe-core/scripts:/u/tisdk/tisdk/build/arago-tmp-default-glibc/work/aarch64-oe-linux/opengl-es-cts/3.2.9.3/recipe-sysroot-native/usr/bin/aarch64-oe-linux:/u/tisdk/tisdk/build/arago-tmp-default-glibc/work/aarch64-oe-linux/opengl-es-cts/3.2.9.3/recipe-sysroot/usr/bin/crossscripts:/u/tisdk/tisdk/build/arago-tmp-default-glibc/work/aarch64-oe-linux/opengl-es-cts/3.2.9.3/recipe-sysroot-native/usr/sbin:/u/tisdk/tisdk/build/arago-tmp-default-glibc/work/aarch64-oe-linux/opengl-es-cts/3.2.9.3/recipe-sysroot-native/usr/bin:/u/tisdk/tisdk/build/arago-tmp-default-glibc/work/aarch64-oe-linux/opengl-es-cts/3.2.9.3/recipe-sysroot-native/sbin:/u/tisdk/tisdk/build/arago-tmp-default-glibc/work/aarch64-oe-linux/opengl-es-cts/3.2.9.3/recipe-sysroot-native/bin:/u/tisdk/tisdk/sources/bitbake/bin:/u/tisdk/tisdk/build/arago-tmp-default-glibc/hosttools"; export HOME="/home/tisdk"; /usr/bin/env wget -t 2 -T 100 -O /u/tisdk/tisdk/downloads/renderdoc_app.h.tmp -P /u/tisdk/tisdk/downloads 'https://raw.githubusercontent.com/baldurk/renderdoc/v1.1/renderdoc/api/app/renderdoc_app.h' --progress=dot -v failed with exit code 8, see logfile for output
ERROR: opengl-es-cts-3.2.9.3-r0 do_fetch: Bitbake Fetcher Error: FetchError('Unable to fetch URL from any source.', 'raw.githubusercontent.com/.../renderdoc_app.h;subdir=g…
ERROR: Logfile of failure stored in: /u/tisdk/tisdk/build/arago-tmp-default-glibc/work/aarch64-oe-linux/opengl-es-cts/3.2.9.3/temp/log.do_fetch.1536352
ERROR: Task (/u/tisdk/tisdk/sources/meta-openembedded/meta-oe/recipes-graphics/vk-gl-cts/opengl-es-cts_3.2.9.3.bb:do_fetch) failed with exit code '1'
ERROR: openntpd-6.8p1-r0 do_fetch: Fetcher failure: Fetch command export PSEUDO_DISABLED=1; export SSL_CERT_DIR="/etc/ssl/certs"; export SSL_CERT_FILE="/etc/ssl/certs/ca-certificates.crt"; export PATH="/u/tisdk/tisdk/sources/oe-core/scripts:/u/tisdk/tisdk/build/arago-tmp-default-glibc/work/aarch64-oe-linux/openntpd/6.8p1/recipe-sysroot-native/usr/bin/aarch64-oe-linux:/u/tisdk/tisdk/build/arago-tmp-default-glibc/work/aarch64-oe-linux/openntpd/6.8p1/recipe-sysroot/usr/bin/crossscripts:/u/tisdk/tisdk/build/arago-tmp-default-glibc/work/aarch64-oe-linux/openntpd/6.8p1/recipe-sysroot-native/usr/sbin:/u/tisdk/tisdk/build/arago-tmp-default-glibc/work/aarch64-oe-linux/openntpd/6.8p1/recipe-sysroot-native/usr/bin:/u/tisdk/tisdk/build/arago-tmp-default-glibc/work/aarch64-oe-linux/openntpd/6.8p1/recipe-sysroot-native/sbin:/u/tisdk/tisdk/build/arago-tmp-default-glibc/work/aarch64-oe-linux/openntpd/6.8p1/recipe-sysroot-native/bin:/u/tisdk/tisdk/sources/bitbake/bin:/u/tisdk/tisdk/build/arago-tmp-default-glibc/hosttools"; export HOME="/home/tisdk"; /usr/bin/env wget -t 2 -T 100 -O /u/tisdk/tisdk/downloads/openntpd-6.8p1.tar.gz.tmp -P /u/tisdk/tisdk/downloads 'https://cdn.openbsd.org/pub/OpenBSD/OpenNTPD/openntpd-6.8p1.tar.gz' --progress=dot -v failed with exit code 8, see logfile for output
ERROR: openntpd-6.8p1-r0 do_fetch: Bitbake Fetcher Error: FetchError('Unable to fetch URL from any source.', 'https://cdn.openbsd.org/pub/OpenBSD/OpenNTPD/openntpd-6.8p1.tar.gz')
ERROR: Logfile of failure stored in: /u/tisdk/tisdk/build/arago-tmp-default-glibc/work/aarch64-oe-linux/openntpd/6.8p1/temp/log.do_fetch.1536613
Summary: 6 tasks failed:
/u/tisdk/tisdk/sources/meta-arago/meta-arago-extras/recipes-devtools/arm-compute-library/arm-compute-library_24.12.bb:do_fetch
log: /u/tisdk/tisdk/build/arago-tmp-default-glibc/work/aarch64-oe-linux/arm-compute-library/24.12/temp/log.do_fetch.1536326
/u/tisdk/tisdk/sources/meta-openembedded/meta-oe/recipes-graphics/vk-gl-cts/vulkan-cts_1.3.7.3.bb:do_fetch
log: /u/tisdk/tisdk/build/arago-tmp-default-glibc/work/aarch64-oe-linux/vulkan-cts/1.3.7.3/temp/log.do_fetch.1536351
/u/tisdk/tisdk/sources/meta-tisdk/meta-ti-foundational/recipes-demos/seva/seva-launcher.bb:do_fetch
log: /u/tisdk/tisdk/build/arago-tmp-default-glibc/work/aarch64-oe-linux/seva-launcher/v1.0.7/temp/log.do_fetch.1536603
virtual:native:/u/tisdk/tisdk/sources/meta-ti/meta-ti-extras/recipes-ti/devtools/ti-cgt-pru_2.3.3.bb:do_fetch
log: /u/tisdk/tisdk/build/arago-tmp-default-glibc/work/x86_64-linux/ti-cgt-pru-native/2.3.3/temp/log.do_fetch.1536350
/u/tisdk/tisdk/sources/meta-openembedded/meta-oe/recipes-graphics/vk-gl-cts/opengl-es-cts_3.2.9.3.bb:do_fetch
log: /u/tisdk/tisdk/build/arago-tmp-default-glibc/work/aarch64-oe-linux/opengl-es-cts/3.2.9.3/temp/log.do_fetch.1536352
/u/tisdk/tisdk/sources/meta-arago/meta-arago-test/recipes-connectivity/openntpd/openntpd_6.8p1.bb:do_fetch
log: /u/tisdk/tisdk/build/arago-tmp-default-glibc/work/aarch64-oe-linux/openntpd/6.8p1/temp/log.do_fetch.1536613
Summary: There were 6 WARNING messages.
Summary: There were 12 ERROR messages, returning a non-zero exit code.
tisdk@74f134eb899b:/u/tisdk/tisdk/build$ cd sources/meta-arago/meta-arago-extras/recipes-devtools/arm-compute-library/
bash: cd: sources/meta-arago/meta-arago-extras/recipes-devtools/arm-compute-library/: No such file or directory