Other Parts Discussed in Thread: AM3703
Hi all,
I 'm using am3703 board,
I want to do lcd_initialisation in u-boot code.
Can anyone help me?
Regards,
santosh vastrad
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: AM3703
Hi all,
I 'm using am3703 board,
I want to do lcd_initialisation in u-boot code.
Can anyone help me?
Regards,
santosh vastrad
Basic display driver support is already available in the u-boot mainline, please refer to the
Having said that, note that this has never been supported in any of the PSP release yet. You have to either use mainline u-boot OR backport this patch to PSP release u-boot.
Thanks,
Vaibhav
Thanks for the reply Vaibhav,
I will check out the link you sent!!!!!!!!!!!!!!!!!
Regards,
santosh vastrad
HI Vaibhav,
According to your suggestions, and also the information given by you , I referred and accroding to that i 've modified in my am3703 board,
board/ti/beagle/beagel.c -> Initialisation of the LCD i did.
board/ti/beagle/logo.c-> Logo to display on LCD
arch/arm/include/asm/arch-omap3/omapdss.h
drivers/video/omapdss.c
Everything i did needed to display the Logo on LCD.
But the thing is that when in my u-boot execution flow, omapdss_init(&lcd);
drivers/video/omapdss.c => some junk is coming!!!!!!!!!!!!!!!!!!!
U-Boot 2010.06-rc1 (Jan 23 2012 - 12:07:15)
OMAP34xx/35xx-GP ES2.1, CPU-OPP2 L3-165MHz
OMAP3 Beagle board + LPDDR/NAND
I2C: ready
DRAM: 256 MiB
NAND: 512 MiB
In: serial
Out: serial
Err: serial
Beagle Rev Ax/Bx
Die ID #6e4600029e380000016830c501032014
???????????????????????????????????????????^*(^&*(###########
Just i shown some characters, there it is problem!!!!!!!!!!!
Regards,
santosh vastrad