Other Parts Discussed in Thread: TLV320AIC34, TLV320AIC3106
Hi all,
We are interfacing the AIC34 to beaglebone AM335x McASP0(as we do not have McASP1 lines accessible in the beaglebone).
In TI AM335x EVM McASP1 is interfaced with the codec AIC3106.
Following are the changes made in order to configure the McASP0 and to interface with AIC34.
arch/arm/mach-omap2/board-am335xevm.c
static struct pinmux_config mcasp0_pin_mux[] = {
{"lcd_data8.mcasp0_aclkx", OMAP_MUX_MODE3 |AM33XX_PIN_INPUT_PULLDOWN},
{"lcd_data9.mcasp0_fsx", OMAP_MUX_MODE3 |AM33XX_PIN_INPUT_PULLDOWN},
{"lcd_data12.mcasp0_axr2", OMAP_MUX_MODE4 |AM33XX_PIN_INPUT_PULLDOWN},
{"lcd_data13.mcasp0_axr3", OMAP_MUX_MODE4 |AM33XX_PIN_INPUT_PULLDOWN},
{NULL, 0},
};
static u8 am335x_iis_serializer_direction1[] = {
INACTIVE_MODE, INACTIVE_MODE, TX_MODE, RX_MODE,
INACTIVE_MODE, INACTIVE_MODE, INACTIVE_MODE, INACTIVE_MODE,
INACTIVE_MODE, INACTIVE_MODE, INACTIVE_MODE, INACTIVE_MODE,
INACTIVE_MODE, INACTIVE_MODE, INACTIVE_MODE, INACTIVE_MODE,
};
static struct snd_platform_data am335x_evm_snd_data0 = {
.tx_dma_offset = 0x46000000, /* McASP0 */
.rx_dma_offset = 0x46000000,
.op_mode = DAVINCI_MCASP_IIS_MODE,
.num_serializer = ARRAY_SIZE(am335x_iis_serializer_direction1),
.tdm_slots = 2,
.serial_dir = am335x_iis_serializer_direction1,
.asp_chan_q = EVENTQ_2,
.version = MCASP_VERSION_3,
.txnumevt = 1,
.rxnumevt = 1,
};
/* Setup McASP 0 */
static void mcasp0_init(int evm_id, int profile)
{
/* Configure McASP */
setup_pin_mux(mcasp0_pin_mux);
am335x_register_mcasp0(&am335x_evm_snd_data0);
return;
}
arch/arm/mach-omap2/devices.c
static struct resource am335x_mcasp0_resource[] = {
{
.name = "mcasp0",
.start = AM33XX_ASP0_BASE,
.end = AM33XX_ASP0_BASE + (SZ_1K * 12) - 1,
.flags = IORESOURCE_MEM,
},
/* TX event */
{
.start = AM33XX_DMA_MCASP0_X,
.end = AM33XX_DMA_MCASP0_X,
.flags = IORESOURCE_DMA,
},
/* RX event */
{
.start = AM33XX_DMA_MCASP0_R,
.end = AM33XX_DMA_MCASP0_R,
.flags = IORESOURCE_DMA,
},
};
static struct platform_device am335x_mcasp0_device = {
.name = "davinci-mcasp",
.id = 0,
.num_resources = ARRAY_SIZE(am335x_mcasp0_resource),
.resource = am335x_mcasp0_resource,
};
void __init am335x_register_mcasp0(struct snd_platform_data *pdata)
{
am335x_mcasp0_device.dev.platform_data = pdata;
platform_device_register(&am335x_mcasp0_device);
}
sound/soc/davinci/davinci-evm.c
static struct snd_soc_dai_link am335x_evm_dai = {
.name = "TLV320AIC3X",
.stream_name = "AIC3X",
.cpu_dai_name = "davinci-mcasp.0",
.codec_dai_name = "tlv320aic3x-hifi",
.codec_name = "tlv320aic3x-codec.2-001a",
.platform_name = "davinci-pcm-audio",
.init = evm_aic3x_init,
.ops = &evm_ops,
};
With the above mentioned changes I am able to register the McASP0
[ 1.276813] asoc: tlv320aic3x-hifi <-> davinci-mcasp.0 mapping ok
when I try to play song using aplay I am getting the following error.
aplay: pcm_write:1575: write error: Input/output error
Please suggest.
Regards,
Vishwas HC