Part Number: AM4372
Hi team,
I have questions regarding the AM4372 power pins and power-down sequence.
-
In the datasheet section [5.12.1.1 Power Supply Slew Rate Requirement], what specifically are the "internal ESD protection devices" mentioned? Are these clamp diodes or similar? If diodes are used, which lines are they connected to?
-
In the datasheet section [5.12.1.3 Power-Down Sequencing], it states that the potential difference between VDDS/VDDS_CLKOUT and VDDSHVx[x=1-11] must always be less than 2V during power-down. Is it correct to assume that VDDS/VDDS_CLKOUT exceeding VDDSHV[x] during the power-down sequence is not inherently problematic, as long as the 2V differential requirement is met? Please confirm this understanding.
Best regards,
Goto