Part Number: AM3357
Hi Team,
Condition:
Customer is using am3357 connect fpga to transform data, base on this feature they are using gprmc to send the data.
Requirement:
Previous : sdk_01.01.02.01 with ccs 6.1.3
Current : sdk_6_03_00_106
Feasture : GPMC_Transfer() minimam 4 byte (if set as 2 Bytes, then it can send continuely)
In the previous sdk is around 800ns per transfer
In the new sdk is over 1us
Requirement :
As the customer they have capability to modified code
First solution -> they are asking is it possible to teach them how to build (ti.drv.gpmc.aa8fg)
as picture they can't find the lib, i think they just don't know where the feature definition?
And how to build
Secound solution -> could the bu provide the control method to only work
HW_WR_REG16(hwAttrs->gpmcBaseAddr + GPMC_NAND_DATA_N(hwAttrs->chipSel), *pData16) HW_RD_REG16(hwAttrs->gpmcBaseAddr + GPMC_NAND_DATA_N(hwAttrs->chipSel))