Hi,
I'm having trouble using the SPI programmer for the ezdsp5535 available at: http://support.spectrumdigital.com/boards/ezdsp5535/revc/
When I run it I get the following result:
C5535 eZDSP...
Input <filepath>
C:\Users\user\Desktop\bootimg.bin
SPI Flash...
Erasing chip (SPI Flash)...
Opening C:\Users\user\Desktop\bootimg.bin...
Input file opened
WRITE ERROR! at 0x00008000
Wrote 0x09aa Read 0x0000
I got it working once a couple of weeks ago, but now when I tried it again the result is this error. Any idea whats wrong?
I'm using the gel file from the same site mentioned above, and the bin I'm trying to flash is a slightly modified version of the audio framework for the ezdsp5535. I've tried flashing the original bootimg.bin from the audio framework as well without luck.
Best regards
Marcus