Hi,
I've got a question according to a certain PHY we are using on our board, The PHY is the DP83848YB by TI. We've tried to build a simple UDP client using the EVM6748 from LogicPD. The application works fine on the evaluation board and we are able to receive data on the PC-side, but when the same application runs on the custom board which has the mentioned PHY, no data is sent via ethernet. It seems that the PHY is simply not supported. Is there any code out there which adds support to NSP / NDK for this transceiver? If we have to port this device to the NDK is there any guideline what describes what to do? http://processors.wiki.ti.com/index.php/Guidelines_when_porting_NDK_to_different_PHYs seems to be a little bit outdated?
Any help on this issue would be very appreciated. Please let me know if you need additional information...
NDK Version is 2.20.6.35
NSP Version is 1.10.0.03
Kind Regards,
Steve