Other Parts Discussed in Thread: OMAP-L137
Hello,
I'm using an evmomapl137 board from Spectrum Digital for educational purpose. What I would like to do is to send a signal to the microphone input, filter it with the DSP, and send it back to headphone output, all of this with the interruptions. While I have succeeded in doing that (I see the signal on the oscilloscope), there is no difference between the left and the right channel, despite modifying the balance on the computer.
The board is equiped with an OMAP-L137 and an AIC3106 audio codec. After studying the manual of the McASP of the omap and the codec, I was unable to find the source of my problems. I tried to compare with several configurations I found on the net without success. I don't even know if the problem comes from the McASP or the AIC3106...
Does anyone ever realize a similar thing or have the explanation of this problem?
Thank you in advance
Guillaume
Here is the configuration I'm using for the AIC3106:
int16_t
EVMOMAPL137_AIC3106_open (void)
{
// Configure AIC3106
EVMOMAPL137_AIC3106_rset( AIC3106_PAGESELECT, 0 );
// Select page 0
EVMOMAPL137_AIC3106_rset( AIC3106_RESET, 0x80 );
// Reset AIC3106
// Configure AIC3106 registers
EVMOMAPL137_AIC3106_rset( 3, 0x22 );// 5 PLL A <- [PLL=OFF][Q=4][P=2]
EVMOMAPL137_AIC3106_rset( 4, 0x20 );// 4 PLL B <- [J=8]
EVMOMAPL137_AIC3106_rset( 5, 0x6E );// 5 PLL C <- [D=7075]
EVMOMAPL137_AIC3106_rset( 6, 0x23 );// 6 PLL D <- [D=7075]
EVMOMAPL137_AIC3106_rset( 7, 0x0A );// 7 Codec Datapath Setup <- [FS=48 kHz][LeftDAC=LEFT][RightDAC=RIGHT]
EVMOMAPL137_AIC3106_rset( 8, 0x00 );// 8 Audio Interface Control A <- [BCLK=Slave][MCLK=Slave]
EVMOMAPL137_AIC3106_rset( 9, 0x00 );// 9 Audio Interface Control B <- [I2S mode][16 bit]
EVMOMAPL137_AIC3106_rset( 10, 0x00);// 10 Audio Interface Control C <- [Data offset=0]
EVMOMAPL137_AIC3106_rset( 15, 0x17 );// 15 Left ADC PGA Gain <- [Mute=OFF][Gain=8.5dB]
EVMOMAPL137_AIC3106_rset( 16, 0x17 );// 16 Right ADC PGA Gain <- [Mute=OFF][Gain=8.5dB]
EVMOMAPL137_AIC3106_rset( 17, 0x0F );// 17 MIC3L/R to Left ADC <- [MIC3L=0dBGain][MIC3R=NotConnect]
EVMOMAPL137_AIC3106_rset( 18, 0xF0 );// 18 MIC3L/R to Right ADC <- [MIC3L=NotConnect][MIC3R=0dBGain]
EVMOMAPL137_AIC3106_rset( 19, 0x7C );// 19 LINE1L to Left ADC <- [SingleEnd][NotConnect][Power=ON][SoftStep=OncePerFS]
EVMOMAPL137_AIC3106_rset( 22, 0x7C );// 22 LINE1R to Right ADC <- [SingleEnd][NotConnect][Power=ON][SoftStep=OncePerFS]
EVMOMAPL137_AIC3106_rset( 25, 0x40 );// 25 MICBIAS <- [MICBIAS=2.0V]
EVMOMAPL137_AIC3106_rset( 27, 0 );// 27 Left AGC B <- [OFF]
EVMOMAPL137_AIC3106_rset( 30, 0 );// 30 Right AGC B <- [OFF]
EVMOMAPL137_AIC3106_rset( 37, 0xE0 ); // 37 DAC Power & Output Dvr <- [LeftDAC=ON][RightDAC=ON][HPLCOM=SingleEnd]
EVMOMAPL137_AIC3106_rset( 38, 0x10 ); // 38 High Power Output Dvr <- [HPRCOM=SingleEnd][ShortCircuit=OFF]
EVMOMAPL137_AIC3106_rset( 43, 0 );// 43 Left DAC Digital Volume <- [Mute=OFF][Gain=0dB]
EVMOMAPL137_AIC3106_rset( 44, 0 );// 44 Right DAC Digital Volume <- [Mute=OFF][Gain=0dB]
EVMOMAPL137_AIC3106_rset( 47, 0x80 );// 47 DAC_L1 to HPLOUT Volume <- [Routed]
EVMOMAPL137_AIC3106_rset( 51, 0x09 );// 51 HPLOUT Output <- [Mute=OFF][Power=ON]
EVMOMAPL137_AIC3106_rset( 58, 0 );// 58 HPLCOM Output <- []
EVMOMAPL137_AIC3106_rset( 64, 0x80 );// 64 DAC_R1 to HPROUT Volume <- [Routed]
EVMOMAPL137_AIC3106_rset( 65, 0x09 );// 65 HPROUT Output <- [Mute=OFF][Power=ON]
EVMOMAPL137_AIC3106_rset( 72, 0 );// 72 HPRCOM Output <- []
EVMOMAPL137_AIC3106_rset( 82, 0x80 );// 82 DAC_L1 to LEFT_LOP/M Volume <- [Routed]
EVMOMAPL137_AIC3106_rset( 86, 0x09 );// 86 LEFT_LOP/M Output <- [Mute=OFF][Power=ON]
EVMOMAPL137_AIC3106_rset( 92, 0x80 );// 92 DAC_R1 to RIGHT_LOP/M Volume <- [Routed]
EVMOMAPL137_AIC3106_rset( 93, 0x09 );// 93 RIGHT_LOP/M Output <- [Mute=OFF][Power=ON]
EVMOMAPL137_AIC3106_rset( 101, 0x01 );// 101 GPIO Control Register B <- [CODEC_CLKIN = CLKDIV_OUT]
EVMOMAPL137_AIC3106_rset( 102, 0 );// 102 Clock Generation Control <- [PLLCLK_IN and CLKDIV_IN use MCLK]
return 0;
}
And the configuration of the McASP:
int16_t
EVMOMAPL137_MCASP_open (void)
{
mcasp = &MCASP_MODULE_1;
mcasp->regs->GBLCTL = 0; // Reset
mcasp->regs->RGBLCTL = 0; // Reset RX
mcasp->regs->XGBLCTL = 0; // Reset TX
mcasp->regs->PWRDEMU = 1; // Free-running
// RX
mcasp->regs->RMASK = 0xffffffff; // No padding used
mcasp->regs->RFMT = 0x00008078; // MSB 16bit, 1-delay, no pad, CFGBus
mcasp->regs->AFSRCTL = 0x00000112; // 2TDM, 1bit Rising, INTERNAL FS, word
mcasp->regs->ACLKRCTL = 0x000000AF; // Rising INTERNAL CLK,(from tx side)
mcasp->regs->AHCLKRCTL = 0x00000000; // INT CLK (from tx side)
mcasp->regs->RTDM = 0x00000003; // Slots 0,1
mcasp->regs->RINTCTL = 0x00000000; // Not used
mcasp->regs->RCLKCHK = 0x00FF0008; // 255-MAX 0-MIN, div-by-256
// TX
mcasp->regs->XMASK = 0xffffffff; // No padding used
mcasp->regs->XFMT = 0x00008078; // MSB 16bit, 1-delay, no pad, CFGBus
mcasp->regs->AFSXCTL = 0x00000112; // 2TDM, 1bit Rising edge INTERNAL FS, word
mcasp->regs->ACLKXCTL = 0x000000AF; // ASYNC, Rising INTERNAL CLK, div-by-16
mcasp->regs->AHCLKXCTL = 0x00000000; // EXT CLK
mcasp->regs->XTDM = 0x00000003; // Slots 0,1
mcasp->regs->XINTCTL = 0x00000000; // Not used
mcasp->regs->XCLKCHK = 0x00FF0008; // 255-MAX 0-MIN, div-by-256
mcasp->regs->SRCTL5 = 0x000D; // MCASP1.AXR1[5] --> DIN
mcasp->regs->SRCTL0 = 0x000E; // MCASP1.AXR1[0] <-- DOUT
mcasp->regs->PFUNC = 0; // All MCASPs
mcasp->regs->PDIR = 0x14000020; // All inputs except AXR0[5], ACLKX1, AFSX1
mcasp->regs->DITCTL = 0x00000000; // Not used
mcasp->regs->DLBCTL = 0x00000000; // Not used
mcasp->regs->AMUTE = 0x00000000; // Not used
// Starting sections of the McASP
mcasp->regs->XGBLCTL |= GBLCTL_XHCLKRST_ON; // HS Clk
while ( ( mcasp->regs->XGBLCTL & GBLCTL_XHCLKRST_ON ) != GBLCTL_XHCLKRST_ON );
mcasp->regs->RGBLCTL |= GBLCTL_RHCLKRST_ON; // HS Clk
while ( ( mcasp->regs->RGBLCTL & GBLCTL_RHCLKRST_ON ) != GBLCTL_RHCLKRST_ON );
mcasp->regs->XGBLCTL |= GBLCTL_XCLKRST_ON; // Clk
while ( ( mcasp->regs->XGBLCTL & GBLCTL_XCLKRST_ON ) != GBLCTL_XCLKRST_ON );
mcasp->regs->RGBLCTL |= GBLCTL_RCLKRST_ON; // Clk
while ( ( mcasp->regs->RGBLCTL & GBLCTL_RCLKRST_ON ) != GBLCTL_RCLKRST_ON );
mcasp->regs->XSTAT = 0x0000ffff; // Clear all
mcasp->regs->RSTAT = 0x0000ffff; // Clear all
mcasp->regs->XGBLCTL |= GBLCTL_XSRCLR_ON; // Serialize
while ( ( mcasp->regs->XGBLCTL & GBLCTL_XSRCLR_ON ) != GBLCTL_XSRCLR_ON );
mcasp->regs->RGBLCTL |= GBLCTL_RSRCLR_ON; // Serialize
while ( ( mcasp->regs->RGBLCTL & GBLCTL_RSRCLR_ON ) != GBLCTL_RSRCLR_ON );
// Write a 0, so that no underrun occurs after releasing the state machine
mcasp->regs->XBUF5= 0;
mcasp->regs->XGBLCTL |= GBLCTL_XSMRST_ON; // State Machine
while ( ( mcasp->regs->XGBLCTL & GBLCTL_XSMRST_ON ) != GBLCTL_XSMRST_ON );
mcasp->regs->RGBLCTL |= GBLCTL_RSMRST_ON; // State Machine
while ( ( mcasp->regs->RGBLCTL & GBLCTL_RSMRST_ON ) != GBLCTL_RSMRST_ON );
mcasp->regs->XGBLCTL |= GBLCTL_XFRST_ON; // Frame Sync
while ( ( mcasp->regs->XGBLCTL & GBLCTL_XFRST_ON ) != GBLCTL_XFRST_ON );
mcasp->regs->RGBLCTL |= GBLCTL_RFRST_ON; // Frame Sync
while ( ( mcasp->regs->RGBLCTL & GBLCTL_RFRST_ON ) != GBLCTL_RFRST_ON );
// Start by sending a dummy write
while( ! ( mcasp->regs->SRCTL5 & 0x10 ) ); // Check for Tx ready
mcasp->regs->XBUF5 = 0;
return 0;
}