This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCSTUDIO: Issue with Silent Installation of CCS

Part Number: CCSTUDIO

Hello,

During the silent installation of CCS, the following problem occurs:

The installation via PowerShell hangs at the end because the process 10544 (cmd.exe) remains active. Only after manually kill this process does the installation complete successfully.

Please find a screenshot attached for reference.


Could you kindly assist us in analyzing and resolving this issue?

Thank you in advance for your support.

Best regards,
Ali Tekagac
IT Application Administrator

  • Hi Ali,

    Few questions:

    1, What's your Windows version? 

    2. Was a new CCS install or a patch update? If update, what was the original CS version?

    3. What the exact command you used for this silent install?

    Also, please attach the install log ( ccs\install_logs\2025xxxxxxxx\ccs_install_12.8.1.00005.log)

    Thanks,

    Michael

  • Hi Michael,

     

    Here are the details you requested:

     

    Windows Version: Windows 10

    Installation Type: Initially a fresh installation to verify the package works, followed by an update from version 12.6.0.00008

    Silent Install Command: --mode unattended --install-BlackHawk true --install-Segger true

     

    Please let me know if you need any additional information.

    Best regards,

    Ali Tekagac

     

    Autoflug GmbH

     

    Ali Tekagac

    IT Application Administrator

     

     

    THINKING SAFETY5444.ccs_install_12.8.1.00005.log

  • Hi Ali,

    Is that log 5444.ccs_install_12.8.1.00005.log from the hanged installation? I hoped to see which individual component is responsible for the hang but in your log everything seems to be progressing normally.

    Also, did you try to switch to the Theia based CCS20.X versions?

    Michael

  • Log started 11/28/2025 at 13:07:17
    Preferred installation mode : win32
    Trying to init installer in mode win32
    Mode win32 successfully initialized
    [13:07:21] CCS_INFO: Installer timestamp 20251128130721
    [13:07:21] Installer arguments 
    [13:07:21] CCS_INFO: Initialization sets components_download_url to http://software-dl.ti.com/ccs/esd/CCSv20/CCS20.3.1.00005_win64/components
    Could not find registry key HKEY_LOCAL_MACHINE\SOFTWARE\Texas Instruments\CCS 20.3.1.00005 Version. Setting variable oldVersion to empty value
    [13:07:22] createshortcuts set to true
    [13:07:24] CCS_INFO: Temporary folder set to C:\Temp/ccs_37f90eb4-bfc1-4fd2-42f7-b40a0205b1e1
    [13:07:27] CCS_INFO: Components available: ARM_MPU_FEATURE_METADATA,AUTO_FEATURE_METADATA,BLACKHAWK_EMUPACK,C2000_FEATURE_METADATA,C29_FEATURE_METADATA,CC35XX_FEATURE_METADATA,CCS_DOC,CCS_UTILS,CGT_DEFAULTLIBS_C2800,CGT_DEFAULTLIBS_C29,CGT_DEFAULTLIBS_C6000_V8P,CGT_DEFAULTLIBS_C7000,CGT_DEFAULTLIBS_MSP430,CLOUDAGENT,DEV_SUPPORT_CC26XX,DEV_SUPPORT_CC3220,DEV_SUPPORT_CC3230,DEV_SUPPORT_CC32XX,DEV_SUPPORT_CC32XX_COMMON,DEV_SUPPOR_CC35XX,DS,DS_FLASH,ECLIPSE,EMU_C2000_FLASH,EMU_TI,IDE_METADATA,LPCS_FEATURE_METADATA,MMWAVE_FEATURE_METADATA,MSP430_HEADER,MSP430_HEADER_GCC,MSP430_SUPPORT,MSP432_BUILD_DEBUG,MSPM0_FEATURE_METADATA,MSPM33_FEATURE_METADATA,MSVC_REDIST_LATEST,NODEJS,PF_ARM_MPU,PF_AUTO,PF_C28,PF_C29,PF_C6000SC,PF_DIGITAL_POWER,PF_HERCULES,PF_MMWAVE,PF_MSP430,PF_MSP432,PF_MSPM0,PF_MSPM33,PF_OMAPL,PF_PGA,PF_SITARA_MCU,PF_SP_MCU,PF_TM4C,PF_TM4E,PF_UCDR,SEGGER_J_LINK,SEGGER_J_LINK_DRIVERS,SHARED_DEVICE_SUPPORT,SITARA_MCU_FEATURE_METADATA,SP_MCU_FEATURE_METADATA,SYSCONFIG,TARGETDB_DEF_PROPS,THEIA,TIREX,TIVA_STELLARIS_DRIVERS,TI_ARM_CLANG,UCDR_FEATURE_METADATA,YAROV
    [13:07:28] CCS_INFO: Components default folder is set to C:\Source\CCS_20.3.1.00005_win/components
    [13:07:28] CCS_INFO: Components override folder is set to C:\Source\CCS_20.3.1.00005_win/components
    [13:07:33] CCS_INFO: Anti-virus detected
    [13:07:42] Logdir = C:\ti\ccs2031/ccs/install_logs/20251128130721
    [13:07:42] CCS_INFO: CCStudio set to C:/ti/ccs2031/ccs/theia/ccstudio.exe
    [13:07:43] CCS_INFO: setting project.component(CCS_UTILS).selected to 0
    [13:07:43] CCS_INFO: setting project.component(TIREX).selected to 0
    [13:07:43] CCS_INFO: setting project.component(ECLIPSE).selected to 0
    [13:07:43] CCS_INFO: setting project.component(NODEJS).selected to 0
    [13:07:43] CCS_INFO: setting project.component(DS).selected to 0
    [13:07:43] CCS_INFO: setting project.component(DS_FLASH).selected to 0
    [13:07:43] CCS_INFO: setting project.component(CLOUDAGENT).selected to 0
    [13:07:43] CCS_INFO: setting project.component(SYSCONFIG).selected to 0
    [13:07:43] CCS_INFO: setting project.component(EMU_TI).selected to 0
    [13:07:43] CCS_INFO: setting project.component(TI_ARM_CLANG).selected to 0
    [13:07:43] CCS_INFO: setting project.component(CCS_DOC).selected to 0
    [13:07:43] CCS_INFO: setting project.component(TARGETDB_DEF_PROPS).selected to 0
    [13:07:43] CCS_INFO: setting project.component(YAROV).selected to 0
    [13:07:43] CCS_INFO: setting project.component(IDE_METADATA).selected to 0
    [13:07:43] CCS_INFO: setting project.component(SEGGER_J_LINK).selected to 0
    [13:07:43] CCS_INFO: setting project.component(CGT_DEFAULTLIBS_MSP430).selected to 0
    [13:07:43] CCS_INFO: setting project.component(CGT_DEFAULTLIBS_C2800).selected to 0
    [13:07:43] CCS_INFO: setting project.component(CGT_DEFAULTLIBS_C6000_V8P).selected to 0
    [13:07:43] CCS_INFO: setting project.component(CGT_DEFAULTLIBS_C29).selected to 0
    [13:07:43] CCS_INFO: setting project.component(CGT_DEFAULTLIBS_C7000).selected to 0
    [13:07:43] CCS_INFO: setting project.component(TIVA_STELLARIS_DRIVERS).selected to 0
    [13:07:43] CCS_INFO: setting project.component(THEIA).selected to 0
    [13:07:43] ECLIPSE NOTSET 20.3.0.202507301956
    [13:07:44] ECLIPSE selected: 1
    [13:07:44] ECLIPSE: Installed Version: NOTSET Current Version: 20.3.0.202507301956
    [13:07:44] DS NOTSET 20.3.0.3849
    [13:07:44] DS selected: 1
    [13:07:44] DS: Installed Version: NOTSET Current Version: 20.3.0.3849
    [13:07:44] DS_FLASH NOTSET 20.3.0.3849
    [13:07:44] DS_FLASH selected: 1
    [13:07:44] DS_FLASH: Installed Version: NOTSET Current Version: 20.3.0.3849
    [13:07:44] CLOUDAGENT NOTSET 0.5.5353
    [13:07:44] CLOUDAGENT selected: 1
    [13:07:44] CLOUDAGENT: Installed Version: NOTSET Current Version: 0.5.5353
    [13:07:44] EMU_TI NOTSET 20.3.0.3656
    [13:07:44] EMU_TI selected: 1
    [13:07:44] EMU_TI: Installed Version: NOTSET Current Version: 20.3.0.3656
    [13:07:44] NODEJS NOTSET 18.16.0
    [13:07:44] NODEJS selected: 1
    [13:07:44] NODEJS: Installed Version: NOTSET Current Version: 18.16.0
    [13:07:44] CCS_UTILS NOTSET 1.0.2.20250509
    [13:07:45] CCS_UTILS selected: 1
    [13:07:45] CCS_UTILS: Installed Version: NOTSET Current Version: 1.0.2.20250509
    [13:07:45] SYSCONFIG NOTSET 1.25.0.4268
    [13:07:45] SYSCONFIG selected: 1
    [13:07:45] SYSCONFIG: Installed Version: NOTSET Current Version: 1.25.0.4268
    [13:07:45] YAROV NOTSET 2.0.2
    [13:07:45] YAROV selected: 1
    [13:07:45] YAROV: Installed Version: NOTSET Current Version: 2.0.2
    [13:07:45] TARGETDB_DEF_PROPS NOTSET 12.3.0.N202303010900
    [13:07:45] TARGETDB_DEF_PROPS selected: 1
    [13:07:45] TARGETDB_DEF_PROPS: Installed Version: NOTSET Current Version: 12.3.0.N202303010900
    [13:07:45] TIREX NOTSET 4.20.0.202411191616
    [13:07:45] TIREX selected: 1
    [13:07:45] TIREX: Installed Version: NOTSET Current Version: 4.20.0.202411191616
    [13:07:45] TI_ARM_CLANG NOTSET 4.0.4.LTS
    [13:07:46] TI_ARM_CLANG selected: 1
    [13:07:46] TI_ARM_CLANG: Installed Version: NOTSET Current Version: 4.0.4.LTS
    [13:07:46] CCS_DOC NOTSET 20.3.1.00005
    [13:07:46] CCS_DOC selected: 1
    [13:07:46] CCS_DOC: Installed Version: NOTSET Current Version: 20.3.1.00005
    [13:07:46] IDE_METADATA NOTSET 1.9.1
    [13:07:46] IDE_METADATA selected: 1
    [13:07:46] IDE_METADATA: Installed Version: NOTSET Current Version: 1.9.1
    [13:07:46] SEGGER_J_LINK NOTSET 8.70.0
    [13:07:46] SEGGER_J_LINK selected: 1
    [13:07:46] SEGGER_J_LINK: Installed Version: NOTSET Current Version: 8.70.0
    [13:07:46] CGT_DEFAULTLIBS_MSP430 NOTSET 21.6.1.LTS
    [13:07:46] CGT_DEFAULTLIBS_MSP430 selected: 1
    [13:07:46] CGT_DEFAULTLIBS_MSP430: Installed Version: NOTSET Current Version: 21.6.1.LTS
    [13:07:46] CGT_DEFAULTLIBS_C2800 NOTSET 22.6.2.LTS
    [13:07:47] CGT_DEFAULTLIBS_C2800 selected: 1
    [13:07:47] CGT_DEFAULTLIBS_C2800: Installed Version: NOTSET Current Version: 22.6.2.LTS
    [13:07:47] CGT_DEFAULTLIBS_C6000_V8P NOTSET 8.5.0.LTS
    [13:07:47] CGT_DEFAULTLIBS_C6000_V8P selected: 1
    [13:07:47] CGT_DEFAULTLIBS_C6000_V8P: Installed Version: NOTSET Current Version: 8.5.0.LTS
    [13:07:47] CGT_DEFAULTLIBS_C29 NOTSET 2.0.0.STS
    [13:07:47] CGT_DEFAULTLIBS_C29 selected: 1
    [13:07:47] CGT_DEFAULTLIBS_C29: Installed Version: NOTSET Current Version: 2.0.0.STS
    [13:07:47] CGT_DEFAULTLIBS_C7000 NOTSET 5.0.0.LTS
    [13:07:47] CGT_DEFAULTLIBS_C7000 selected: 1
    [13:07:47] CGT_DEFAULTLIBS_C7000: Installed Version: NOTSET Current Version: 5.0.0.LTS
    [13:07:47] TIVA_STELLARIS_DRIVERS NOTSET 2.1.3.15
    [13:07:47] TIVA_STELLARIS_DRIVERS selected: 1
    [13:07:47] TIVA_STELLARIS_DRIVERS: Installed Version: NOTSET Current Version: 2.1.3.15
    [13:07:47] THEIA NOTSET 20.3.0.20250827212308
    [13:07:48] THEIA selected: 1
    [13:07:48] THEIA: Installed Version: NOTSET Current Version: 20.3.0.20250827212308
    [13:07:48] PF_MSPM0 selected: 1
    [13:07:48] PF_MSPM0: Installed Version: NOTSET Current Version: 1.16.0
    [13:07:48] PF_MSPM33 selected: 1
    [13:07:48] PF_MSPM33: Installed Version: NOTSET Current Version: 1.0.9
    [13:07:48] PF_MSP430 selected: 1
    [13:07:48] PF_MSP430: Installed Version: NOTSET Current Version: 11.1.0.20211104
    [13:07:49] PF_C28 selected: 1
    [13:07:49] PF_C28: Installed Version: NOTSET Current Version: 6.27.0
    [13:07:49] PF_WCONN selected: 1
    [13:07:49] PF_ARM_MPU selected: 1
    [13:07:49] PF_ARM_MPU: Installed Version: NOTSET Current Version: 1.6.10
    [13:07:49] PF_SITARA_MCU selected: 1
    [13:07:49] PF_SITARA_MCU: Installed Version: NOTSET Current Version: 1.5.0
    [13:07:49] PF_MMWAVE selected: 1
    [13:07:49] PF_MMWAVE: Installed Version: NOTSET Current Version: 1.7.19
    [13:07:50] PF_HERCULES selected: 1
    [13:07:50] PF_HERCULES: Installed Version: NOTSET Current Version: 6.0.9
    [13:07:50] PF_TM4C selected: 1
    [13:07:50] PF_TM4C: Installed Version: NOTSET Current Version: 2.1.1.15071
    [13:07:50] PF_C6000SC selected: 1
    [13:07:50] PF_C6000SC: Installed Version: NOTSET Current Version: 1.1.7
    [13:07:50] PF_OMAPL selected: 1
    [13:07:50] PF_OMAPL: Installed Version: NOTSET Current Version: 1.1.2
    [13:07:50] PF_MSP432 selected: 1
    [13:07:50] PF_MSP432: Installed Version: NOTSET Current Version: 8.2.2.0
    [13:07:51] PF_PGA selected: 1
    [13:07:51] PF_PGA: Installed Version: NOTSET Current Version: 1.0.2
    [13:07:51] PF_DIGITAL_POWER selected: 1
    [13:07:51] PF_DIGITAL_POWER: Installed Version: NOTSET Current Version: 1.1.5
    [13:07:51] PF_AUTO selected: 1
    [13:07:51] PF_AUTO: Installed Version: NOTSET Current Version: 1.1.18
    [13:07:51] MSVC_REDIST_LATEST NOTSET 14.38.33135
    [13:07:51] MSVC_REDIST_LATEST selected: 1}
    [13:07:51] SEGGER_J_LINK_DRIVERS NOTSET 1.0.1.0
    [13:07:52] SEGGER_J_LINK_DRIVERS selected: 1}
    [13:07:52] BLACKHAWK_EMUPACK NOTSET 9.0.0.002
    [13:07:52] BLACKHAWK_EMUPACK selected: 1}
    Preparing to Install
    [13:08:30] CCS_INFO: Components default url is set to http://software-dl.ti.com/ccs/esd/CCSv20/CCS20.3.1.00005_win64/components
    [13:08:30] CCS_INFO: Components download url is set to http://software-dl.ti.com/ccs/esd/CCSv20/CCS20.3.1.00005_win64/components
    [13:08:30] CCS_INFO: Starting installation
    [13:08:30] Install Version : 20.3.1.00005
    [13:08:30] Install Source  : C:/Source/CCS_20.3.1.00005_win
    [13:08:30] Install Temp    : C:/Temp/ccs_37f90eb4-bfc1-4fd2-42f7-b40a0205b1e1
    [13:08:30] Install Type    : Offline
    [13:08:30] OS              : Windows NT
    [13:08:30] OS Name         : Windows 10
    [13:08:30] OS Version      : 10.0 sp 0
    [13:08:30] OS  Platform    : windows-x64 64-bit
    [13:08:30] OSD             : Windows10-64-bit
    [13:08:30] User ID         : tekagac.admin
    [13:08:30] Timezone        : +0100
    [13:08:30] InstallTime(GMT): 11/28/2025 12:07:21(GMT) 
    [13:08:30] IPAddress       : 192.168.1.213
    [13:08:30] Update/Rerun    : false
    [13:08:30] Install GUID    : 37f90eb4-bfc1-4fd2-42f7-b40a0205b1e1
    [13:08:30] Command line    : 
    Setting variable proxyInfoTmp from C:\Temp/ccs_37f90eb4-bfc1-4fd2-42f7-b40a0205b1e1/util/lsproxy.exe http://www.google.com
    Script exit code: 0
    
    Script output:
     
    
    Script stderr:
     
    
    [13:08:31] CCS_INFO: Running ccs_monitor 6372 C:\Temp/mon_37f90eb4-bfc1-4fd2-42f7-b40a0205b1e1 http://software-dl.ti.com/ccs/esd/tia 
    Executing C:\Temp/mon_37f90eb4-bfc1-4fd2-42f7-b40a0205b1e1/util/ccs_monitor.bat 6372 "C:\Temp/mon_37f90eb4-bfc1-4fd2-42f7-b40a0205b1e1" http://software-dl.ti.com/ccs/esd/tia/CCS20.3.1.00005_windows-x64_ "" &
    Script exit code: 0
    
    Script output:
     
    
    Script stderr:
     
    
    [13:08:33] CCS_INFO: Downloading http://software-dl.ti.com/ccs/esd/tia/CCS20.3.1.00005_tia_windows-x64_start_offline.zip
    [13:08:34] CCS_INFO: Return values from downloadMarker http://software-dl.ti.com/ccs/esd/tia/CCS20.3.1.00005_tia_windows-x64_start_offline.zip: 404
    [13:08:34] CCS_INFO: Running install-certs.bat to pre-install driver certificates.
    Executing C:\Temp/ccs_37f90eb4-bfc1-4fd2-42f7-b40a0205b1e1/util/certificates/install-certs.bat 
    Script exit code: 0
    
    Script output:
     
    C:\Temp\ccs_37f90eb4-bfc1-4fd2-42f7-b40a0205b1e1\util\certificates>C:\Windows\system32\certutil.exe -addstore "TrustedPublisher" C:\Temp\CCS_37~1\util\CERTIF~1\\ewa1.p7b 
    TrustedPublisher "Vertrauenswürdige Herausgeber"
    Verwandte Zertifikate:
    
    Genaue Übereinstimmung:
    Element 13:
    Seriennummer: 655226e1b22e18e1590f2985ac22e75c
    Aussteller: OU=Class 3 Public Primary Certification Authority, O=VeriSign, Inc., C=US
     Nicht vor: 21.05.2009 01:00
     Nicht nach: 21.05.2019 00:59
    Antragsteller: CN=VeriSign Class 3 Code Signing 2009-2 CA, OU=Terms of use at https://www.verisign.com/rpa (c)09, OU=VeriSign Trust Network, O=VeriSign, Inc., C=US
    Kein Stammzertifikat
    Zertifikathash(sha1): 12d4872bc3ef019e7e0b6f132480ae29db5b1ca3
    
    Das Zertifikat "VeriSign Class 3 Code Signing 2009-2 CA" befindet sich bereits im Speicher.
    Signatur stimmt mit dem öffentlichen Schlüssel überein.
    Verwandte Zertifikate:
    
    Genaue Übereinstimmung:
    Element 6:
    Seriennummer: 70bae41d10d92934b638ca7b03ccbabf
    Aussteller: OU=Class 3 Public Primary Certification Authority, O=VeriSign, Inc., C=US
     Nicht vor: 29.01.1996 01:00
     Nicht nach: 02.08.2028 00:59
    Antragsteller: OU=Class 3 Public Primary Certification Authority, O=VeriSign, Inc., C=US
    Signatur stimmt mit dem öffentlichen Schlüssel überein.
    Stammzertifikat: Antragsteller stimmt mit Aussteller überein
    Zertifikathash(sha1): 742c3192e607e424eb4549542be1bbc53e6174e2
    
    Das Zertifikat "Class 3 Public Primary Certification Authority" befindet sich bereits im Speicher.
    Verwandte Zertifikate:
    
    Genaue Übereinstimmung:
    Element 11:
    Seriennummer: 5a27decb3e7f05e384eab0f1f0d11764
    Aussteller: CN=VeriSign Class 3 Code Signing 2009-2 CA, OU=Terms of use at https://www.verisign.com/rpa (c)09, OU=VeriSign Trust Network, O=VeriSign, Inc., C=US
     Nicht vor: 23.03.2010 01:00
     Nicht nach: 26.04.2011 00:59
    Antragsteller: CN=EWA Technologies, Inc., OU=Blackhawk, OU=Digital ID Class 3 - Microsoft Software Validation v2, O=EWA Technologies, Inc., L=Mount Laurel, S=New Jersey, C=US
    Kein Stammzertifikat
    Zertifikathash(sha1): 1d4adcd44ecf1b182c380f9e2a39e5c61bca6d83
    
    Das Zertifikat "EWA Technologies, Inc." befindet sich bereits im Speicher.
    CertUtil: -addstore-Befehl wurde erfolgreich ausgeführt.
    
    C:\Temp\ccs_37f90eb4-bfc1-4fd2-42f7-b40a0205b1e1\util\certificates>C:\Windows\system32\certutil.exe -addstore "TrustedPublisher" C:\Temp\CCS_37~1\util\CERTIF~1\\ewa2.p7b 
    TrustedPublisher "Vertrauenswürdige Herausgeber"
    Verwandte Zertifikate:
    
    Genaue Übereinstimmung:
    Element 10:
    Seriennummer: 5200e5aa2556fc1a86ed96c9d44b33c7
    Aussteller: CN=VeriSign Class 3 Public Primary Certification Authority - G5, OU=(c) 2006 VeriSign, Inc. - For authorized use only, OU=VeriSign Trust Network, O=VeriSign, Inc., C=US
     Nicht vor: 08.02.2010 01:00
     Nicht nach: 08.02.2020 00:59
    Antragsteller: CN=VeriSign Class 3 Code Signing 2010 CA, OU=Terms of use at https://www.verisign.com/rpa (c)10, OU=VeriSign Trust Network, O=VeriSign, Inc., C=US
    Kein Stammzertifikat
    Zertifikathash(sha1): 495847a93187cfb8c71f840cb7b41497ad95c64f
    
    Das Zertifikat "VeriSign Class 3 Code Signing 2010 CA" befindet sich bereits im Speicher.
    Signatur stimmt mit dem öffentlichen Schlüssel überein.
    Verwandte Zertifikate:
    
    Genaue Übereinstimmung:
    Element 9:
    Seriennummer: 18dad19e267de8bb4a2158cdcc6b3b4a
    Aussteller: CN=VeriSign Class 3 Public Primary Certification Authority - G5, OU=(c) 2006 VeriSign, Inc. - For authorized use only, OU=VeriSign Trust Network, O=VeriSign, Inc., C=US
     Nicht vor: 08.11.2006 01:00
     Nicht nach: 17.07.2036 00:59
    Antragsteller: CN=VeriSign Class 3 Public Primary Certification Authority - G5, OU=(c) 2006 VeriSign, Inc. - For authorized use only, OU=VeriSign Trust Network, O=VeriSign, Inc., C=US
    Signatur stimmt mit dem öffentlichen Schlüssel überein.
    Stammzertifikat: Antragsteller stimmt mit Aussteller überein
    Zertifikathash(sha1): 4eb6d578499b1ccf5f581ead56be3d9b6744a5e5
    
    Das Zertifikat "VeriSign Class 3 Public Primary Certification Authority - G5" befindet sich bereits im Speicher.
    Verwandte Zertifikate:
    
    Genaue Übereinstimmung:
    Element 7:
    Seriennummer: 7db731a79cdcb7a070905db1d0b25663
    Aussteller: CN=VeriSign Class 3 Code Signing 2010 CA, OU=Terms of use at https://www.verisign.com/rpa (c)10, OU=VeriSign Trust Network, O=VeriSign, Inc., C=US
     Nicht vor: 27.03.2011 01:00
     Nicht nach: 25.04.2012 00:59
    Antragsteller: CN=EWA Technologies, Inc., OU=Blackhawk, OU=Digital ID Class 3 - Microsoft Software Validation v2, O=EWA Technologies, Inc., L=Mount Laurel, S=New Jersey, C=US
    Kein Stammzertifikat
    Zertifikathash(sha1): 51924ab0175bfeca92812bc475b949ab0c00b27a
    
    Das Zertifikat "EWA Technologies, Inc." befindet sich bereits im Speicher.
    CertUtil: -addstore-Befehl wurde erfolgreich ausgeführt.
    
    C:\Temp\ccs_37f90eb4-bfc1-4fd2-42f7-b40a0205b1e1\util\certificates>C:\Windows\system32\certutil.exe -addstore "TrustedPublisher" C:\Temp\CCS_37~1\util\CERTIF~1\\ewa3.p7b 
    TrustedPublisher "Vertrauenswürdige Herausgeber"
    Verwandte Zertifikate:
    
    Genaue Übereinstimmung:
    Element 10:
    Seriennummer: 5200e5aa2556fc1a86ed96c9d44b33c7
    Aussteller: CN=VeriSign Class 3 Public Primary Certification Authority - G5, OU=(c) 2006 VeriSign, Inc. - For authorized use only, OU=VeriSign Trust Network, O=VeriSign, Inc., C=US
     Nicht vor: 08.02.2010 01:00
     Nicht nach: 08.02.2020 00:59
    Antragsteller: CN=VeriSign Class 3 Code Signing 2010 CA, OU=Terms of use at https://www.verisign.com/rpa (c)10, OU=VeriSign Trust Network, O=VeriSign, Inc., C=US
    Kein Stammzertifikat
    Zertifikathash(sha1): 495847a93187cfb8c71f840cb7b41497ad95c64f
    
    Das Zertifikat "VeriSign Class 3 Code Signing 2010 CA" befindet sich bereits im Speicher.
    Signatur stimmt mit dem öffentlichen Schlüssel überein.
    Verwandte Zertifikate:
    
    Genaue Übereinstimmung:
    Element 9:
    Seriennummer: 18dad19e267de8bb4a2158cdcc6b3b4a
    Aussteller: CN=VeriSign Class 3 Public Primary Certification Authority - G5, OU=(c) 2006 VeriSign, Inc. - For authorized use only, OU=VeriSign Trust Network, O=VeriSign, Inc., C=US
     Nicht vor: 08.11.2006 01:00
     Nicht nach: 17.07.2036 00:59
    Antragsteller: CN=VeriSign Class 3 Public Primary Certification Authority - G5, OU=(c) 2006 VeriSign, Inc. - For authorized use only, OU=VeriSign Trust Network, O=VeriSign, Inc., C=US
    Signatur stimmt mit dem öffentlichen Schlüssel überein.
    Stammzertifikat: Antragsteller stimmt mit Aussteller überein
    Zertifikathash(sha1): 4eb6d578499b1ccf5f581ead56be3d9b6744a5e5
    
    Das Zertifikat "VeriSign Class 3 Public Primary Certification Authority - G5" befindet sich bereits im Speicher.
    Verwandte Zertifikate:
    
    Genaue Übereinstimmung:
    Element 14:
    Seriennummer: 60cedd5bcb8f3f2e8c7ae62ab9f6bcf3
    Aussteller: CN=VeriSign Class 3 Code Signing 2010 CA, OU=Terms of use at https://www.verisign.com/rpa (c)10, OU=VeriSign Trust Network, O=VeriSign, Inc., C=US
     Nicht vor: 27.03.2012 01:00
     Nicht nach: 25.04.2013 00:59
    Antragsteller: CN=EWA Technologies, Inc., OU=Blackhawk, OU=Digital ID Class 3 - Microsoft Software Validation v2, O=EWA Technologies, Inc., L=Mount Laurel, S=New Jersey, C=US
    Kein Stammzertifikat
    Zertifikathash(sha1): 10fcb6f91153ef02cfe71a0ad1359795b57e9baf
    
    Das Zertifikat "EWA Technologies, Inc." befindet sich bereits im Speicher.
    CertUtil: -addstore-Befehl wurde erfolgreich ausgeführt.
    
    C:\Temp\ccs_37f90eb4-bfc1-4fd2-42f7-b40a0205b1e1\util\certificates>C:\Windows\system32\certutil.exe -addstore "TrustedPublisher" C:\Temp\CCS_37~1\util\CERTIF~1\\ewa4.p7b 
    TrustedPublisher "Vertrauenswürdige Herausgeber"
    Verwandte Zertifikate:
    
    Genaue Übereinstimmung:
    Element 10:
    Seriennummer: 5200e5aa2556fc1a86ed96c9d44b33c7
    Aussteller: CN=VeriSign Class 3 Public Primary Certification Authority - G5, OU=(c) 2006 VeriSign, Inc. - For authorized use only, OU=VeriSign Trust Network, O=VeriSign, Inc., C=US
     Nicht vor: 08.02.2010 01:00
     Nicht nach: 08.02.2020 00:59
    Antragsteller: CN=VeriSign Class 3 Code Signing 2010 CA, OU=Terms of use at https://www.verisign.com/rpa (c)10, OU=VeriSign Trust Network, O=VeriSign, Inc., C=US
    Kein Stammzertifikat
    Zertifikathash(sha1): 495847a93187cfb8c71f840cb7b41497ad95c64f
    
    Das Zertifikat "VeriSign Class 3 Code Signing 2010 CA" befindet sich bereits im Speicher.
    Signatur stimmt mit dem öffentlichen Schlüssel überein.
    Verwandte Zertifikate:
    
    Genaue Übereinstimmung:
    Element 9:
    Seriennummer: 18dad19e267de8bb4a2158cdcc6b3b4a
    Aussteller: CN=VeriSign Class 3 Public Primary Certification Authority - G5, OU=(c) 2006 VeriSign, Inc. - For authorized use only, OU=VeriSign Trust Network, O=VeriSign, Inc., C=US
     Nicht vor: 08.11.2006 01:00
     Nicht nach: 17.07.2036 00:59
    Antragsteller: CN=VeriSign Class 3 Public Primary Certification Authority - G5, OU=(c) 2006 VeriSign, Inc. - For authorized use only, OU=VeriSign Trust Network, O=VeriSign, Inc., C=US
    Signatur stimmt mit dem öffentlichen Schlüssel überein.
    Stammzertifikat: Antragsteller stimmt mit Aussteller überein
    Zertifikathash(sha1): 4eb6d578499b1ccf5f581ead56be3d9b6744a5e5
    
    Das Zertifikat "VeriSign Class 3 Public Primary Certification Authority - G5" befindet sich bereits im Speicher.
    Verwandte Zertifikate:
    
    Genaue Übereinstimmung:
    Element 4:
    Seriennummer: 2d895bb38dcba4e8df667fb7cebb29f7
    Aussteller: CN=VeriSign Class 3 Code Signing 2010 CA, OU=Terms of use at https://www.verisign.com/rpa (c)10, OU=VeriSign Trust Network, O=VeriSign, Inc., C=US
     Nicht vor: 04.04.2013 01:00
     Nicht nach: 05.07.2014 00:59
    Antragsteller: CN=EWA TECHNOLOGIES, INC., OU=Blackhawk, OU=Digital ID Class 3 - Microsoft Software Validation v2, O=EWA TECHNOLOGIES, INC., L=Mount Laurel, S=New Jersey, C=US
    Kein Stammzertifikat
    Zertifikathash(sha1): b82dbed803d99e9d6240cd2318286fd2ce9c480c
    
    Das Zertifikat "EWA TECHNOLOGIES, INC." befindet sich bereits im Speicher.
    CertUtil: -addstore-Befehl wurde erfolgreich ausgeführt.
    
    C:\Temp\ccs_37f90eb4-bfc1-4fd2-42f7-b40a0205b1e1\util\certificates>C:\Windows\system32\certutil.exe -addstore "TrustedPublisher" C:\Temp\CCS_37~1\util\CERTIF~1\\ti1.p7b 
    TrustedPublisher "Vertrauenswürdige Herausgeber"
    Verwandte Zertifikate:
    
    Genaue Übereinstimmung:
    Element 10:
    Seriennummer: 5200e5aa2556fc1a86ed96c9d44b33c7
    Aussteller: CN=VeriSign Class 3 Public Primary Certification Authority - G5, OU=(c) 2006 VeriSign, Inc. - For authorized use only, OU=VeriSign Trust Network, O=VeriSign, Inc., C=US
     Nicht vor: 08.02.2010 01:00
     Nicht nach: 08.02.2020 00:59
    Antragsteller: CN=VeriSign Class 3 Code Signing 2010 CA, OU=Terms of use at https://www.verisign.com/rpa (c)10, OU=VeriSign Trust Network, O=VeriSign, Inc., C=US
    Kein Stammzertifikat
    Zertifikathash(sha1): 495847a93187cfb8c71f840cb7b41497ad95c64f
    
    Das Zertifikat "VeriSign Class 3 Code Signing 2010 CA" befindet sich bereits im Speicher.
    Signatur stimmt mit dem öffentlichen Schlüssel überein.
    Verwandte Zertifikate:
    
    Genaue Übereinstimmung:
    Element 9:
    Seriennummer: 18dad19e267de8bb4a2158cdcc6b3b4a
    Aussteller: CN=VeriSign Class 3 Public Primary Certification Authority - G5, OU=(c) 2006 VeriSign, Inc. - For authorized use only, OU=VeriSign Trust Network, O=VeriSign, Inc., C=US
     Nicht vor: 08.11.2006 01:00
     Nicht nach: 17.07.2036 00:59
    Antragsteller: CN=VeriSign Class 3 Public Primary Certification Authority - G5, OU=(c) 2006 VeriSign, Inc. - For authorized use only, OU=VeriSign Trust Network, O=VeriSign, Inc., C=US
    Signatur stimmt mit dem öffentlichen Schlüssel überein.
    Stammzertifikat: Antragsteller stimmt mit Aussteller überein
    Zertifikathash(sha1): 4eb6d578499b1ccf5f581ead56be3d9b6744a5e5
    
    Das Zertifikat "VeriSign Class 3 Public Primary Certification Authority - G5" befindet sich bereits im Speicher.
    Verwandte Zertifikate:
    
    Genaue Übereinstimmung:
    Element 8:
    Seriennummer: 7ba5aab20f054f4560dedc8991e62a27
    Aussteller: CN=VeriSign Class 3 Code Signing 2010 CA, OU=Terms of use at https://www.verisign.com/rpa (c)10, OU=VeriSign Trust Network, O=VeriSign, Inc., C=US
     Nicht vor: 25.07.2012 01:00
     Nicht nach: 26.07.2013 00:59
    Antragsteller: CN=Texas Instruments Incorporated, OU=Digital ID Class 3 - Microsoft Software Validation v2, O=Texas Instruments Incorporated, L=Dallas, S=Texas, C=US
    Kein Stammzertifikat
    Zertifikathash(sha1): 50fcdbea5930e04e0ced6746715f2380ec6d03a9
    
    Das Zertifikat "Texas Instruments Incorporated" befindet sich bereits im Speicher.
    CertUtil: -addstore-Befehl wurde erfolgreich ausgeführt.
    
    C:\Temp\ccs_37f90eb4-bfc1-4fd2-42f7-b40a0205b1e1\util\certificates>C:\Windows\system32\certutil.exe -addstore "TrustedPublisher" C:\Temp\CCS_37~1\util\CERTIF~1\\ti2.p7b 
    TrustedPublisher "Vertrauenswürdige Herausgeber"
    Verwandte Zertifikate:
    
    Genaue Übereinstimmung:
    Element 10:
    Seriennummer: 5200e5aa2556fc1a86ed96c9d44b33c7
    Aussteller: CN=VeriSign Class 3 Public Primary Certification Authority - G5, OU=(c) 2006 VeriSign, Inc. - For authorized use only, OU=VeriSign Trust Network, O=VeriSign, Inc., C=US
     Nicht vor: 08.02.2010 01:00
     Nicht nach: 08.02.2020 00:59
    Antragsteller: CN=VeriSign Class 3 Code Signing 2010 CA, OU=Terms of use at https://www.verisign.com/rpa (c)10, OU=VeriSign Trust Network, O=VeriSign, Inc., C=US
    Kein Stammzertifikat
    Zertifikathash(sha1): 495847a93187cfb8c71f840cb7b41497ad95c64f
    
    Das Zertifikat "VeriSign Class 3 Code Signing 2010 CA" befindet sich bereits im Speicher.
    Signatur stimmt mit dem öffentlichen Schlüssel überein.
    Verwandte Zertifikate:
    
    Genaue Übereinstimmung:
    Element 9:
    Seriennummer: 18dad19e267de8bb4a2158cdcc6b3b4a
    Aussteller: CN=VeriSign Class 3 Public Primary Certification Authority - G5, OU=(c) 2006 VeriSign, Inc. - For authorized use only, OU=VeriSign Trust Network, O=VeriSign, Inc., C=US
     Nicht vor: 08.11.2006 01:00
     Nicht nach: 17.07.2036 00:59
    Antragsteller: CN=VeriSign Class 3 Public Primary Certification Authority - G5, OU=(c) 2006 VeriSign, Inc. - For authorized use only, OU=VeriSign Trust Network, O=VeriSign, Inc., C=US
    Signatur stimmt mit dem öffentlichen Schlüssel überein.
    Stammzertifikat: Antragsteller stimmt mit Aussteller überein
    Zertifikathash(sha1): 4eb6d578499b1ccf5f581ead56be3d9b6744a5e5
    
    Das Zertifikat "VeriSign Class 3 Public Primary Certification Authority - G5" befindet sich bereits im Speicher.
    Verwandte Zertifikate:
    
    Genaue Übereinstimmung:
    Element 3:
    Seriennummer: 1124ac88d0430481e0eaa40ef04118a9
    Aussteller: CN=VeriSign Class 3 Code Signing 2010 CA, OU=Terms of use at https://www.verisign.com/rpa (c)10, OU=VeriSign Trust Network, O=VeriSign, Inc., C=US
     Nicht vor: 04.10.2011 01:00
     Nicht nach: 04.10.2012 00:59
    Antragsteller: CN=Texas Instruments Inc, OU=Stellaris MCU, OU=Digital ID Class 3 - Microsoft Software Validation v2, O=Texas Instruments Inc, L=Austin, S=Texas, C=US
    Kein Stammzertifikat
    Zertifikathash(sha1): bcccf26267cee6b58b3818782d26f4307bcb6a4f
    
    Das Zertifikat "Texas Instruments Inc" befindet sich bereits im Speicher.
    CertUtil: -addstore-Befehl wurde erfolgreich ausgeführt.
    
    C:\Temp\ccs_37f90eb4-bfc1-4fd2-42f7-b40a0205b1e1\util\certificates>C:\Windows\system32\certutil.exe -addstore "TrustedPublisher" C:\Temp\CCS_37~1\util\CERTIF~1\\ti3.p7b 
    TrustedPublisher "Vertrauenswürdige Herausgeber"
    Verwandte Zertifikate:
    
    Genaue Übereinstimmung:
    Element 10:
    Seriennummer: 5200e5aa2556fc1a86ed96c9d44b33c7
    Aussteller: CN=VeriSign Class 3 Public Primary Certification Authority - G5, OU=(c) 2006 VeriSign, Inc. - For authorized use only, OU=VeriSign Trust Network, O=VeriSign, Inc., C=US
     Nicht vor: 08.02.2010 01:00
     Nicht nach: 08.02.2020 00:59
    Antragsteller: CN=VeriSign Class 3 Code Signing 2010 CA, OU=Terms of use at https://www.verisign.com/rpa (c)10, OU=VeriSign Trust Network, O=VeriSign, Inc., C=US
    Kein Stammzertifikat
    Zertifikathash(sha1): 495847a93187cfb8c71f840cb7b41497ad95c64f
    
    Das Zertifikat "VeriSign Class 3 Code Signing 2010 CA" befindet sich bereits im Speicher.
    Signatur stimmt mit dem öffentlichen Schlüssel überein.
    Verwandte Zertifikate:
    
    Genaue Übereinstimmung:
    Element 9:
    Seriennummer: 18dad19e267de8bb4a2158cdcc6b3b4a
    Aussteller: CN=VeriSign Class 3 Public Primary Certification Authority - G5, OU=(c) 2006 VeriSign, Inc. - For authorized use only, OU=VeriSign Trust Network, O=VeriSign, Inc., C=US
     Nicht vor: 08.11.2006 01:00
     Nicht nach: 17.07.2036 00:59
    Antragsteller: CN=VeriSign Class 3 Public Primary Certification Authority - G5, OU=(c) 2006 VeriSign, Inc. - For authorized use only, OU=VeriSign Trust Network, O=VeriSign, Inc., C=US
    Signatur stimmt mit dem öffentlichen Schlüssel überein.
    Stammzertifikat: Antragsteller stimmt mit Aussteller überein
    Zertifikathash(sha1): 4eb6d578499b1ccf5f581ead56be3d9b6744a5e5
    
    Das Zertifikat "VeriSign Class 3 Public Primary Certification Authority - G5" befindet sich bereits im Speicher.
    Verwandte Zertifikate:
    
    Genaue Übereinstimmung:
    Element 2:
    Seriennummer: 558c8cedb57ce54fa6fb351fb84b222f
    Aussteller: CN=VeriSign Class 3 Code Signing 2010 CA, OU=Terms of use at https://www.verisign.com/rpa (c)10, OU=VeriSign Trust Network, O=VeriSign, Inc., C=US
     Nicht vor: 15.04.2014 01:00
     Nicht nach: 17.04.2015 00:59
    Antragsteller: CN=Texas Instruments, OU=WCS, O=Texas Instruments, L=Dallas, S=Texas, C=US
    Kein Stammzertifikat
    Zertifikathash(sha1): c76e488afc115ad09da669cbe413316fe56e9438
    
    Das Zertifikat "Texas Instruments" befindet sich bereits im Speicher.
    CertUtil: -addstore-Befehl wurde erfolgreich ausgeführt.
    
    C:\Temp\ccs_37f90eb4-bfc1-4fd2-42f7-b40a0205b1e1\util\certificates>C:\Windows\system32\certutil.exe -addstore "TrustedPublisher" C:\Temp\CCS_37~1\util\CERTIF~1\\ti4.p7b 
    TrustedPublisher "Vertrauenswürdige Herausgeber"
    Verwandte Zertifikate:
    
    Genaue Übereinstimmung:
    Element 10:
    Seriennummer: 5200e5aa2556fc1a86ed96c9d44b33c7
    Aussteller: CN=VeriSign Class 3 Public Primary Certification Authority - G5, OU=(c) 2006 VeriSign, Inc. - For authorized use only, OU=VeriSign Trust Network, O=VeriSign, Inc., C=US
     Nicht vor: 08.02.2010 01:00
     Nicht nach: 08.02.2020 00:59
    Antragsteller: CN=VeriSign Class 3 Code Signing 2010 CA, OU=Terms of use at https://www.verisign.com/rpa (c)10, OU=VeriSign Trust Network, O=VeriSign, Inc., C=US
    Kein Stammzertifikat
    Zertifikathash(sha1): 495847a93187cfb8c71f840cb7b41497ad95c64f
    
    Das Zertifikat "VeriSign Class 3 Code Signing 2010 CA" befindet sich bereits im Speicher.
    Signatur stimmt mit dem öffentlichen Schlüssel überein.
    Verwandte Zertifikate:
    
    Genaue Übereinstimmung:
    Element 9:
    Seriennummer: 18dad19e267de8bb4a2158cdcc6b3b4a
    Aussteller: CN=VeriSign Class 3 Public Primary Certification Authority - G5, OU=(c) 2006 VeriSign, Inc. - For authorized use only, OU=VeriSign Trust Network, O=VeriSign, Inc., C=US
     Nicht vor: 08.11.2006 01:00
     Nicht nach: 17.07.2036 00:59
    Antragsteller: CN=VeriSign Class 3 Public Primary Certification Authority - G5, OU=(c) 2006 VeriSign, Inc. - For authorized use only, OU=VeriSign Trust Network, O=VeriSign, Inc., C=US
    Signatur stimmt mit dem öffentlichen Schlüssel überein.
    Stammzertifikat: Antragsteller stimmt mit Aussteller überein
    Zertifikathash(sha1): 4eb6d578499b1ccf5f581ead56be3d9b6744a5e5
    
    Das Zertifikat "VeriSign Class 3 Public Primary Certification Authority - G5" befindet sich bereits im Speicher.
    Verwandte Zertifikate:
    
    Genaue Übereinstimmung:
    Element 0:
    Seriennummer: 39ad63d2f5c9efdc46d734ae5e381b8f
    Aussteller: CN=VeriSign Class 3 Code Signing 2010 CA, OU=Terms of use at https://www.verisign.com/rpa (c)10, OU=VeriSign Trust Network, O=VeriSign, Inc., C=US
     Nicht vor: 26.02.2014 01:00
     Nicht nach: 26.02.2017 00:59
    Antragsteller: CN=Texas Instruments Incorporated, OU=Digital ID Class 3 - Microsoft Software Validation v2, O=Texas Instruments Incorporated, L=Dallas, S=Texas, C=US
    Kein Stammzertifikat
    Zertifikathash(sha1): ee0c8ba018ce926432c3cc23523a34073d01954a
    
    Das Zertifikat "Texas Instruments Incorporated" befindet sich bereits im Speicher.
    CertUtil: -addstore-Befehl wurde erfolgreich ausgeführt.
    
    C:\Temp\ccs_37f90eb4-bfc1-4fd2-42f7-b40a0205b1e1\util\certificates>C:\Windows\system32\certutil.exe -addstore "TrustedPublisher" C:\Temp\CCS_37~1\util\CERTIF~1\\msp_704.p7b 
    TrustedPublisher "Vertrauenswürdige Herausgeber"
    Verwandte Zertifikate:
    
    Genaue Übereinstimmung:
    Element 10:
    Seriennummer: 5200e5aa2556fc1a86ed96c9d44b33c7
    Aussteller: CN=VeriSign Class 3 Public Primary Certification Authority - G5, OU=(c) 2006 VeriSign, Inc. - For authorized use only, OU=VeriSign Trust Network, O=VeriSign, Inc., C=US
     Nicht vor: 08.02.2010 01:00
     Nicht nach: 08.02.2020 00:59
    Antragsteller: CN=VeriSign Class 3 Code Signing 2010 CA, OU=Terms of use at https://www.verisign.com/rpa (c)10, OU=VeriSign Trust Network, O=VeriSign, Inc., C=US
    Kein Stammzertifikat
    Zertifikathash(sha1): 495847a93187cfb8c71f840cb7b41497ad95c64f
    
    Das Zertifikat "VeriSign Class 3 Code Signing 2010 CA" befindet sich bereits im Speicher.
    Signatur stimmt mit dem öffentlichen Schlüssel überein.
    Verwandte Zertifikate:
    
    Genaue Übereinstimmung:
    Element 9:
    Seriennummer: 18dad19e267de8bb4a2158cdcc6b3b4a
    Aussteller: CN=VeriSign Class 3 Public Primary Certification Authority - G5, OU=(c) 2006 VeriSign, Inc. - For authorized use only, OU=VeriSign Trust Network, O=VeriSign, Inc., C=US
     Nicht vor: 08.11.2006 01:00
     Nicht nach: 17.07.2036 00:59
    Antragsteller: CN=VeriSign Class 3 Public Primary Certification Authority - G5, OU=(c) 2006 VeriSign, Inc. - For authorized use only, OU=VeriSign Trust Network, O=VeriSign, Inc., C=US
    Signatur stimmt mit dem öffentlichen Schlüssel überein.
    Stammzertifikat: Antragsteller stimmt mit Aussteller überein
    Zertifikathash(sha1): 4eb6d578499b1ccf5f581ead56be3d9b6744a5e5
    
    Das Zertifikat "VeriSign Class 3 Public Primary Certification Authority - G5" befindet sich bereits im Speicher.
    Verwandte Zertifikate:
    
    Genaue Übereinstimmung:
    Element 0:
    Seriennummer: 39ad63d2f5c9efdc46d734ae5e381b8f
    Aussteller: CN=VeriSign Class 3 Code Signing 2010 CA, OU=Terms of use at https://www.verisign.com/rpa (c)10, OU=VeriSign Trust Network, O=VeriSign, Inc., C=US
     Nicht vor: 26.02.2014 01:00
     Nicht nach: 26.02.2017 00:59
    Antragsteller: CN=Texas Instruments Incorporated, OU=Digital ID Class 3 - Microsoft Software Validation v2, O=Texas Instruments Incorporated, L=Dallas, S=Texas, C=US
    Kein Stammzertifikat
    Zertifikathash(sha1): ee0c8ba018ce926432c3cc23523a34073d01954a
    
    Das Zertifikat "Texas Instruments Incorporated" befindet sich bereits im Speicher.
    CertUtil: -addstore-Befehl wurde erfolgreich ausgeführt.
    
    Script stderr:
     
    
    [13:08:36] CCS_INFO: Components:
    [13:08:36] CCS_INFO: BLACKHAWK_EMUPACK: 1
    [13:08:36] CCS_INFO: CCS_DOC: 1
    [13:08:36] CCS_INFO: CCS_UTILS: 1
    [13:08:36] CCS_INFO: CGT_DEFAULTLIBS_C2800: 1
    [13:08:36] CCS_INFO: CGT_DEFAULTLIBS_C29: 1
    [13:08:36] CCS_INFO: CGT_DEFAULTLIBS_C6000_V8P: 1
    [13:08:36] CCS_INFO: CGT_DEFAULTLIBS_C7000: 1
    [13:08:36] CCS_INFO: CGT_DEFAULTLIBS_MSP430: 1
    [13:08:36] CCS_INFO: CLOUDAGENT: 1
    [13:08:37] CCS_INFO: DS: 1
    [13:08:37] CCS_INFO: DS_FLASH: 1
    [13:08:37] CCS_INFO: ECLIPSE: 1
    [13:08:37] CCS_INFO: EMU_TI: 1
    [13:08:37] CCS_INFO: IDE_METADATA: 1
    [13:08:37] CCS_INFO: MSVC_REDIST_LATEST: 1
    [13:08:37] CCS_INFO: NODEJS: 1
    [13:08:37] CCS_INFO: PF_ARM_MPU: 1
    [13:08:37] CCS_INFO: PF_AUTO: 1
    [13:08:37] CCS_INFO: PF_C28: 1
    [13:08:37] CCS_INFO: PF_C6000SC: 1
    [13:08:37] CCS_INFO: PF_DIGITAL_POWER: 1
    [13:08:37] CCS_INFO: PF_HERCULES: 1
    [13:08:37] CCS_INFO: PF_MMWAVE: 1
    [13:08:37] CCS_INFO: PF_MSP430: 1
    [13:08:37] CCS_INFO: PF_MSP432: 1
    [13:08:37] CCS_INFO: PF_MSPM0: 1
    [13:08:37] CCS_INFO: PF_MSPM33: 1
    [13:08:37] CCS_INFO: PF_OMAPL: 1
    [13:08:37] CCS_INFO: PF_PGA: 1
    [13:08:37] CCS_INFO: PF_SITARA_MCU: 1
    [13:08:37] CCS_INFO: PF_TM4C: 1
    [13:08:37] CCS_INFO: SEGGER_J_LINK: 1
    [13:08:37] CCS_INFO: SEGGER_J_LINK_DRIVERS: 1
    [13:08:37] CCS_INFO: SYSCONFIG: 1
    [13:08:37] CCS_INFO: TARGETDB_DEF_PROPS: 1
    [13:08:37] CCS_INFO: THEIA: 1
    [13:08:37] CCS_INFO: TIREX: 1
    [13:08:37] CCS_INFO: TIVA_STELLARIS_DRIVERS: 1
    [13:08:37] CCS_INFO: TI_ARM_CLANG: 1
    [13:08:37] CCS_INFO: YAROV: 1
    [13:08:37] CCS_INFO: rerun/update: false
    Preparing to Install
    Unpacking files
    [13:09:13] CCS_INFO: Done installing THEIA
    Unpacking files
    [13:09:32] CCS_INFO: Done installing Eclipse
    Unpacking files
    [13:09:34] CCS_INFO: Installing DS
    [13:09:34] showprogress = false
    [13:09:34] CCS_INFO: Installing C:/Temp/ccs_37f90eb4-bfc1-4fd2-42f7-b40a0205b1e1/DS/ti_dspack_ibsetup_x64_20.3.0.3849.exe
    [13:09:34] CCS_INFO: Actual executable C:/Temp/ccs_37f90eb4-bfc1-4fd2-42f7-b40a0205b1e1/DS/ti_dspack_ibsetup_x64_20.3.0.3849.exe
    Executing C:/Temp/ccs_37f90eb4-bfc1-4fd2-42f7-b40a0205b1e1/DS/ti_dspack_ibsetup_x64_20.3.0.3849.exe --prefix "C:\ti\ccs2031/ccs" --eclipseprefix "C:/ti/ccs2031/ccs/eclipse" --mode unattended   --installer-log "C:\ti\ccs2031/ccs/install_logs/20251128130721"  
    Script exit code: 0
    
    Script output:
     
    
    Script stderr:
     
    
    [13:10:17] CCS_INFO: Done installing executable DS C:/Temp/ccs_37f90eb4-bfc1-4fd2-42f7-b40a0205b1e1/DS/ti_dspack_ibsetup_x64_20.3.0.3849.exe
    Unpacking files
    [13:10:20] CCS_INFO: Done installing DS_FLASH
    Unpacking files
    [13:13:25] CCS_INFO: Done installing CLOUDAGENT
    Unpacking files
    [13:13:27] CCS_INFO: Installing EMU_TI
    [13:13:27] showprogress = false
    [13:13:27] CCS_INFO: Installing C:/Temp/ccs_37f90eb4-bfc1-4fd2-42f7-b40a0205b1e1/EMU_TI/ti_emupack_setup_20.3.0.3656_win_64.exe
    [13:13:27] CCS_INFO: Actual executable C:/Temp/ccs_37f90eb4-bfc1-4fd2-42f7-b40a0205b1e1/EMU_TI/ti_emupack_setup_20.3.0.3656_win_64.exe
    Executing C:/Temp/ccs_37f90eb4-bfc1-4fd2-42f7-b40a0205b1e1/EMU_TI/ti_emupack_setup_20.3.0.3656_win_64.exe --prefix "C:\ti\ccs2031/ccs" --eclipseprefix "C:/ti/ccs2031/ccs/eclipse" --mode unattended   --installer-log "C:\ti\ccs2031/ccs/install_logs/20251128130721"  --installdrivers true --enable-components c2800,arm,xds100,xds2xx,xds560,c6000 --disable-components c5500,omap,davinci,scripting,doc
    Script exit code: 0
    
    Script output:
     
    
    Script stderr:
     
    
    [13:15:25] CCS_INFO: Done installing executable EMU_TI C:/Temp/ccs_37f90eb4-bfc1-4fd2-42f7-b40a0205b1e1/EMU_TI/ti_emupack_setup_20.3.0.3656_win_64.exe
    Unpacking files
    [13:15:27] CCS_INFO: Done installing NODEJS
    Unpacking files
    [13:15:29] CCS_INFO: Done installing CCS_UTILS
    Unpacking files
    [13:16:07] CCS_INFO: Done installing SYSCONFIG
    Unpacking files
    [13:16:08] CCS_INFO: Installing MSVC_REDIST_LATEST 14.38.33135
    Executing C:\Temp/ccs_37f90eb4-bfc1-4fd2-42f7-b40a0205b1e1/MSVC_REDIST_LATEST/VC_redist.x64_14.38.33135.exe  /q /l "C:\ti\ccs2031/ccs/install_logs/20251128130721/MSVC_REDIST_LATEST.log" /norestart 
    Script exit code: 0
    
    Script output:
     
    
    Script stderr:
     
    
    [13:16:10] CCS_INFO: Done installing MSVC_REDIST_LATEST
    Unpacking files
    [13:16:10] CCS_INFO: Done installing YAROV
    Unpacking files
    [13:16:11] CCS_INFO: Done installing TARGETDB_DEF_PROPS
    Unpacking files
    [13:18:01] CCS_INFO: Done installing TIREX
    Unpacking files
    [13:18:04] CCS_INFO: Installing TI_ARM_CLANG
    [13:18:04] showprogress = false
    [13:18:04] CCS_INFO: Installing C:/Temp/ccs_37f90eb4-bfc1-4fd2-42f7-b40a0205b1e1/TI_ARM_CLANG/ti_cgt_armllvm_4.0.4.LTS_windows-x64_installer.exe
    [13:18:04] CCS_INFO: Actual executable C:/Temp/ccs_37f90eb4-bfc1-4fd2-42f7-b40a0205b1e1/TI_ARM_CLANG/ti_cgt_armllvm_4.0.4.LTS_windows-x64_installer.exe
    Executing C:/Temp/ccs_37f90eb4-bfc1-4fd2-42f7-b40a0205b1e1/TI_ARM_CLANG/ti_cgt_armllvm_4.0.4.LTS_windows-x64_installer.exe --prefix "C:\ti\ccs2031/ccs" --eclipseprefix "C:/ti/ccs2031/ccs/eclipse" --mode unattended   --installer-log "C:\ti\ccs2031/ccs/install_logs/20251128130721" --ccs true 
    Script exit code: 0
    
    Script output:
     
    
    Script stderr:
     
    
    [13:19:03] CCS_INFO: Done installing executable TI_ARM_CLANG C:/Temp/ccs_37f90eb4-bfc1-4fd2-42f7-b40a0205b1e1/TI_ARM_CLANG/ti_cgt_armllvm_4.0.4.LTS_windows-x64_installer.exe
    Unpacking files
    [13:19:04] CCS_INFO: Done installing CCS_DOC
    Unpacking files
    [13:19:04] CCS_INFO: Done installing IDE_METADATA
    Unpacking files
    [13:19:06] CCS_INFO: Done installing SEGGER_J_LINK
    Unpacking files
    [13:19:07] CCS_INFO: Installing SEGGER_J_LINK_DRIVERS
    [13:19:07] showprogress = false
    [13:19:07] CCS_INFO: Installing C:/Temp/ccs_37f90eb4-bfc1-4fd2-42f7-b40a0205b1e1/SEGGER_J_LINK_DRIVERS/JLinkDriver_setup_1.0.1.0.exe
    [13:19:07] CCS_INFO: Actual executable C:/Temp/ccs_37f90eb4-bfc1-4fd2-42f7-b40a0205b1e1/SEGGER_J_LINK_DRIVERS/JLinkDriver_setup_1.0.1.0.exe
    Executing C:/Temp/ccs_37f90eb4-bfc1-4fd2-42f7-b40a0205b1e1/SEGGER_J_LINK_DRIVERS/JLinkDriver_setup_1.0.1.0.exe --prefix "C:\ti\ccs2031/ccs" --eclipseprefix "C:/ti/ccs2031/ccs/eclipse" --mode unattended   --installer-log "C:\ti\ccs2031/ccs/install_logs/20251128130721"  
    Script exit code: 0
    
    Script output:
     
    
    Script stderr:
     
    
    [13:19:14] CCS_INFO: Done installing executable SEGGER_J_LINK_DRIVERS C:/Temp/ccs_37f90eb4-bfc1-4fd2-42f7-b40a0205b1e1/SEGGER_J_LINK_DRIVERS/JLinkDriver_setup_1.0.1.0.exe
    Unpacking files
    [13:19:16] CCS_INFO: Installing BLACKHAWK_EMUPACK
    [13:19:16] showprogress = false
    [13:19:16] CCS_INFO: Installing C:/Temp/ccs_37f90eb4-bfc1-4fd2-42f7-b40a0205b1e1/BLACKHAWK_EMUPACK/bh_emupack_setup_9.0.0.002_win_64.exe
    [13:19:16] CCS_INFO: Actual executable C:/Temp/ccs_37f90eb4-bfc1-4fd2-42f7-b40a0205b1e1/BLACKHAWK_EMUPACK/bh_emupack_setup_9.0.0.002_win_64.exe
    Executing C:/Temp/ccs_37f90eb4-bfc1-4fd2-42f7-b40a0205b1e1/BLACKHAWK_EMUPACK/bh_emupack_setup_9.0.0.002_win_64.exe --prefix "C:\ti\ccs2031/ccs" --eclipseprefix "C:/ti/ccs2031/ccs/eclipse" --mode unattended   --installer-log "C:\ti\ccs2031/ccs/install_logs/20251128130721"  
    Script exit code: 0
    
    Script output:
     
    
    Script stderr:
     
    
    [13:19:40] CCS_INFO: Done installing executable BLACKHAWK_EMUPACK C:/Temp/ccs_37f90eb4-bfc1-4fd2-42f7-b40a0205b1e1/BLACKHAWK_EMUPACK/bh_emupack_setup_9.0.0.002_win_64.exe
    Unpacking files
    [13:19:42] CCS_INFO: Installing CGT_DEFAULTLIBS_C6000_V8P
    [13:19:42] showprogress = false
    [13:19:42] CCS_INFO: Installing C:/Temp/ccs_37f90eb4-bfc1-4fd2-42f7-b40a0205b1e1/CGT_DEFAULTLIBS_C6000_V8P/ti_cgt_c6000_8.5.0.LTS_windows-x64_installer.exe
    [13:19:42] CCS_INFO: Actual executable C:/Temp/ccs_37f90eb4-bfc1-4fd2-42f7-b40a0205b1e1/CGT_DEFAULTLIBS_C6000_V8P/ti_cgt_c6000_8.5.0.LTS_windows-x64_installer.exe
    Executing C:/Temp/ccs_37f90eb4-bfc1-4fd2-42f7-b40a0205b1e1/CGT_DEFAULTLIBS_C6000_V8P/ti_cgt_c6000_8.5.0.LTS_windows-x64_installer.exe --prefix "C:\ti\ccs2031/ccs" --eclipseprefix "C:/ti/ccs2031/ccs/eclipse" --mode unattended   --installer-log "C:\ti\ccs2031/ccs/install_logs/20251128130721" --ccs true 
    Script exit code: 0
    
    Script output:
     
    
    Script stderr:
     
    
    [13:20:16] CCS_INFO: Done installing executable CGT_DEFAULTLIBS_C6000_V8P C:/Temp/ccs_37f90eb4-bfc1-4fd2-42f7-b40a0205b1e1/CGT_DEFAULTLIBS_C6000_V8P/ti_cgt_c6000_8.5.0.LTS_windows-x64_installer.exe
    [13:20:16] CCS_INFO: Done installing CGT_DEFAULTLIBS_C6000_V8P
    Unpacking files
    [13:20:19] CCS_INFO: Installing CGT_DEFAULTLIBS_C29
    [13:20:19] showprogress = false
    [13:20:19] CCS_INFO: Installing C:/Temp/ccs_37f90eb4-bfc1-4fd2-42f7-b40a0205b1e1/CGT_DEFAULTLIBS_C29/ti_cgt_c29_2.0.0.STS_windows-x64_installer.exe
    [13:20:19] CCS_INFO: Actual executable C:/Temp/ccs_37f90eb4-bfc1-4fd2-42f7-b40a0205b1e1/CGT_DEFAULTLIBS_C29/ti_cgt_c29_2.0.0.STS_windows-x64_installer.exe
    Executing C:/Temp/ccs_37f90eb4-bfc1-4fd2-42f7-b40a0205b1e1/CGT_DEFAULTLIBS_C29/ti_cgt_c29_2.0.0.STS_windows-x64_installer.exe --prefix "C:\ti\ccs2031/ccs" --eclipseprefix "C:/ti/ccs2031/ccs/eclipse" --mode unattended   --installer-log "C:\ti\ccs2031/ccs/install_logs/20251128130721" --ccs true 
    Script exit code: 0
    
    Script output:
     
    
    Script stderr:
     
    
    [13:21:20] CCS_INFO: Done installing executable CGT_DEFAULTLIBS_C29 C:/Temp/ccs_37f90eb4-bfc1-4fd2-42f7-b40a0205b1e1/CGT_DEFAULTLIBS_C29/ti_cgt_c29_2.0.0.STS_windows-x64_installer.exe
    [13:21:20] CCS_INFO: Done installing CGT_DEFAULTLIBS_C29
    Unpacking files
    [13:21:22] CCS_INFO: Installing CGT_DEFAULTLIBS_C7000
    [13:21:22] showprogress = false
    [13:21:23] CCS_INFO: Installing C:/Temp/ccs_37f90eb4-bfc1-4fd2-42f7-b40a0205b1e1/CGT_DEFAULTLIBS_C7000/ti_cgt_c7000_5.0.0.LTS_windows-x64_installer.exe
    [13:21:23] CCS_INFO: Actual executable C:/Temp/ccs_37f90eb4-bfc1-4fd2-42f7-b40a0205b1e1/CGT_DEFAULTLIBS_C7000/ti_cgt_c7000_5.0.0.LTS_windows-x64_installer.exe
    Executing C:/Temp/ccs_37f90eb4-bfc1-4fd2-42f7-b40a0205b1e1/CGT_DEFAULTLIBS_C7000/ti_cgt_c7000_5.0.0.LTS_windows-x64_installer.exe --prefix "C:\ti\ccs2031/ccs" --eclipseprefix "C:/ti/ccs2031/ccs/eclipse" --mode unattended   --installer-log "C:\ti\ccs2031/ccs/install_logs/20251128130721" --ccs true 
    Script exit code: 0
    
    Script output:
     
    
    Script stderr:
     
    
    [13:21:53] CCS_INFO: Done installing executable CGT_DEFAULTLIBS_C7000 C:/Temp/ccs_37f90eb4-bfc1-4fd2-42f7-b40a0205b1e1/CGT_DEFAULTLIBS_C7000/ti_cgt_c7000_5.0.0.LTS_windows-x64_installer.exe
    [13:21:53] CCS_INFO: Done installing CGT_DEFAULTLIBS_C7000
    Unpacking files
    [13:21:53] CCS_INFO: Done installing TIVA_STELLARIS_DRIVERS
    Unpacking files
    [13:22:18] CCS_INFO: Done installing PF_SITARA_MCU
    Unpacking files
    [13:23:49] CCS_INFO: Done installing PF_ARM_MPU
    Unpacking files
    [13:24:22] CCS_INFO: Done installing PF_C28
    Unpacking files
    [13:24:52] CCS_INFO: Done installing PF_C6000SC
    Unpacking files
    [13:24:58] CCS_INFO: Done installing PF_HERCULES
    Unpacking files
    [13:25:29] CCS_INFO: Done installing PF_MMWAVE
    Unpacking files
    [13:27:25] CCS_INFO: Done installing PF_MSP430
    Unpacking files
    [13:27:42] CCS_INFO: Done installing PF_MSPM0
    Unpacking files
    [13:27:45] CCS_INFO: Done installing PF_MSPM33
    Unpacking files
    [13:27:46] CCS_INFO: Installing CGT_DEFAULTLIBS_MSP430
    [13:27:46] showprogress = false
    [13:27:47] CCS_INFO: Installing C:/Temp/ccs_37f90eb4-bfc1-4fd2-42f7-b40a0205b1e1/CGT_DEFAULTLIBS_MSP430/ti_cgt_msp430_21.6.1.LTS_windows-x64_installer.exe
    [13:27:47] CCS_INFO: Actual executable C:/Temp/ccs_37f90eb4-bfc1-4fd2-42f7-b40a0205b1e1/CGT_DEFAULTLIBS_MSP430/ti_cgt_msp430_21.6.1.LTS_windows-x64_installer.exe
    Executing C:/Temp/ccs_37f90eb4-bfc1-4fd2-42f7-b40a0205b1e1/CGT_DEFAULTLIBS_MSP430/ti_cgt_msp430_21.6.1.LTS_windows-x64_installer.exe --prefix "C:\ti\ccs2031/ccs" --eclipseprefix "C:/ti/ccs2031/ccs/eclipse" --mode unattended   --installer-log "C:\ti\ccs2031/ccs/install_logs/20251128130721" --ccs true 
    Script exit code: 0
    
    Script output:
     
    
    Script stderr:
     
    
    [13:28:15] CCS_INFO: Done installing executable CGT_DEFAULTLIBS_MSP430 C:/Temp/ccs_37f90eb4-bfc1-4fd2-42f7-b40a0205b1e1/CGT_DEFAULTLIBS_MSP430/ti_cgt_msp430_21.6.1.LTS_windows-x64_installer.exe
    [13:28:15] CCS_INFO: Done installing CGT_DEFAULTLIBS_MSP430
    Unpacking files
    [13:28:16] CCS_INFO: Installing CGT_DEFAULTLIBS_C2800
    [13:28:16] showprogress = false
    [13:28:16] CCS_INFO: Installing C:/Temp/ccs_37f90eb4-bfc1-4fd2-42f7-b40a0205b1e1/CGT_DEFAULTLIBS_C2800/ti_cgt_c2000_22.6.2.LTS_windows-x64_installer.exe
    [13:28:16] CCS_INFO: Actual executable C:/Temp/ccs_37f90eb4-bfc1-4fd2-42f7-b40a0205b1e1/CGT_DEFAULTLIBS_C2800/ti_cgt_c2000_22.6.2.LTS_windows-x64_installer.exe
    Executing C:/Temp/ccs_37f90eb4-bfc1-4fd2-42f7-b40a0205b1e1/CGT_DEFAULTLIBS_C2800/ti_cgt_c2000_22.6.2.LTS_windows-x64_installer.exe --prefix "C:\ti\ccs2031/ccs" --eclipseprefix "C:/ti/ccs2031/ccs/eclipse" --mode unattended   --installer-log "C:\ti\ccs2031/ccs/install_logs/20251128130721" --ccs true 
    Script exit code: 0
    
    Script output:
     
    
    Script stderr:
     
    
    [13:28:45] CCS_INFO: Done installing executable CGT_DEFAULTLIBS_C2800 C:/Temp/ccs_37f90eb4-bfc1-4fd2-42f7-b40a0205b1e1/CGT_DEFAULTLIBS_C2800/ti_cgt_c2000_22.6.2.LTS_windows-x64_installer.exe
    [13:28:45] CCS_INFO: Done installing CGT_DEFAULTLIBS_C2800
    Unpacking files
    [13:29:10] CCS_INFO: Done installing PF_OMAPL
    Unpacking files
    [13:29:10] CCS_INFO: Done installing PF_PGA
    Unpacking files
    [13:29:15] CCS_INFO: Done installing PF_MSP432
    Unpacking files
    [13:32:20] CCS_INFO: Done installing PF_AUTO
    Unpacking files
    [13:32:35] CCS_INFO: Done installing PF_TM4C
    Unpacking files
    [13:32:44] CCS_INFO: Done installing PF_DIGITAL_POWER
    Unpacking files
    [13:33:08] CCS_INFO: Done installing PF_WCONN
    [13:33:09] CCS_INFO: Done installing all components, doing postinstall now
    [13:33:09] CCS_INFO: Writing C:/ti/ccs2031/ccs/eclipse/ccs.properties
    Executing C:\ti\ccs2031\ccs\ccs_base\EMULAT~1\drivers\msp430/DPInst/DPInst64.exe /q /se /sa /lm /path C:\ti\ccs2031\ccs\ccs_base\EMULAT~1\drivers\msp430\USB_CDC
    Script exit code: 256
    
    Script output:
     
    
    Script stderr:
     Program ended with an error exit code
    
    Error running C:\ti\ccs2031\ccs\ccs_base\EMULAT~1\drivers\msp430/DPInst/DPInst64.exe /q /se /sa /lm /path C:\ti\ccs2031\ccs\ccs_base\EMULAT~1\drivers\msp430\USB_CDC: Program ended with an error exit code
    Executing C:\ti\ccs2031\ccs\ccs_base\EMULAT~1\drivers\msp430/DPInst/DPInst64.exe /q /se /sa /lm /path C:\ti\ccs2031\ccs\ccs_base\EMULAT~1\drivers\msp430\USB_EZ~1
    Script exit code: 256
    
    Script output:
     
    
    Script stderr:
     Program ended with an error exit code
    
    Error running C:\ti\ccs2031\ccs\ccs_base\EMULAT~1\drivers\msp430/DPInst/DPInst64.exe /q /se /sa /lm /path C:\ti\ccs2031\ccs\ccs_base\EMULAT~1\drivers\msp430\USB_EZ~1: Program ended with an error exit code
    Executing C:\ti\ccs2031\ccs\ccs_base\EMULAT~1\drivers\msp430/DPInst/DPInst64.exe /q /se /sa /lm /path C:\ti\ccs2031\ccs\ccs_base\EMULAT~1\drivers\msp430\USB_FE~1
    Script exit code: 256
    
    Script output:
     
    
    Script stderr:
     Program ended with an error exit code
    
    Error running C:\ti\ccs2031\ccs\ccs_base\EMULAT~1\drivers\msp430/DPInst/DPInst64.exe /q /se /sa /lm /path C:\ti\ccs2031\ccs\ccs_base\EMULAT~1\drivers\msp430\USB_FE~1: Program ended with an error exit code
    [13:33:12] CCS_INFO: Running C:/ti/ccs2031/ccs/eclipse/ccs-server -nosplash -clean -data C:\ti\ccs2031/ccs/install_logs -application com.ti.ccs.initialize
    Running C:/ti/ccs2031/ccs/eclipse/ccs-server.
    Executing C:/ti/ccs2031/ccs/eclipse/ccs-server -nosplash -clean -data "C:\ti\ccs2031/ccs/install_logs" -application com.ti.ccs.initialize
    Script exit code: 0
    
    Script output:
     
    --------------------------------------------------------------------------------
    Initializing CCS...
    
    Initializing TargetDB cache... Finished!
    Generating dynamic tool-definitions... Finished!
    Discovering products and compilers... Finished!
    
    Done
    
    Script stderr:
     
    
    [13:33:39] CCS_INFO: Successfully ran com.ti.ccs.initialize.
    [13:33:39] CCS_INFO: copyCCSInstaller copying to C:\ti\ccs2031/ccs/install_info/ccs_setup_20.3.1.00005.exe
    Executing C:\Temp/ccs_37f90eb4-bfc1-4fd2-42f7-b40a0205b1e1/copyinstaller.bat 
    Script exit code: 0
    
    Script output:
             1 Datei(en) kopiert.
    
    Script stderr:
     
    
    [13:33:40] CCS_INFO: copyCCSInstaller successfully copied C:\ti\ccs2031/ccs/install_info/ccs_setup_20.3.1.00005.exe.
    [13:33:45] CCS_INFO: Components installed:  BLACKHAWK_EMUPACK CCS_DOC CCS_UTILS CGT_DEFAULTLIBS_C2800 CGT_DEFAULTLIBS_C29 CGT_DEFAULTLIBS_C6000_V8P CGT_DEFAULTLIBS_C7000 CGT_DEFAULTLIBS_MSP430 CLOUDAGENT DS DS_FLASH ECLIPSE EMU_TI IDE_METADATA MSVC_REDIST_LATEST NODEJS PF_ARM_MPU PF_AUTO PF_C28 PF_C6000SC PF_DIGITAL_POWER PF_HERCULES PF_MMWAVE PF_MSP430 PF_MSP432 PF_MSPM0 PF_MSPM33 PF_OMAPL PF_PGA PF_SITARA_MCU PF_TM4C SEGGER_J_LINK SEGGER_J_LINK_DRIVERS SYSCONFIG TARGETDB_DEF_PROPS THEIA TIREX TIVA_STELLARIS_DRIVERS TI_ARM_CLANG YAROV CCS_UTILS TIREX ECLIPSE NODEJS DS DS_FLASH CLOUDAGENT SYSCONFIG EMU_TI TI_ARM_CLANG CCS_DOC TARGETDB_DEF_PROPS YAROV IDE_METADATA SEGGER_J_LINK CGT_DEFAULTLIBS_MSP430 CGT_DEFAULTLIBS_C2800 CGT_DEFAULTLIBS_C6000_V8P CGT_DEFAULTLIBS_C29 CGT_DEFAULTLIBS_C7000 TIVA_STELLARIS_DRIVERS THEIA
    Executing C:\ti\ccs2031/ccs/tools/node/node "C:\Temp/ccs_37f90eb4-bfc1-4fd2-42f7-b40a0205b1e1/modifyCloudAgentConfig.js"
    Script exit code: 0
    
    Script output:
     
    
    Script stderr:
     
    
    [13:33:46] createShortcuts set to true
    [13:33:47] CCS_INFO: Updating core component and restarting ccstudio
    [13:33:47] CCS_INFO: CCStudio set to C:/ti/ccs2031/ccs/theia/ccstudio.exe
    [13:33:47] CCS_INFO: Updating core component and restarting ccstudio
    [13:33:47] CCS_INFO: CCStudio set to C:/ti/ccs2031/ccs/theia/ccstudio.exe
    Creating Uninstaller
    Creating uninstaller 50%
    Creating uninstaller 75%
    Creating uninstaller 100%
    Installation completed
    [13:34:01] CCS_INFO: CCS 20.3.1.00005 installed successfully.
    [13:34:01] CCS_INFO: Downloading http://software-dl.ti.com/ccs/esd/tia/CCS20.3.1.00005_tia_windows-x64_complete_offline.zip
    [13:34:02] CCS_INFO: Return values from downloadMarker http://software-dl.ti.com/ccs/esd/tia/CCS20.3.1.00005_tia_windows-x64_complete_offline.zip: 404
    [13:34:03] Moving logfile to C:\ti\ccs2031/ccs/install_logs/20251128130721/ccs_install_20.3.1.00005.log
    

    Hi Michael,

    Yes, the log file 5444.ccs_install_12.8.1.00005.log is indeed from the installation that hung. The installation using PSADT generally works fine, but the issue occurs at the very end: the process does not finish properly, which prevents the registration from completing. As shown in the previous screenshot, another process remains active and causes the hang.

    The same behavior also happens with the Theia-based CCS 20.X versions. I will send you the corresponding logs for those installations as well.

    Please let me know if you need any further details.

    Best regards,
    Ali