This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Customizing programs with the Red Suite tools for the LM3S9B90 evaluation board

Hi,

I'm trying to build the SoundTest project from the RDB board to run on the Code Red tools. I want to play with I2S clock timing as part of my evaluation.

When I try to build the project, it posts a error: fatal error: inc/hw_memmap.h: No such file or directory adc.c /driverlib line 34

The file exists in my work space in the inc folder.

How do I set up the project to look in that folder for the file?

I found a setting for Include paths [SoundTest Debug] and it has values "${workspace_loc:/inc}", but I don't what just what the "${workspace_loc:/inc}" macro is including.

I didn't see a forum for the LM3S9B90 microcontroller, so I'm not sure where to post this.

If you can shed any light in my darkness, I would appreciate it.

Thanks,

Bob Kruse