This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM335x EVM boot-mode switch (SW3) wrong labelled

Expert 2280 points


I would like to outline that boot-mode DIP switch on AM335x EVM (SW3) is labelled in a the wrong way, that means:

SW3[1] = ON  ---> SYSBOOT[0] = 0

SW3[1] = OFF ---> SYSBOOT[0] = 1

This is also clarified in U-Boot and StarterWare user guides, which IMHO are not the best places for an EVM HW detail.

Regards, Max