Part Number: TDA3MV
I'd like to use multiple cameras with the TDA3.
Is a PARALLEL + CSI2 combination possible?
If so, how should I connect the pins?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TDA3MV
I'd like to use multiple cameras with the TDA3.
Is a PARALLEL + CSI2 combination possible?
If so, how should I connect the pins?
you can use CSI interface to connect multiple cameras via CSI Hub. CSI supports multiple interleaved virtual channels/camera..
Regards,
Brijesh
Is there a way to connect directly without the SER/DES structure?
Regards,
Kim
I really doubt it.. But CSI as a protocol supports multiple interleaved camera input.. So if you can bring in this camera over CSI, they can be captured using just single interface.
Regards,
Brijesh
Hi

I came across this while looking through the TDA3 TRM documentation.
Does this image indicate that serial and parallel interface multi-camera connections are possible on the ISS interface?
Regards,
Kim
Hi,
Yes, ISS does support both parallel and CSI interface, but may not be simultaneously. Please check the TRM for this.
Regards,
brijesh