This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM62P: SK-AM62p-LP : MCU + SDK : Kernel Log Reduction for Boot Time Optimisation

Part Number: AM62P

I am working on a Cluster application using the MCU+SDK, where the R5 core handles telltales and the A53 core runs a Qt application. To reduce Linux boot time, we need to quiet the kernel logs and disable printk.

Current Issue

I have set the desired kernel command-line values in both uEnv.txt and the kernel device tree (k3-am62p5-sk.dts).

However, during boot, the default kernel command-line value is overriding our settings.

Need assistance with the following:

  1. How to properly set the boot arguments (e.g., adding quiet, loglevel=0, or similar parameters).

  2. How to disable or prevent the default Kernel command line from overriding the desired settings.

Log : 

Welcome to minicom 2.8

OPTIONS: I18n 
Port /dev/ttyUSB0, 13:26:40

Press CTRL-A Z for help on special keys


[BOOTLOADER_PROFILE] Boot Media       : FLASH 
[BOOTLOADER_PROFILE] Boot Media Clock : 166.667 MHz 
[BOOTLOADER_PROFILE] Boot Image Size  : 585 KB 
[BOOTLOADER_PROFILE] Cores present    : 
wkup-r5f0-0
[BOOTLOADER PROFILE] System_init                      :      38431us 
[BOOTLOADER PROFILE] App_waitForMcuPbist              :          2us 
[BOOTLOADER PROFILE] Board_init                       :          0us 
[BOOTLOADER PROFILE] Drivers_open                     :         91us 
[BOOTLOADER PROFILE] SBL Drivers_open                 :        133us 
[BOOTLOADER PROFILE] Board_driversOpen                :          9us 
[BOOTLOADER PROFILE] SBL Board_driversOpen            :       1298us 
[BOOTLOADER PROFILE] App_loadSelfcoreImage            :       7480us 
[BOOTLOADER_PROFILE] SBL Total Time Taken             :      47446us 

Image loading done, switching to application ...
Starting 2nd stage bootloader
Sciserver Testapp Built On: May 13 2025 14:44:12
Sciserver Version: v2024.12.0.0-REL.MCUSDK.K3.10.01.00.33+
RM_PM_HAL Version: v10.01.08
Starting Sciserver..... PASSED
Configure DSS region firewall... DONE !!!
Configure DSS framebuffer region firewall... DONE !!!
[Driver] HWIP HwiP_Params_init 

[Driver] HWIP HwiP_construct 

[Driver] HWIP HwiP_construct callback : 9CABF461

DispApp_init() - DONE !!!
DSS display share application started...
Display create complete!!
Starting display ... !!!
Display in progress ... DO NOT HALT !!!
DSS display share Passed!!
[BOOTLOADER_PROFILE] Boot Media       : FLASH 
[BOOTLOADER_PROFILE] Boot Image Size  : 886 KB 
[BOOTLOADER_PROFILE] Cores present    : 
hsm-m4f0-0
mcu-r5f0-0
a530-0
[BOOTLOADER PROFILE] System_init                      :       7900us 
[BOOTLOADER PROFILE] Board_init                       :          7us 
[BOOTLOADER PROFILE] FreeRtosTask Create              :        268us 
[BOOTLOADER PROFILE] SBL Drivers_open                 :       1233us 
[BOOTLOADER PROFILE] SBL Board_driversOpen            :        189us 
[BOOTLOADER PROFILE] HSM Image Load                   :       3915us 
[BOOTLOADER PROFILE] MCU R5 Image Load                :       4407us 
[BOOTLOADER PROFILE] A53 Image Load                   :      14183us 
[BOOTLOADER_PROFILE] SBL Total Time Taken             :      32105us 

Image loading done, switching to application ...
Starting linux and RTOS/Baremetal applications
NOTICE:  BL31: v2.11.0(release):v2.11.0-906-g58b25570c9-dirty
NOTICE:  BL31: Built : 04:20:32, Nov  1 2024

U-Boot SPL 2024.04-dirty (Nov 18 2025 - 13:28:34 +0530)
SYSFW ABI: 4.0 (firmware rev 0x000a '10.1.8--v10.01.08 (Fiery Fox)')
SPL initial stack usage: 1904 bytes
ti_sci system-controller@44043000: Message not acknowledged
ti-sci-pm-domains power-controller: ti_sci_power_domain_on: get_device(186) failed (-19)
ti_sci system-controller@44043000: Message not acknowledged
ti-sci-pm-domains power-controller: ti_sci_power_domain_on: get_device(243) failed (-19)
ti_sci system-controller@44043000: Message not acknowledged
ti-sci-pm-domains power-controller: ti_sci_power_domain_on: get_device(244) failed (-19)
Trying to boot from SPI
Authentication passed
Authentication passed


U-Boot 2024.04-dirty (Nov 26 2025 - 18:29:26 +0530)

SoC:   AM62PX SR1.0 HS-FS
Model: Texas Instruments AM62P5 SK
DRAM:  2 GiB (effective 8 GiB)
Core:  85 devices, 31 uclasses, devicetree: separate
MMC:   mmc@fa10000: 0, mmc@fa00000: 1
Loading Environment from nowhere... OK
In:    serial
Out:   serial
Err:   serial
Net:   eth0: ethernet@8000000port@1
Warning: ethernet@8000000port@2 (eth1) using random MAC address - b6:59:71:2c:38:df
, eth1: ethernet@8000000port@2
Hit any key to stop autoboot:  0 
switch to partitions #0, OK
mmc1 is current device
SD/MMC found on device 1
828 bytes read in 7 ms (115.2 KiB/s)
Loaded env from uEnv.txt
Importing environment from mmc1 ...
21029376 bytes read in 223 ms (89.9 MiB/s)
65828 bytes read in 10 ms (6.3 MiB/s)
Working FDT set to 88000000
3096 bytes read in 10 ms (301.8 KiB/s)
985 bytes read in 9 ms (106.4 KiB/s)
## Flattened Device Tree blob at 88000000
   Booting using the fdt blob at 0x88000000
Working FDT set to 88000000
   Loading Device Tree to 000000008feec000, end 000000008fffffff ... OK
Working FDT set to 8feec000

Starting kernel ...

[    0.000000] Booting Linux on physical CPU 0x0000000000 [0x410fd034]
[    0.000000] Linux version 6.6.58-ti-01497-ga7758da17c28-dirty (oe-user@oe-host) (aarch64-oe-linux-gcc (GCC) 13.3.0, GNU ld (GNU Binutils) 2.42.0.20240723) #1 SMP PREEMPT Wed Nov 27 13:23:15 UTC 2024
[    0.000000] KASLR disabled due to lack of seed
[    0.000000] Machine model: Texas Instruments AM62P5 SK
[    0.000000] earlycon: ns16550a0 at MMIO32 0x0000000002800000 (options '')
[    0.000000] printk: bootconsole [ns16550a0] enabled
[    0.000000] efi: UEFI not found.
[    0.000000] Reserved memory: created CMA memory pool at 0x00000009dc000000, size 576 MiB
[    0.000000] OF: reserved mem: initialized node linux,cma, compatible id shared-dma-pool
[    0.000000] OF: reserved mem: 0x00000009dc000000..0x00000009ffffffff (589824 KiB) map reusable linux,cma
[    0.000000] OF: reserved mem: 0x0000000080000000..0x000000008007ffff (512 KiB) nomap non-reusable tfa@80000000
[    0.000000] OF: reserved mem: 0x0000000093500000..0x000000009b4fffff (131072 KiB) nomap non-reusable rtos-framebuffer-memory@93500000
[    0.000000] OF: reserved mem: 0x000000009e800000..0x000000009fffffff (24576 KiB) nomap non-reusable optee@9e800000
[    0.000000] Zone ranges:
[    0.000000]   DMA      [mem 0x0000000080000000-0x00000000ffffffff]
[    0.000000]   DMA32    empty
[    0.000000]   Normal   [mem 0x0000000100000000-0x00000009ffffffff]
[    0.000000] Movable zone start for each node
[    0.000000] Early memory node ranges
[    0.000000]   node   0: [mem 0x0000000080000000-0x000000008007ffff]
[    0.000000]   node   0: [mem 0x0000000080080000-0x00000000934fffff]
[    0.000000]   node   0: [mem 0x0000000093500000-0x000000009b4fffff]
[    0.000000]   node   0: [mem 0x000000009b500000-0x000000009e7fffff]
[    0.000000]   node   0: [mem 0x000000009e800000-0x000000009fffffff]
[    0.000000]   node   0: [mem 0x00000000a0000000-0x00000000ffffffff]
[    0.000000]   node   0: [mem 0x0000000880000000-0x00000009ffffffff]
[    0.000000] Initmem setup node 0 [mem 0x0000000080000000-0x00000009ffffffff]
[    0.000000] psci: probing for conduit method from DT.
[    0.000000] psci: PSCIv1.1 detected in firmware.
[    0.000000] psci: Using standard PSCI v0.2 function IDs
[    0.000000] psci: Trusted OS migration not required
[    0.000000] psci: SMC Calling Convention v1.5
[    0.000000] percpu: Embedded 20 pages/cpu s43176 r8192 d30552 u81920
[    0.000000] Detected VIPT I-cache on CPU0
[    0.000000] CPU features: detected: GIC system register CPU interface
[    0.000000] CPU features: detected: ARM erratum 845719
[    0.000000] alternatives: applying boot alternatives
[    0.000000] Kernel command line: console=ttyS2,115200n8 earlycon=ns16550a,mmio32,0x02800000 root=PARTUUID=076c4a2a-02 rw rootfstype=ext4 rootwait
[    0.000000] Dentry cache hash table entries: 1048576 (order: 11, 8388608 bytes, linear)
[    0.000000] Inode-cache hash table entries: 524288 (order: 10, 4194304 bytes, linear)
[    0.000000] Built 1 zonelists, mobility grouping on.  Total pages: 2064384
[    0.000000] mem auto-init: stack:all(zero), heap alloc:off, heap free:off
[    0.000000] software IO TLB: area num 4.
[    0.000000] software IO TLB: mapped [mem 0x00000000fbfff000-0x00000000fffff000] (64MB)
[    0.000000] Memory: 7395028K/8388608K available (12480K kernel code, 1272K rwdata, 4184K rodata, 2496K init, 528K bss, 403756K reserved, 589824K cma-reserved)
[    0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=4, Nodes=1
[    0.000000] rcu: Preemptible hierarchical RCU implementation.
[    0.000000] rcu:     RCU event tracing is enabled.
[    0.000000] rcu:     RCU restricting CPUs from NR_CPUS=256 to nr_cpu_ids=4.
[    0.000000]  Trampoline variant of Tasks RCU enabled.
[    0.000000]  Tracing variant of Tasks RCU enabled.
[    0.000000] rcu: RCU calculated value of scheduler-enlistment delay is 25 jiffies.
[    0.000000] rcu: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=4
[    0.000000] NR_IRQS: 64, nr_irqs: 64, preallocated irqs: 0
[    0.000000] GICv3: GIC: Using split EOI/Deactivate mode
[    0.000000] GICv3: 256 SPIs implemented
[    0.000000] GICv3: 0 Extended SPIs implemented
[    0.000000] Root IRQ handler: gic_handle_irq
[    0.000000] GICv3: GICv3 features: 16 PPIs
[    0.000000] GICv3: CPU0: found redistributor 0 region 0:0x0000000001880000
[    0.000000] ITS [mem 0x01820000-0x0182ffff]
[    0.000000] GIC: enabling workaround for ITS: Socionext Synquacer pre-ITS
[    0.000000] ITS@0x0000000001820000: Devices Table too large, reduce ids 20->19
[    0.000000] ITS@0x0000000001820000: allocated 524288 Devices @880800000 (flat, esz 8, psz 64K, shr 0)
[    0.000000] ITS: using cache flushing for cmd queue
[    0.000000] GICv3: using LPI property table @0x0000000880040000
[    0.000000] GIC: using cache flushing for LPI property table
[    0.000000] GICv3: CPU0: using allocated LPI pending table @0x0000000880050000
[    0.000000] rcu: srcu_init: Setting srcu_struct sizes based on contention.
[    0.000000] arch_timer: cp15 timer(s) running at 200.00MHz (phys).
[    0.000000] clocksource: arch_sys_counter: mask: 0x3ffffffffffffff max_cycles: 0x2e2049d3e8, max_idle_ns: 440795210634 ns
[    0.000001] sched_clock: 58 bits at 200MHz, resolution 5ns, wraps every 4398046511102ns
[    0.008513] Console: colour dummy device 80x25
[    0.013104] Calibrating delay loop (skipped), value calculated using timer frequency.. 400.00 BogoMIPS (lpj=800000)
[    0.023780] pid_max: default: 32768 minimum: 301
[    0.028570] LSM: initializing lsm=capability,selinux,integrity
[    0.034548] SELinux:  Initializing.
[    0.038226] Mount-cache hash table entries: 16384 (order: 5, 131072 bytes, linear)
[    0.045984] Mountpoint-cache hash table entries: 16384 (order: 5, 131072 bytes, linear)
[    0.055746] RCU Tasks: Setting shift to 2 and lim to 1 rcu_task_cb_adjust=1.
[    0.063039] RCU Tasks Trace: Setting shift to 2 and lim to 1 rcu_task_cb_adjust=1.
[    0.070932] rcu: Hierarchical SRCU implementation.
[    0.075832] rcu:     Max phase no-delay instances is 1000.
[    0.081405] Platform MSI: msi-controller@1820000 domain created
[    0.087667] PCI/MSI: /bus@f0000/interrupt-controller@1800000/msi-controller@1820000 domain created
[    0.097060] EFI services will not be available.
[    0.101927] smp: Bringing up secondary CPUs ...
[    0.107185] Detected VIPT I-cache on CPU1
[    0.107255] GICv3: CPU1: found redistributor 1 region 0:0x00000000018a0000
[    0.107270] GICv3: CPU1: using allocated LPI pending table @0x0000000880060000
[    0.107315] CPU1: Booted secondary processor 0x0000000001 [0x410fd034]
[    0.107977] Detected VIPT I-cache on CPU2
[    0.108026] GICv3: CPU2: found redistributor 2 region 0:0x00000000018c0000
[    0.108039] GICv3: CPU2: using allocated LPI pending table @0x0000000880070000
[    0.108069] CPU2: Booted secondary processor 0x0000000002 [0x410fd034]
[    0.108644] Detected VIPT I-cache on CPU3
[    0.108689] GICv3: CPU3: found redistributor 3 region 0:0x00000000018e0000
[    0.108700] GICv3: CPU3: using allocated LPI pending table @0x0000000880080000
[    0.108726] CPU3: Booted secondary processor 0x0000000003 [0x410fd034]
[    0.108796] smp: Brought up 1 node, 4 CPUs
[    0.188431] SMP: Total of 4 processors activated.
[    0.193239] CPU features: detected: 32-bit EL0 Support
[    0.198500] CPU features: detected: CRC32 instructions
[    0.203800] CPU: All CPU(s) started at EL2
[    0.207991] alternatives: applying system-wide alternatives
[    0.215261] devtmpfs: initialized
[    0.228602] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 7645041785100000 ns
[    0.238592] futex hash table entries: 1024 (order: 4, 65536 bytes, linear)
[    0.259321] pinctrl core: initialized pinctrl subsystem
[    0.265131] DMI not present or invalid.
[    0.269620] NET: Registered PF_NETLINK/PF_ROUTE protocol family
[    0.276494] DMA: preallocated 1024 KiB GFP_KERNEL pool for atomic allocations
[    0.283918] DMA: preallocated 1024 KiB GFP_KERNEL|GFP_DMA pool for atomic allocations
[    0.292017] DMA: preallocated 1024 KiB GFP_KERNEL|GFP_DMA32 pool for atomic allocations
[    0.300259] audit: initializing netlink subsys (disabled)
[    0.305955] audit: type=2000 audit(0.192:1): state=initialized audit_enabled=0 res=1
[    0.306366] thermal_sys: Registered thermal governor 'step_wise'
[    0.313879] thermal_sys: Registered thermal governor 'power_allocator'
[    0.320056] cpuidle: using governor menu
[    0.330879] hw-breakpoint: found 6 breakpoint and 4 watchpoint registers.
[    0.337887] ASID allocator initialised with 65536 entries
[    0.348201] /bus@f0000/interrupt-controller@1800000: Fixed dependency cycle(s) with /bus@f0000/interrupt-controller@1800000
[    0.359673] /bus@f0000/i2c@20000000/usb-power-controller@3f/connector: Fixed dependency cycle(s) with /bus@f0000/usb@f900000/usb@31000000
[    0.372338] /bus@f0000/usb@f900000/usb@31000000: Fixed dependency cycle(s) with /bus@f0000/i2c@20000000/usb-power-controller@3f/connector
[    0.385028] /bus@f0000/dss@30200000: Fixed dependency cycle(s) with /bus@f0000/dss@30200000/oldi-txes/oldi@1
[    0.395076] /bus@f0000/dss@30200000: Fixed dependency cycle(s) with /bus@f0000/dss@30200000/oldi-txes/oldi@0
[    0.405126] /bus@f0000/dss@30200000/oldi-txes/oldi@0: Fixed dependency cycle(s) with /bus@f0000/dss@30200000
[    0.415173] /bus@f0000/dss@30200000/oldi-txes/oldi@1: Fixed dependency cycle(s) with /bus@f0000/dss@30200000
[    0.430103] /bus@f0000/i2c@20000000/usb-power-controller@3f/connector: Fixed dependency cycle(s) with /bus@f0000/usb@f900000/usb@31000000
[    0.443506] /bus@f0000/usb@f900000/usb@31000000: Fixed dependency cycle(s) with /bus@f0000/i2c@20000000/usb-power-controller@3f/connector
[    0.457890] /bus@f0000/dss@30200000: Fixed dependency cycle(s) with /bus@f0000/dss@30200000/oldi-txes/oldi@1
[    0.467954] /bus@f0000/dss@30200000: Fixed dependency cycle(s) with /bus@f0000/dss@30200000/oldi-txes/oldi@0
[    0.478016] /bus@f0000/dss@30200000/oldi-txes/oldi@0: Fixed dependency cycle(s) with /bus@f0000/dss@30200000
[    0.488073] /bus@f0000/dss@30200000/oldi-txes/oldi@1: Fixed dependency cycle(s) with /bus@f0000/dss@30200000
[    0.499362] /bus@f0000/dss@30200000/oldi-txes/oldi@1: Fixed dependency cycle(s) with /display
[    0.508141] /bus@f0000/dss@30200000/oldi-txes/oldi@0: Fixed dependency cycle(s) with /display
[    0.516866] /display: Fixed dependency cycle(s) with /bus@f0000/dss@30200000/oldi-txes/oldi@1
[    0.525587] /display: Fixed dependency cycle(s) with /bus@f0000/dss@30200000/oldi-txes/oldi@0
[    0.534675] Modules: 27488 pages in range for non-PLT usage
[    0.534681] Modules: 519008 pages in range for PLT usage
[    0.541027] HugeTLB: registered 1.00 GiB page size, pre-allocated 0 pages
[    0.553407] HugeTLB: 0 KiB vmemmap can be freed for a 1.00 GiB page
[    0.559809] HugeTLB: registered 32.0 MiB page size, pre-allocated 0 pages
[    0.566738] HugeTLB: 0 KiB vmemmap can be freed for a 32.0 MiB page
[    0.573140] HugeTLB: registered 2.00 MiB page size, pre-allocated 0 pages
[    0.580072] HugeTLB: 0 KiB vmemmap can be freed for a 2.00 MiB page
[    0.586473] HugeTLB: registered 64.0 KiB page size, pre-allocated 0 pages
[    0.593405] HugeTLB: 0 KiB vmemmap can be freed for a 64.0 KiB page
[    0.601053] k3-chipinfo 43000014.chipid: Family:AM62PX rev:SR1.0 JTAGID[0x0bb9d02f] Detected
[    0.610306] iommu: Default domain type: Translated
[    0.615221] iommu: DMA domain TLB invalidation policy: strict mode
[    0.621798] SCSI subsystem initialized
[    0.625906] usbcore: registered new interface driver usbfs
[    0.631540] usbcore: registered new interface driver hub
[    0.636988] usbcore: registered new device driver usb
[    0.642583] pps_core: LinuxPPS API ver. 1 registered
[    0.647654] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>
[    0.656992] PTP clock support registered
[    0.661174] EDAC MC: Ver: 3.0.0
[    0.664831] scmi_core: SCMI protocol bus registered
[    0.670087] FPGA manager framework
[    0.673636] Advanced Linux Sound Architecture Driver Initialized.
[    0.680714] vgaarb: loaded
[    0.683810] clocksource: Switched to clocksource arch_sys_counter
[    0.690297] VFS: Disk quotas dquot_6.6.0
[    0.694341] VFS: Dquot-cache hash table entries: 512 (order 0, 4096 bytes)
[    0.707324] NET: Registered PF_INET protocol family
[    0.712591] IP idents hash table entries: 131072 (order: 8, 1048576 bytes, linear)
[    0.724993] tcp_listen_portaddr_hash hash table entries: 4096 (order: 4, 65536 bytes, linear)
[    0.733820] Table-perturb hash table entries: 65536 (order: 6, 262144 bytes, linear)
[    0.741754] TCP established hash table entries: 65536 (order: 7, 524288 bytes, linear)
[    0.750197] TCP bind hash table entries: 65536 (order: 9, 2097152 bytes, linear)
[    0.759364] TCP: Hash tables configured (established 65536 bind 65536)
[    0.766223] UDP hash table entries: 4096 (order: 5, 131072 bytes, linear)
[    0.773314] UDP-Lite hash table entries: 4096 (order: 5, 131072 bytes, linear)
[    0.780977] NET: Registered PF_UNIX/PF_LOCAL protocol family
[    0.787180] RPC: Registered named UNIX socket transport module.
[    0.793253] RPC: Registered udp transport module.
[    0.798057] RPC: Registered tcp transport module.
[    0.802868] RPC: Registered tcp-with-tls transport module.
[    0.808469] RPC: Registered tcp NFSv4.1 backchannel transport module.
[    0.815050] NET: Registered PF_XDP protocol family
[    0.819959] PCI: CLS 0 bytes, default 64
[    0.825236] Initialise system trusted keyrings
[    0.829979] workingset: timestamp_bits=46 max_order=21 bucket_order=0
[    0.836854] squashfs: version 4.0 (2009/01/31) Phillip Lougher
[    0.843057] NFS: Registering the id_resolver key type
[    0.848246] Key type id_resolver registered
[    0.852517] Key type id_legacy registered
[    0.856626] nfs4filelayout_init: NFSv4 File Layout Driver Registering...
[    0.863480] nfs4flexfilelayout_init: NFSv4 Flexfile Layout Driver Registering...
[    0.900256] Key type asymmetric registered
[    0.904448] Asymmetric key parser 'x509' registered
[    0.909473] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 244)
[    0.917166] io scheduler mq-deadline registered
[    0.921799] io scheduler kyber registered
[    0.925922] io scheduler bfq registered
[    0.932822] pinctrl-single 4084000.pinctrl: 34 pins, size 136
[    0.939357] pinctrl-single f4000.pinctrl: 171 pins, size 684
[    0.951281] Serial: 8250/16550 driver, 12 ports, IRQ sharing enabled
[    0.967718] loop: module loaded
[    0.971930] megasas: 07.725.01.00-rc1
[    0.978865] tun: Universal TUN/TAP device driver, 1.6
[    0.984933] VFIO - User Level meta-driver version: 0.3
[    0.991154] usbcore: registered new interface driver usb-storage
[    0.997855] i2c_dev: i2c /dev entries driver
[    1.003579] sdhci: Secure Digital Host Controller Interface driver
[    1.009917] sdhci: Copyright(c) Pierre Ossman
[    1.014565] sdhci-pltfm: SDHCI platform and OF driver helper
[    1.020994] ledtrig-cpu: registered to indicate activity on CPUs
[    1.027395] SMCCC: SOC_ID: ARCH_SOC_ID not implemented, skipping ....
[    1.034581] usbcore: registered new interface driver usbhid
[    1.040280] usbhid: USB HID core driver
[    1.045345] hw perfevents: enabled with armv8_cortex_a53 PMU driver, 7 counters available
[    1.054218] optee: probing for conduit method.
[    1.058796] optee: revision 4.4 (8f645256efc0dc66)
[    1.059085] optee: dynamic shared memory is enabled
[    1.069177] optee: initialized driver
[    1.074385] Initializing XFRM netlink socket
[    1.078809] NET: Registered PF_PACKET protocol family
[    1.084057] Key type dns_resolver registered
[    1.095735] registered taskstats version 1
[    1.100065] Loading compiled-in X.509 certificates
[    1.116894] ti-sci 44043000.system-controller: ABI: 4.0 (firmware rev 0x000a '10.1.8--v10.01.08 (Fiery Fox)')
[    1.178851] /bus@f0000/bus@b00000/i2c@2b200000/pmic@48: Fixed dependency cycle(s) with /bus@f0000/bus@b00000/i2c@2b200000/pmic@48/regulators/buck3
[    1.192500] omap_i2c 2b200000.i2c: bus 0 rev0.12 at 400 kHz
[    1.199449] /bus@f0000/i2c@20000000/usb-power-controller@3f/connector: Fixed dependency cycle(s) with /bus@f0000/usb@f900000/usb@31000000
[    1.212208] omap_i2c 20000000.i2c: bus 1 rev0.12 at 400 kHz
[    1.219264] pca953x 2-0023: supply vcc not found, using dummy regulator
[    1.226151] pca953x 2-0023: using AI
[    1.253853] omap_i2c 20010000.i2c: bus 2 rev0.12 at 100 kHz
[    1.260546] omap_i2c 20020000.i2c: bus 3 rev0.12 at 400 kHz
[    1.266784] ti-sci-intr 4210000.interrupt-controller: Interrupt Router 5 domain created
[    1.275117] ti-sci-intr bus@f0000:interrupt-controller@a00000: Interrupt Router 3 domain created
[    1.284356] ti-sci-inta 48000000.interrupt-controller: Interrupt Aggregator domain 28 created
[    1.293431] ti-sci-inta 4e400000.interrupt-controller: Interrupt Aggregator domain 200 created
[    1.302782] simple-framebuffer chosen:framebuffer@0: Can't parse width property
[    1.310267] simple-framebuffer: probe of chosen:framebuffer@0 failed with error -22
[    1.318360] ti-udma 485c0100.dma-controller: Number of rings: 82
[    1.326879] ti-udma 485c0100.dma-controller: Channels: 48 (bchan: 18, tchan: 12, rchan: 18)
[    1.337752] ti-udma 485c0000.dma-controller: Number of rings: 150
[    1.348708] ti-udma 485c0000.dma-controller: Channels: 35 (tchan: 20, rchan: 15)
[    1.358052] ti-udma 4e230000.dma-controller: Number of rings: 6
[    1.365372] ti-udma 4e230000.dma-controller: Channels: 6 (bchan: 0, tchan: 0, rchan: 6)
[    1.374860] printk: console [ttyS2] disabled
[    1.379539] 2800000.serial: ttyS2 at MMIO 0x2800000 (irq = 251, base_baud = 3000000) is a 8250
[    1.388404] printk: console [ttyS2] enabled
[    1.388404] printk: console [ttyS2] enabled
[    1.396868] printk: bootconsole [ns16550a0] disabled
[    1.396868] printk: bootconsole [ns16550a0] disabled
[    1.411334] spi-nor spi0.0: s28hs512t (65536 Kbytes)
[    1.416427] 7 fixed-partitions partitions found on MTD device fc40000.spi.0
[    1.423386] Creating 7 MTD partitions on "fc40000.spi.0":
[    1.428778] 0x000000000000-0x000000080000 : "ospi.tiboot3"
[    1.435477] 0x000000080000-0x000000280000 : "ospi.tispl"
[    1.441944] 0x000000280000-0x000000680000 : "ospi.u-boot"
[    1.448495] 0x000000680000-0x0000006c0000 : "ospi.env"
[    1.454670] 0x0000006c0000-0x000000700000 : "ospi.env.backup"
[    1.461455] 0x000000800000-0x000003fc0000 : "ospi.rootfs"
[    1.467920] 0x000003fc0000-0x000004000000 : "ospi.phypattern"
[    1.605357] am65-cpsw-nuss 8000000.ethernet: initializing am65 cpsw nuss version 0x6BA01903, cpsw version 0x6BA81903 Ports: 3 quirks:00000006
[    1.618241] am65-cpsw-nuss 8000000.ethernet: initialized cpsw ale version 1.5
[    1.625371] am65-cpsw-nuss 8000000.ethernet: ALE Table size 512
[    1.632629] am65-cpsw-nuss 8000000.ethernet: CPTS ver 0x4e8a010d, freq:500000000, add_val:1 pps:0
[    1.647133] am65-cpsw-nuss 8000000.ethernet: set new flow-id-base 19
[    1.657918] /bus@f0000/i2c@20000000/usb-power-controller@3f/connector: Fixed dependency cycle(s) with /bus@f0000/usb@f900000/usb@31000000
[    1.670392] /bus@f0000/usb@f900000/usb@31000000: Fixed dependency cycle(s) with /bus@f0000/i2c@20000000/usb-power-controller@3f/connector
[    1.685089] xhci-hcd xhci-hcd.0.auto: xHCI Host Controller
[    1.690632] xhci-hcd xhci-hcd.0.auto: new USB bus registered, assigned bus number 1
[    1.698393] xhci-hcd xhci-hcd.0.auto: USB3 root hub has no ports
[    1.704397] xhci-hcd xhci-hcd.0.auto: hcc params 0x0258fe6d hci version 0x110 quirks 0x0000008020000010
[    1.713821] xhci-hcd xhci-hcd.0.auto: irq 266, io mem 0x31100000
[    1.720623] hub 1-0:1.0: USB hub found
[    1.724409] hub 1-0:1.0: 1 port detected
[    1.809071] pca953x 2-0022: supply vcc not found, using dummy regulator
[    1.815838] pca953x 2-0022: using AI
[    1.826989] mmc1: CQHCI version 5.10
[    1.827959] clk: Disabling unused clocks
[    1.841257] ALSA device list:
[    1.844294]   No soundcards found.
[    1.874401] mmc1: SDHCI controller on fa00000.mmc [fa00000.mmc] using ADMA 64-bit
[    1.882195] Waiting for root device PARTUUID=076c4a2a-02...
[    1.934102] mmc1: new ultra high speed SDR104 SDXC card at address aaaa
[    1.941350] mmcblk1: mmc1:aaaa SR64G 59.5 GiB
[    1.947539]  mmcblk1: p1 p2
[    2.133076] EXT4-fs (mmcblk1p2): mounted filesystem e3d052ce-243a-4df4-aae0-f48d8df77bc1 r/w with ordered data mode. Quota mode: none.
[    2.145293] VFS: Mounted root (ext4 filesystem) on device 179:2.
[    2.151946] devtmpfs: mounted
[    2.155574] Freeing unused kernel memory: 2496K
[    2.160196] Run /sbin/init as init process
[    2.171502] Run /etc/init as init process
[    2.176029] Run /bin/init as init process
[    2.181080] Run /bin/sh as init process
[    2.356887] panel-simple display: supply power not found, using dummy regulator
[    2.387529] [drm] Initialized tidss 1.0.0 20180215 for 30200000.dss on minor 0
[    2.455851] Console: switching to colour frame buffer device 240x45
[    2.478253] tidss 30200000.dss: [drm] fb0: tidssdrmfb frame buffer device
bash.real: cannot set terminal process group (-1): Inappropriate ioctl for device
bash.real: no job control in this shell
bash.real-5.2#

 As per the log, uEnv.txt is loading, and 'below' is loading all the time.

Kernel command line: console=ttyS2,115200n8 earlycon=ns16550a,mmio32,0x02800000 root=PARTUUID=076c4a2a-02 rw rootfstype=ext4 rootwait

  • Hi Shanooj,

    Have you tried to add "quiet" to boot args either in the kernel device tree or kernel config(CONFIG_CMDLINE) as mentioned in the below SDK documentation:

    https://software-dl.ti.com/processor-sdk-linux/esd/AM62X/10_01_10_04/exports/docs/linux/How_to_Guides/Target/How_to_boot_quickly.html#reducing-linux-kernel-boot-time

    Best Regards,

    Suren

  • Have you tried to add "quiet" to boot args either in the kernel device tree or kernel config(CONFIG_CMDLINE) as mentioned in the below SDK documentation:

    Yes.

    Added in K3-am62p5-sk.dts 

    chosen {
    		#address-cells = <2>;
    		#size-cells = <2>;
    		ranges;
    
    		bootargs = "console=ttyS2,115200n8 earlycon=ns16550a,mmio32,0x02800000 root=/dev/mmcblk1p2 rw rootfstype=ext4 rootwait init=/init quiet bootdelay=0";
    		stdout-path = &main_uart0;
    		// bootargs = "console=ttyS2,115200n8 earlycon=ns16550a,mmio32,0x02800000 root=/dev/mmcblk1p2 rw rootfstype=ext4 rootwait quiet loglevel=0 bootdelay=0";
    		framebuffer0: framebuffer@0 {
    			compatible = "simple-framebuffer";
    			power-domains = <&k3_pds 186 TI_SCI_PD_EXCLUSIVE>,
    					<&k3_pds 243 TI_SCI_PD_EXCLUSIVE>,	/* OLDI0 */
    					<&k3_pds 244 TI_SCI_PD_EXCLUSIVE>;	/* OLDI1 */
    			clocks = <&k3_clks 186 6>,
    				 <&dss0_vp1_clk>,
    				 <&k3_clks 186 2>;
    			display = <&dss0>;
    			status = "okay";
    		};
    	};

    And in config 

    #
    # Boot options
    #
    CONFIG_CMDLINE="console=ttyS2,115200n8 rootwait init=/init quiet loglevel=0 bootdelay=0"
    CONFIG_CMDLINE_FROM_BOOTLOADER=y
    # CONFIG_CMDLINE_FORCE is not set
    CONFIG_EFI_STUB=y
    CONFIG_EFI=y
    CONFIG_DMI=y
    # end of Boot options

    But still a getting the same 

    "Kernel command line: console=ttyS2,115200n8 earlycon=ns16550a,mmio32,0x02800000 root=PARTUUID=076c4a2a-02 rw rootfstype=ext4 rootwait"

  • Hi Shanooj,

    Can you run  "env default -a -f" at u-boot and then boot. I assume its  still taking the previous bootargs.

    Best Regards,

    Suren

  • => env default -a -f
    ## Resetting to default environment
    => saveenv
    Unknown command 'saveenv' - try 'help'
    => reset
    resetting ..

    Tried the same, and the result is still the same.

    Starting kernel ...
    
    [    0.000000] Booting Linux on physical CPU 0x0000000000 [0x410fd034]
    [    0.000000] Linux version 6.6.58-ti-01497-ga7758da17c28-dirty (oe-user@oe-host) (aarch64-oe-linux-gcc (GCC) 13.3.0, GNU ld (GNU Binutils) 2.42.0.20240723) #1 SMP PREEMPT Wed Nov 27 13:23:15 UTC 2024
    [    0.000000] KASLR disabled due to lack of seed
    [    0.000000] Machine model: Texas Instruments AM62P5 SK
    [    0.000000] earlycon: ns16550a0 at MMIO32 0x0000000002800000 (options '')
    [    0.000000] printk: bootconsole [ns16550a0] enabled
    [    0.000000] efi: UEFI not found.
    [    0.000000] Reserved memory: created CMA memory pool at 0x00000009dc000000, size 576 MiB
    [    0.000000] OF: reserved mem: initialized node linux,cma, compatible id shared-dma-pool
    [    0.000000] OF: reserved mem: 0x00000009dc000000..0x00000009ffffffff (589824 KiB) map reusable linux,cma
    [    0.000000] OF: reserved mem: 0x0000000080000000..0x000000008007ffff (512 KiB) nomap non-reusable tfa@80000000
    [    0.000000] OF: reserved mem: 0x0000000093500000..0x000000009b4fffff (131072 KiB) nomap non-reusable rtos-framebuffer-memory@93500000
    [    0.000000] OF: reserved mem: 0x000000009e800000..0x000000009fffffff (24576 KiB) nomap non-reusable optee@9e800000
    [    0.000000] Zone ranges:
    [    0.000000]   DMA      [mem 0x0000000080000000-0x00000000ffffffff]
    [    0.000000]   DMA32    empty
    [    0.000000]   Normal   [mem 0x0000000100000000-0x00000009ffffffff]
    [    0.000000] Movable zone start for each node
    [    0.000000] Early memory node ranges
    [    0.000000]   node   0: [mem 0x0000000080000000-0x000000008007ffff]
    [    0.000000]   node   0: [mem 0x0000000080080000-0x00000000934fffff]
    [    0.000000]   node   0: [mem 0x0000000093500000-0x000000009b4fffff]
    [    0.000000]   node   0: [mem 0x000000009b500000-0x000000009e7fffff]
    [    0.000000]   node   0: [mem 0x000000009e800000-0x000000009fffffff]
    [    0.000000]   node   0: [mem 0x00000000a0000000-0x00000000ffffffff]
    [    0.000000]   node   0: [mem 0x0000000880000000-0x00000009ffffffff]
    [    0.000000] Initmem setup node 0 [mem 0x0000000080000000-0x00000009ffffffff]
    [    0.000000] psci: probing for conduit method from DT.
    [    0.000000] psci: PSCIv1.1 detected in firmware.
    [    0.000000] psci: Using standard PSCI v0.2 function IDs
    [    0.000000] psci: Trusted OS migration not required
    [    0.000000] psci: SMC Calling Convention v1.5
    [    0.000000] percpu: Embedded 20 pages/cpu s43176 r8192 d30552 u81920
    [    0.000000] Detected VIPT I-cache on CPU0
    [    0.000000] CPU features: detected: GIC system register CPU interface
    [    0.000000] CPU features: detected: ARM erratum 845719
    [    0.000000] alternatives: applying boot alternatives
    [    0.000000] Kernel command line: console=ttyS2,115200n8 earlycon=ns16550a,mmio32,0x02800000 root=PARTUUID=076c4a2a-02 rw rootfstype=ext4 rootwait
    [    0.000000] Dentry cache hash table entries: 1048576 (order: 11, 8388608 bytes, linear)
    [    0.000000] Inode-cache hash table entries: 524288 (order: 10, 4194304 bytes, linear)
    [    0.000000] Built 1 zonelists, mobility grouping on.  Total pages: 2064384
    [    0.000000] mem auto-init: stack:all(zero), heap alloc:off, heap free:off
    

  • Hi Shanooj,

    Do you still need help here? 

    Best Regards,

    Suren

  • Yes, still the bootargs are not taking. its always pointing to default. 

  • Hi Shanooj,

    I am currently testing with 11.1 SDK and I do have this change on my device tree:

    diff --git a/arch/arm64/boot/dts/ti/k3-am62p5-sk.dts b/arch/arm64/boot/dts/ti/k3-am62p5-sk.dts
    index ddcbdee853e6..fae7dc52d539 100644
    --- a/arch/arm64/boot/dts/ti/k3-am62p5-sk.dts
    +++ b/arch/arm64/boot/dts/ti/k3-am62p5-sk.dts
    @@ -38,6 +38,7 @@ chosen {
                    ranges;
    
                    stdout-path = &main_uart0;
    +               bootargs = "console=ttyS2,115200n8 quiet earlycon=ns16550a,mmio32,0x02800000 root=/dev/mmcblk1p2 rw rootfstype=ext4 rootwait";
    
                    framebuffer0: framebuffer@0 {
                            compatible = "simple-framebuffer";

    I am using yocto to build my core minimal image for fast boot and take the Linux Image and DTS file generated by yocto, convert it to Linux AppImage and flash that image on NOR flash.

    I can share a document via email that will walk you through the steps.

    Best Regards,

    Suren

  • Thank you. I will try and update.