Part Number: AM2431
Hi experts,
The TMDS234EVM uses HiTg material(Iteq IT180A) with a glass transition temperature (Tg) of 170 °C or higher.
Could you please explain why a substrate with Tg above 170 °C is necessary?
Generally, I assume it’s for heat resistance and rigidity, but since this is a microcontroller board, it shouldn’t generate much heat, so I expect it’s to prevent warping.
I’d like to know if there are any other reasons. Because the material is hard, drilling and similar processes may have limitations. When looking ahead to mass production, I want to identify if there are any restrictions.
Best regards,
O.H