Part Number: TDA4VE-Q1
Hello , TI experts ! We have a fast_BEV model , we cut it to two pieces . The input of the second one 's shape is 1*80*100*100 . We use rtos to import the model , because of the input is not picture , so we have to use binary input formal to import the model . But , when wen import the step2 model , the simulation inference result abnormal . So we compared each layer output of both onnx model and bin model . We find the diffenence is big . So how can we sovle this problem ? we use sdk ti-processor-sdk-rtos-j722s-evm-11_00_00_06 . to_ti.zip