Part Number: AM3352
I have a question regarding the RTC on the AM3352. I understand from the TRM that read and write operations only specify up to the second.
When writing the time, are fractions of a second (milliseconds) not reset to zero?
Or is there no way to set fractions of a second to zero?
I believe fractions of a second are active during time writing, causing an error of up to one second when setting the time, which is causing me trouble.
Best Regards,
Kanae