This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA3MV: TDA3 USE ISP

Part Number: TDA3MV

I want to display the format below on my ISP.

    info->width             = 640;
    info->height            = 480;
    info->dataFormat        = SYSTEM_DF_YUV422I_UYVY;
    info->bpp               = SYSTEM_BPP_BITS8;
    info->features          = ISS_SENSORS_THERMAL_FEATURES;

After connecting to the link and running it, I get the following error.

IssCapture -> IssM2mIsp -> Display_Video

[IPU1-0]      2.229854 s:  ISSCAPTURE: Create in progress !!!
[IPU1-0]      2.278716 s:  UTILS: DMA: Allocated CH (TCC) = 48 (48)
[IPU1-0]      2.278838 s:  UTILS: DMA: 0 of 1: Allocated PaRAM = 48 (0x63304800)
[IPU1-0]      2.279052 s:  ISSCAPTURE: Create Done !!!
[IPU1-0]      2.279326 s:  ISSM2MISP: Create in progress !!!
[IPU1-0]      2.320258 s:  Assertion @ Line: 725 in issM2mIspLink_drv_create_delete.c: (Bool)0U : failed !!!
[IPU1-0]      2.320746 s:  Assertion @ Line: 725 in issM2mIspLink_drv_create_delete.c: (Bool)0U : failed !!!

I think it's coming from the BPP side. Could the format settings be incorrect?

According to the link below, my ISP doesn't support YUV input. Is that correct?

e2e.ti.com/.../rtos-tda3-using-capturelink-with-issm2mresizer