This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMDXEVM6678L xds100 connection issue

Hi,

I am trying to set up the xds100 + rs232 interface to the above board from Windows 7 (64-bit).  The OS is running in VirtualBox on a MacBook BTW and is a fresh/new install specifically for this purpose.

I installed CCS 5.1 then inserted the USB cable.  Windows automatically starts installing the driver, but then fails.

I end up with a driver called usbccgp.sys version 6.1.7600.16788 (win7_gdr.110324-1506) 

This is completely different from the driver (and associated "ft....." files) that a colleague with a native Windows 7 has installed after the same procedure.

Looking for help on getting the right driver installed.

thanks