Part Number: AM62P
Hi,
I am using AM62P with two outputs enabled, Dual link OLDI & DSI. I use both outputs with same timing parameters and that are as per datasheet of panel and verified the same with modetest commands.
But while using weston with extended mode by the following command,
weston --backend=drm-backend.do --drm-device=card0 --additional-devices=card1
glmark2-es2-wayland -s 2560x1024
I was able to see a screen tear exactly in the middle of two displays (particularly while the cube rotation in the glmark2-es2-wayland). One side of the display seems to update faster than the other side which causes a screen tear when there is movement from one display to the other.
What causes this issue and how to proceed further?
Best Regards,
Harithan.